what is the startx file for imx53 quickstartboard when i addedd the startx file am able to get the keyboard perfectly but i am unable to see the display can any boady provide the startx file of imx53 quick start board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what is the startx file for imx53 quickstartboard when i addedd the startx file am able to get the keyboard perfectly but i am unable to see the display can any boady provide the startx file of imx53 quick start board

1,603 次查看
arunmondkar
Contributor I

startx file issue

标签 (1)
标记 (1)
0 项奖励
回复
5 回复数

1,290 次查看
Raybiztech
Contributor V

Hi Arun,

                  Try to export the display path and then try it again with the existing startx file you have.

$ export DISPLAY=:0

$ startx

Thanks & Regards,

Raybiztech.

0 项奖励
回复

1,290 次查看
arunmondkar
Contributor I

when i did export DISPLY=:0 and startx it is giving failed to open display matchbox-desktop unable to open display

match box can't open display check your Display variable is coming

0 项奖励
回复

1,290 次查看
YixingKong
Senior Contributor IV

Arun

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,290 次查看
YixingKong
Senior Contributor IV

Arun

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel free to contact Freescale.

Thanks,
Yixing

0 项奖励
回复

1,290 次查看
arunmondkar
Contributor I

thanx for your replay when i attach this startx file my keyboard is working fine but not display

*******************************************************************************************************************************************************************************

!/bin/sh
IS_BABBAGE=NO
grep Babbage /proc/cpuinfo > /dev/null 2>&1
if [ $? = 0 ]; then
if ! test -f do_not_exist; then
        IS_BABBAGE=YES
        Xfbdev -keybd keyboard,,device=/dev/input/keyboard0 -mouse mouse,2,device=/dev/input/mice &
else
        Xfbdev -mouse tslib,2,device=/dev/input/ts0 &
fi
fi
sleep 8

matchbox-window-manager -d :smileylaugh: -use_lowlight no -use_titlebar yes -use_cursor yes&
matchbox-desktop&
matchbox-panel  --bgtrans yes  &


sleep 5
# Calibrate when using the rootfs the first time
if [ $IS_BABBAGE = NO ]; then
        ls /usr/etc | grep pointercal > /dev/null 2>&1
        if [ $? = 1 ]; then
                ts_calibrate
        fi
fi
***************************************************************************************************************************************************************************

but when i attach this startx file

***********************************************************************************************************************************************************************************]

#!/bin/sh
IS_BABBAGE=NO
grep Babbage /proc/cpuinfo > /dev/null 2>&1
if [ $? = 0 ]; then
        IS_BABBAGE=YES
        Xfbdev  -nolisten tcp -keybd keyboard,,device=/dev/input/keyboard0 -mouse mouse,2,device=/dev/input/mice &
fi

if [ -L /dev/input/ts0 ]; then
       Xfbdev -mouse tslib,2,device=/dev/input/ts0 -mouse mouse,2,device=/dev/input/mice&
else
        Xfbdev -mouse mouse,2,device=/dev/input/mice&
fi

sleep 8

matchbox-window-manager -d :smileylaugh: -use_lowlight no -use_titlebar yes -use_cursor yes&
matchbox-desktop&
matchbox-panel  --bgtrans yes  &
sleep 5
# Calibrate when using the rootfs the first time
# Check whether the touch screen exists
if [ -L /dev/input/ts0 ]; then
        ls /usr/etc | grep pointercal > /dev/null 2>&1
        if [ $? = 1 ]; then
                ts_calibrate
        fi
fi
*******************************************************************************************************************************************************************************

Display is working with touch but not keyboard matchbox error is comming what is the problem can any one please give the replay as soon as possible

0 项奖励
回复