Hi all,
With a Sabresd board and linux L4.1.15, vProfiler doesn't work (.vpd file to 0):
1)
- galcore is loaded (built-in)
- export VIV_PROFILE=1
==> vprofiler.vpd file is created but size remains to 0
2)
echo 1 > /sys/module/galcore/parameters/gpuProfiler
echo 0 > /sys/module/galcore/parameters/powerManagement
==> doesn't change anything
Is there other things to do ? Is is due to the linux version ?
Rgds,
Christophe
Hi Christophe,
Have you tried with IMX6_L4.1.15_2.0.0_GPU_TOOL? It is available for download at the following link:
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------