IMX8MPLUS platform
DDR stress test pass successfully.
build flash.bin standalone
"uuu.exe -b emmc flash.bin" stuck on 99%, UART no log output.
is there any debug method for such situation?
ps:add -V parameters, it show error below:
99%libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 设备没有连接。
1:11>Okay (1.libusb: warning [winusb_get_device_list] could not detect installation state of driver for 'USB\VID_1FC9&PID_0146\6&17382A9&0&1': [3758096907] 设备实例不在硬件树中。
Hi Allon
one can recheck if uuu version is compatible with flash.bin,
recommended uuu version is described in Release Notes document of each bsp:
Best regards
igor
one can try on other computer.
Best regards
igor
could you try to reproduce issue on i.MX8M Plus EVK.
Best regards
igor
Hi, Igor,
Sorry,It should not be a uuu tools issue, cannt reproduce on EVK.
It may be customerize hardware or software problem, when stuck here, what's the possible problem, or how to debug it?
thanks a lot.