uuu 工具在win7 下无法自动解压烧录L4.9.123_2.3.0-ga_images_mx8mm.zip。 UUU log如下:
D:\Train\NXP\tools\uuu>uuu L4.9.123_2.3.0-ga_images_mx8mm.zip
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.91-0-g3799f4d
Your console don't support VT mode, fail back to verbose mode
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
Wait for Known USB Device Appear...
Error: fail open file: >L4.9.123_2.3.0-ga_images_mx8mm.zip/fsl-image-validation-imx-imx8mmevk.sdcard [?25h
另外执行 uuu fsl-image-validation-imx-imx8mmevk.sdcard.bz2,同样无法打开.sdcard.bz2压缩,(Error: fail open file:)
你好,和L4.9.123_2.3.0-ga_images_mx8mm.zip 里面uuu.auto脚本文件的FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard 这句有关系。L4.9.123_2.3.0-ga_images_mx8mm.zip 里面没有.sdcard后缀的文件,只有fsl-image-validation-imx-imx8mmevk.sdcard.bz2 但除了手动解压出.sdcard再执行烧录,还有什么别的方法么?
In the windows 7 you need to install driver, you also can see uuu usehttps://community.nxp.com/docs/DOC-342719 here for windows 10 and windows 7.
你好,文档看过了 win7的驱动是正常的能够连接上EV板,目前发现和L4.9.123_2.3.0-ga_images_mx8mm.zip 里面uuu.auto脚本文件的FB: flash -raw2sparse all fsl-image-validation-imx-imx8mmevk.sdcard 这句有关系。L4.9.123_2.3.0-ga_images_mx8mm.zip 里面没有.sdcard后缀的文件,只有fsl-image-validation-imx-imx8mmevk.sdcard.bz2 但除了手动解压出.sdcard再执行烧录,还有什么别的方法么?
Hi,
About use uuu to download the images to i.MX8M Mini EVK board you can refer to the link.
Get Started with the i.MX 8M Mini EVK | NXP
And on the window 7 you need to do some modify. You can see the document UUU.pdf
here Releases · NXPmicro/mfgtools · GitHub .
Have a great day,
Rita
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------