unused pin for eMMC device of i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unused pin for eMMC device of i.MX6

ソリューションへジャンプ
1,145件の閲覧回数
yuuki
Senior Contributor II

Dear all,

A eMMC device is connected to SD1 port.
When a system is booted from eMMC on SD1 port, I understand that a CD signal isn't used.
(GPIO_1 pin)

In that case, is it possible to use this pin as GPIO?

unsued pin for eMMC.png


Best Regards,
Yuuki

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
897件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

No, you cannot use the Card Detect pin as a GPIO, even if you connect the eMMC to the SD1 you still need the CD pin to enable the SD1.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
898件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Yuuki,

No, you cannot use the Card Detect pin as a GPIO, even if you connect the eMMC to the SD1 you still need the CD pin to enable the SD1.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信