ums 1 mmc 0 doesn't work based on kernel 4.14.98-2.3.0 or 2.3.2 in imx8qxpc0mek

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ums 1 mmc 0 doesn't work based on kernel 4.14.98-2.3.0 or 2.3.2 in imx8qxpc0mek

990 次查看
yibhan
Contributor III

Hi guys,

When I execute "ums 1 mmc 0" for downloading kernel image and dtb without entering uuu, the device always doesn't reset cpu and doesn't enter UMS mode.

Is this known issue on kernel 4.14.89-2.3.x? and do you have any idea to download kernel image and dtb without uuu?

Thanks in advance,

0 项奖励
回复
3 回复数

983 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yibeom

 

kernel 4.14.98-2.3.0 is very old kernel not more supported, recommended to migrate

to latest releases    https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Options for downloading image can be found in Linux Guide included in  Documentation

 

Best regards
igor

0 项奖励
回复

978 次查看
yibhan
Contributor III

Hi igorpadykov,

Thank you for answering.

I understand your comment, but i should keep kernel version to 4.14.98.2.3.x.

Do you have any patch to enable ums in kernel 4.14.98.2.3.x?

Thanks in advance

0 项奖励
回复

962 次查看
igorpadykov
NXP Employee
NXP Employee

as workaround one can try with atf from release L4.14.78 (rel_imx_4.14.98_2.0.0_ga + rel_imx_4.14.78_1.0.0_ga atf )

 

Best regards
igor

0 项奖励
回复