uImage in Yocto project not generated

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uImage in Yocto project not generated

ソリューションへジャンプ
2,336件の閲覧回数
disheng
Contributor III

Hello,

I have the Yocto project for L3.14.52_1.1.0_ga setup for imx6qsabred board and by running:

bitbake fsl-image-mfgtool-initramfs


I can see there is zImage_mfgtool generated but no uImage,
and I added


KERNEL_IMAGETYPE = "uImage"

to imx6qsabresd.conf and manage to generate a uImage.bin file, but not "uImage" which I can use in the mfg tool.

Question:
1. is the uImage.bin same as "uImage"? Can I use it directly in the mfg tool?
2. if not, how do I generate a "uImage" file in Yocto project?

Thank you,
Di

0 件の賞賛
返信
1 解決策
2,324件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

why do you need to use uimage? mfgtool can download zimage directly

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,325件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

why do you need to use uimage? mfgtool can download zimage directly

 

0 件の賞賛
返信
2,321件の閲覧回数
disheng
Contributor III

Hello Joan,

I figured that out afterwards... Thanks.

Now when we try to use mfgtool to flash, it gets stuck in the kernel and it seems to have unmatched machine id.

disheng_0-1617934959542.png

 

The id passed by uboot is f8c which is correct for imx6q, but the ids in kernel seems strange, all "ffffffff", do you know what can be wrong?

Regards,

Di

0 件の賞賛
返信