rt1170 jlink issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

rt1170 jlink issue

跳至解决方案
1,613 次查看
sukyeong
Contributor III

MCU : IMXRT1170-EVB

J-LINK , i want to use JTAG mode

swd mode works fine, but jtag mode is error.

I've referred to the posts below, but it doesn't work out.

help me please

 

https://community.nxp.com/t5/i-MX-RT/RT1176-connect-to-JLINK-with-a-warning/m-p/1599341

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1160-EVK-or-MIMXRT1170-E...

 

sukyeong_0-1686792722753.png

1. i try j6,j7 jumper remove

2. Is there anything in the circuit that needs to be changed?

sukyeong_1-1686792812321.png

sukyeong_2-1686792840297.png

 

0 项奖励
回复
1 解答
1,530 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with other functions.

 

Regards,

Jing

在原帖中查看解决方案

7 回复数
1,589 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

Please try to remove R2152 and  R2038.

 

Regards,

Jing

0 项奖励
回复
1,585 次查看
sukyeong
Contributor III

R2152, R2038을 찾을 수 없습니다..
자세한 내용을 알려주실 수 있나요?

 

@jingpan 

标记 (1)
0 项奖励
回复
1,562 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

You can search to this doc.

0 项奖励
回复
1,553 次查看
sukyeong
Contributor III
0 项奖励
回复
1,550 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

What is your board, EVK or EVKB?

 

Regards,

Jing

0 项奖励
回复
1,544 次查看
sukyeong
Contributor III
My board is EVK.
sorry for the confusion
@jingpan
0 项奖励
回复
1,531 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sukyeong ,

By default, the RT1170 silicon can use both SWD and JTAG modes using the Arm stitching sequence. For the RT1170EVK board, it defaults to use the SWD debug without any board modification. If you want to use the JTAG debug, solder out R187, R208, R195, and R78, because some JTAG signals are multiplexed with other functions.

 

Regards,

Jing