qmlscene and qmlviewer are missing from fsl-image-qt5-validation-imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qmlscene and qmlviewer are missing from fsl-image-qt5-validation-imx

ソリューションへジャンプ
2,387件の閲覧回数
grigoritimonen
Contributor II

Hi,

We use a NXP IMX 8MM EVK with Yocto Linux 4.14.98_2.0.0 from NXP.

I made a fsl-image-qt5-validation-imx image and can run some QT examples on target device.

However, I can't see qmlviewer or qmlscene tools for UI prototyping.

I was trying to search for *scene* and *viewer* files under meta-qt5 directory and didn't find anything related.

Any clues on how to build qmlscene and install it?

ラベル(3)
タグ(3)
0 件の賞賛
返信
1 解決策
2,215件の閲覧回数
grigoritimonen
Contributor II

Ok, I found that qmlscene is part of the SDK. So I was able to build a meta-toolchain-qt5 and copy /usr/bin/qt5/* to my rootfs.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,216件の閲覧回数
grigoritimonen
Contributor II

Ok, I found that qmlscene is part of the SDK. So I was able to build a meta-toolchain-qt5 and copy /usr/bin/qt5/* to my rootfs.

0 件の賞賛
返信