HI,
We have been working on iMX8M mini SoC based embedded platform. We need a parallel to MIPI CSI-2 bridge for our application. But most of the MIPI CSI-2 bridges signal operates at 1.2V whereas iMX8mm supports 1.8V logic level.
whether anyone has come across this issue? Please suggest on this !
已解决! 转到解答。
Hi Vijaybhaskar
i.MX8M Mini has 1.2 V power for analog part (VDD_MIPI_1P2) as described in
Table 10. Operating ranges
i.MX 8M Mini Applications Processor Datasheet for Consumer Products
and compliant MIPI CSI2 Specification V1.3, MIPI D-PHY specification V1.2.
Best regards
igor
HI igor,
Thanks for your prompt reply!
1) I have refereed table no 65 in iMX8 mini datasheet, it is mentioned that all the MIPI CSI and DSI signals fall in the power group of 1.8V.
2) previously, we have written a mail to NXP technical support. In reply mail you have mentioned that iMX8 mini MIPI signal voltage level is 1.8V.
Please clarify on above mentioned points. I am attaching some useful information for reference
thanks and regards,
vijay
Hi Vijaybhaskar
i.MX8M Mini has 1.2 V MIPI-CSI levels, though power group of 1.8V.
>2) previously, we have written a mail to NXP technical support. In reply mail
>you have mentioned that iMX8 mini MIPI signal voltage level is 1.8V.
sorry this is not true. In attached answer there are no such words.
Most correct answer can be found in MIPI CSI2, MIPI D-PHY specifications
for example one can look at sect.4.12.12 MIPI D-PHY Timing Parameters
i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet
Best regards
igor