parallel to MIPI CSI-2 bridge for iMX8mm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

parallel to MIPI CSI-2 bridge for iMX8mm

ソリューションへジャンプ
4,303件の閲覧回数
vijay_techsavvy
Contributor II

HI,

We have been working on iMX8M mini SoC based embedded platform. We need a parallel to MIPI CSI-2 bridge for our application. But most of the MIPI CSI-2 bridges signal operates at 1.2V whereas iMX8mm supports 1.8V logic level.

whether anyone has come across this issue? Please suggest on this !

ラベル(1)
0 件の賞賛
返信
1 解決策
4,273件の閲覧回数
vijay_techsavvy
Contributor II

Hi igor,

 

 Thanks for technical support !

We got it clarified on this.

regards,

vijay 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,297件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vijaybhaskar

 

i.MX8M Mini has 1.2 V power for analog part (VDD_MIPI_1P2) as described in

Table 10. Operating ranges

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

and compliant MIPI CSI2 Specification V1.3, MIPI D-PHY specification V1.2.

 

Best regards
igor

0 件の賞賛
返信
4,286件の閲覧回数
vijay_techsavvy
Contributor II

HI igor,

Thanks for your prompt reply!

1) I have refereed table no 65 in iMX8 mini datasheet, it is mentioned that all the MIPI CSI and DSI signals fall in the power group of 1.8V.

2) previously, we have written a mail to NXP technical support. In reply mail you have mentioned that iMX8 mini MIPI signal voltage level is 1.8V.

Please  clarify on above mentioned points. I am attaching some useful information for reference 

thanks and regards,

vijay

 

mipi_imx8.png

 

mipi1_imx8 (2).png

 

 

0 件の賞賛
返信
4,281件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vijaybhaskar

 

i.MX8M Mini has 1.2 V MIPI-CSI levels, though power group of 1.8V.

 

>2) previously, we have written a mail to NXP technical support. In reply mail

>you have mentioned that iMX8 mini MIPI signal voltage level is 1.8V.

 

sorry this is not true. In attached answer there are no such words.

Most correct answer can be found in MIPI CSI2, MIPI D-PHY specifications

for example one can look at sect.4.12.12 MIPI D-PHY Timing Parameters

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

 

Best regards
igor

0 件の賞賛
返信
4,274件の閲覧回数
vijay_techsavvy
Contributor II

Hi igor,

 

 Thanks for technical support !

We got it clarified on this.

regards,

vijay 

 

 

 

0 件の賞賛
返信