ov5640 ipu_prp_vf_sdc.ko ipu_prp_vf_sdc_bg.ko

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ov5640 ipu_prp_vf_sdc.ko ipu_prp_vf_sdc_bg.ko

959 Views
俊宝胡
Contributor I

To test the ov5640_mipi camera, use the following commands to install the kernel

modules of the camera driver and V4L2 Capture

insmod ipu_csi_enc.ko

insmod ipu_prp_enc.ko

insmod ipu_prp_vf_sdc.ko

insmod ipu_prp_vf_sdc_bg.ko

insmod ipu_still.ko

insmod mxc_v4l2_capture.ko

insmod ov5640_camera_mipi.ko

but hower ,i don't  find ipu_prp_vf_sdc.ko ipu_prp_vf_sdc_bg.ko in the /lib/modules/3.10.17-1.0.0_ga+g232293e/kernel/drivers/media/platform/mxc/capture

when i  complie kernel(linux3.10.17),i found CONFIG_MXC_IPU_PRP_VF_SDC  doesn't complie  moudles.

pastedImage_2.png

when i complie in the kernel ,has follows  error

  LD      kernel/built-in.o

  CC      drivers/media/platform/mxc/capture/mxc_v4l2_capture.o

  CC      drivers/media/platform/mxc/capture/ipu_prp_vf_sdc.o

  drivers/media/platform/mxc/capture/ipu_prp_vf_sdc.c:25:27: fatal error: mach/hardware.h: No such file or directory

if i want test mipi ov5640_cammer,how should i do,help me ,thanks!

0 Kudos
Reply
1 Reply

584 Views
joanxie
NXP TechSupport
NXP TechSupport

in L3.0.35_4.1.0bsp, one can build this, but I'm not sure for the yocto bsp, if you don't install these modules, you coudln't test mipi, right?

and could you tell me what funtion you want to test on mx6? let me check this.

0 Kudos
Reply