各位飞思卡尔的工程师:
你们好!
我这边在使用android5.1版本的mfg烧写工具烧写镜像文件之后,使用android4.3版本的mfg烧写工具烧写之前旧版本的镜像文件时uboot没法烧写进去。
android5.1版本的mfg烧写工具烧写的uboot是2015版本的,在使用android4.3版本的mfg烧写工具烧写2009版本的uboot,烧写成功后启动的还是2015的uboot,导致无法正确引导内核
请问如何在烧写了2015版本的uboot之后,如何烧写旧版本的2009 版uboot
Solved! Go to Solution.
Hi li chen,
你这里按照原来的方法和步骤就是可以的,应该不会出现什么问题。你这里内核无法启动,是不是你u-boot中的boot command没有设置正确。你检查一下。有问题我们再沟通。
Have a nice day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi li chen,
你这里按照原来的方法和步骤就是可以的,应该不会出现什么问题。你这里内核无法启动,是不是你u-boot中的boot command没有设置正确。你检查一下。有问题我们再沟通。
Have a nice day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
谢谢Dan
已经搞定了,修改了ucl2.xml文件
修改前:
<CMD state="Updater" type="push" body="$ echo 1 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access boot partition 1</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/u-boot-6q.bin">Sending U-Boot</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=2 skip=2">write U-Boot to sd card</CMD>
<CMD state="Updater" type="push" body="$ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access user partition and enable boot partion 1 to boot</CMD>
修改后:
<CMD state="Updater" type="push" body="$ echo 0 > /sys/block/mmcblk0boot0/force_ro">access boot partition 1</CMD>
<CMD state="Updater" type="push" body="send" file="files/android/u-boot.bin">Sending U-Boot</CMD>
<CMD state="Updater" type="push" body="$ dd if=$FILE of=/dev/mmcblk0boot0 bs=512 seek=2 skip=2">write U-Boot to sd card</CMD>
<CMD state="Updater" type="push" body="$ echo 8 > /sys/devices/platform/sdhci-esdhc-imx.3/mmc_host/mmc0/mmc0:0001/boot_config">access user partition and enable boot partion 1 to boot</CMD>
以上两个步骤做完,用修改过的mfg重新烧写android 4.3版本,启动的uboot
变回2009版本,并且可以正确引导系统启动
Hi chen,
I am very glad your problem solved:smileyhappy:. If you have new questions you can create new threads in our community.
Have a nice day
Dan