Hi,
I downloaded android kitkat image from android_kk4.4.2_1.0.0-ga_core_image_6slevk and set the output to HDMI but it doesn't work. There is an error imx_epdc_fb imx_epdc_fb: Unable to get display PMIC regulator.err = 0xffffffed.
My bootargs: bootargs console=ttymxc0,115200 init=/init androidboot.console=ttymxc0 video=mxcfb0:dev=hdmi,bpp=32 androidboot.hardware=freescale.
Can anyone help me with this issue?
Regards,
Bruce
Original Attachment has been moved to: kitkatboot.txt.zip
Hi Bruce
i.MX6SL (IMX6SLRM ) and i.MX6SL EVK (iMX6SL_EVK_DESIGNFILES ) have not HDMI.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
I have a MCIMXHDMICARD connected. It works fine with Sharp TV using the SD card provided in the package but the Android version is 4.0.4.
Regards,
Bruce.
Hi Bruce
HDMI supports only limited number of video modes provided in android driver, reading EDID from
monitor. After EDID reading, the nearest video mode will be chosen in the
EDID video mode list. One can look at description in sect.
18.3.1 Setting the Video Kernel Parameter MX53UG
So one can check what mode is used by this monitor then recheck driver,
if it is supported. Also one can try other monitor.
Best regards
igor