Hi.
I'm trying to use the latest kernel in 1.5 Yocto release (3.10.9) on a Sabre SD board.
I add PREFERRED_VERSION_linux-imx_mx6 = "3.10.9" in my local.conf and everything compiles fine.
But when I bootup I get following (it hangs when the kernel should be started):
reading uImage
5092288 bytes read in 272 ms (17.9 MiB/s)
Booting from mmc ...
reading imx6q-sabresd.dtb
** Unable to read file imx6q-sabresd.dtb **
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.10.9-1.0.0_alpha+gdbf364
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5092224 Bytes = 4.9 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
Starting kernel ...
(hangs here)
I also tried to build a kernel direct from the Linux tree (version 3.8.0-rc7) and got the same problem.
reading uImage
3960872 bytes read in 215 ms (17.6 MiB/s)
Booting from mmc ...
reading imx6q-sabresd.dtb
18526 bytes read in 18 ms (1004.9 KiB/s)
## Booting kernel from Legacy Image at 12000000 ...
Image Name: Linux-3.8.0-rc7
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3960808 Bytes = 3.8 MiB
Load Address: 10008000
Entry Point: 10008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 13000000
Booting using the fdt blob at 0x13000000
Loading Kernel Image ... OK
Using Device Tree in place at 13000000, end 1300785d
Starting kernel ...
(hangs here)
Anyone who managed to boot the latest kernel version
Thanks,
Niklas
已解决! 转到解答。
I managed to fix it.
The problem was that I was missing the imx6q-sabresd.dtb file in the FAT partition.