Hi,
Could someone help to interpret the below device tree structure in imx6qdl.dtsi?
gpio4: gpio@020a8000 {
compatible = "fsl,imx6q-gpio", "fsl,imx35-gpio";
reg = <0x020a8000 0x4000>;
interrupts = <0 72 0x04 0 73 0x04>;
gpio-controller;
#gpio-cells = <2>;
interrupt-controller;
#interrupt-cells = <2>;
};
my problem is I can not figure out the meaning of "interrupts = <0 72 0x04 0 73 0x04>"
已解决! 转到解答。
combining your info and the fsl-imx-gpio.txt, I think the 6 values were belong to two interrupts
first interrupt
the first byte is type of interrupt (0 = spi interrupt, 1 = ppi interrupt)
the seconds byte is the port that hosts the low 16 pins
the third byte is the interrupt level
second interrupt
the fourth byte is the same of the first byte
the fifth byte is the port that hosts the high 16 pins
the sixth byte is the interrupt level
Hi Damien
description can be found on p.8 AN5125 http://cache.nxp.com/files/32bit/doc/app_note/AN5125.pdf or
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks igor for your message.
Even after read through the links you provided, I am still not able to understand the data block I listed with this question. Because in my data block there are six value inside structure "interrupts", but the links only talked with 2 values situation.
Do you have more info?
Best regards,
Damien