Hello:
I am debugging the rm67199 on IMX93.I have already downloaded the image such as:Image and imx93-11x11-evk-rm67199.dtb.
But the log reported error and the driver of rm67199 cann't work.The log is as follows
Can you help me?
U-Boot SPL 2023.04-dirty (Jun 03 2024 - 21:53:22 -0700)
SOC: 0xa1009300
LC: 0x2040010
PMIC: PCA9451A
PMIC: Over Drive Voltage Mode
DDR: 1866MTS
M33 prepare ok
Normal Boot
Trying to boot from BOOTROM
Boot Stage: Primary boot
image offset 0x8000, pagesize 0x200, ivt offset 0x0
Load image from 0x52400 by ROM_API
NOTICE: BL31: v2.8(release):lf-6.1.55-2.2.0-0-g08e9d4eef
NOTICE: BL31: Built : 06:43:30, Nov 21 2023
U-Boot 2023.04-dirty (Jun 03 2024 - 21:53:22 -0700)
CPU: i.MX93(52) rev1.1 1700 MHz (running at 1692 MHz)
CPU: Industrial temperature grade (-40C to 105C) at 28C
Reset cause: POR (0x1)
Model: NXP i.MX93 11X11 EVK board
DRAM: 2 GiB
tcpc_init: Can't find device id=0x52
setup_typec: tcpc portpd init failed, err=-19
setup_pd_switch: Can't find device id=0x73
TCPC: Vendor ID [0x33ef], Product ID [0x190c], Addr [I2C2 0x51]
tcpc_clear_alert dm_i2c_write failed, err -110
setup_typec: tcpc port1 init failed, err=-5
pca953x gpio@22: Error reading output register
Core: 226 devices, 36 uclasses, devicetree: separate
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... OK
[*]-Video Link 0adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19
[0] lcd-controller@4ae30000, video
[1] dsi@4ae10000, video_bridge
[2] hdmi@3d, panel
adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19
In: serial
Out: serial
Err: serial
BuildInfo:
- ELE firmware version 0.1.0-44880904
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: pca953x gpio@22: Error reading output register
pca953x gpio@22: Error reading output register
Could not get PHY for FEC0: addr 2
pca953x gpio@22: Error reading output register
pca953x gpio@22: Error reading output register
Could not get PHY for FEC0: addr 2
pca953x gpio@22: Error reading output register
pca953x gpio@22: Error reading output register
eth1: ethernet@428a0000 [PRIME]
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Working FDT set to 83000000
switch to partitions #0, OK
mmc0(part 0) is current device
** No partition table - mmc 0 **
Couldn't find partition mmc 0:1
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
65579 bytes read in 5 ms (12.5 MiB/s)
Working FDT set to 83000000
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
starting USB...
Bus usb@4c100000: tcpc_init: Polling TCPC POWER STATUS Initialization Status bit failed, ret = -5
tcpc_get_cc_status dm_i2c_read failed, err 3
tcpc_send_command dm_i2c_write failed, err -110
tcpc_send_command dm_i2c_write failed, err 3
tcpc_get_cc_status dm_i2c_read failed, err 3
Port not available.
Bus usb@4c200000: tcpc_setup_ufp_mode: Polling ALERT register, TCPC_ALERT_CC_STATUS bit failed, ret = -62
Port not available.
USB is stopped. Please issue 'usb start' first.
Running BSP bootcmd ...
switch to partitions #0, OK
mmc1 is current device
Failed to load 'boot.scr'
35009024 bytes read in 377 ms (88.6 MiB/s)
Booting from mmc ...
65579 bytes read in 5 ms (12.5 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Working FDT set to 83000000
Using Device Tree in place at 0000000083000000, end 000000008301302a
Working FDT set to 83000000
adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050]
[ 0.000000] Linux version 6.6.3-gccf0a99701a7-dirty (tangyuan@ubuntu) (aarch64-poky-linux-gcc (GCC) 12.3.0, GNU ld (GNU Binutils) 2.40.0.20230703) #2 SMP PREEMPT Mon Jun 10 00:01:36 PDT 2024
[ 0.000000] KASLR disabled due to lack of seed
[ 0.000000] Machine model: NXP i.MX93 11X11 EVK board
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000b0000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b0000000..0x00000000bfffffff (262144 KiB) map reusable linux,cma
[ 0.000000] OF: reserved mem: 0x000000002021e000..0x000000002021efff (4 KiB) nomap non-reusable rsc-table@2021e000
[ 0.000000] OF: reserved mem: 0x0000000096000000..0x0000000097dfffff (30720 KiB) nomap non-reusable optee_core@96000000
[ 0.000000] OF: reserved mem: 0x0000000097e00000..0x0000000097ffffff (2048 KiB) nomap non-reusable optee_shm@97e00000
[ 0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a4007fff (32 KiB) nomap non-reusable vdev0vring0@a4000000
[ 0.000000] OF: reserved mem: 0x00000000a4008000..0x00000000a400ffff (32 KiB) nomap non-reusable vdev0vring1@a4008000
[ 0.000000] OF: reserved mem: 0x00000000a4010000..0x00000000a4017fff (32 KiB) nomap non-reusable vdev1vring0@a4010000
[ 0.000000] OF: reserved mem: 0x00000000a4018000..0x00000000a401ffff (32 KiB) nomap non-reusable vdev1vring1@a4018000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4020000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer@a4020000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4020000..0x00000000a411ffff (1024 KiB) nomap non-reusable vdevbuffer@a4020000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4120000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node ele-reserved@a4120000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4120000..0x00000000a421ffff (1024 KiB) nomap non-reusable ele-reserved@a4120000
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node ethosu_region@C0000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000c0000000..0x00000000cfffffff (262144 KiB) map reusable ethosu_region@C0000000
[ 0.000000] earlycon: lpuart32 at MMIO32 0x0000000044380000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xffbc76c0-0xffbc9fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x0000000095ffffff]
[ 0.000000] node 0: [mem 0x0000000098000000-0x00000000a3ffffff]
[ 0.000000] node 0: [mem 0x00000000a4000000-0x00000000a421ffff]
[ 0.000000] node 0: [mem 0x00000000a4220000-0x00000000ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] On node 0, zone DMA: 8192 pages in unavailable ranges
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 22 pages/cpu s50536 r8192 d31384 u90112
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Virtualization Host Extensions
[ 0.000000] CPU features: detected: Qualcomm erratum 1009, or ARM erratum 1286807, 2441009
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] Fallback order for Node 0: 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 507904
[ 0.000000] Policy zone: DMA
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000f9800000-0x00000000fd800000] (64MB)
[ 0.000000] Memory: 1396328K/2064384K available (20864K kernel code, 1612K rwdata, 7628K rodata, 3904K init, 634K bss, 143768K reserved, 524288K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000048040000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 24.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x588fe9dc0, max_idle_ns: 440795202592 ns
[ 0.000000] sched_clock: 56 bits at 24MHz, resolution 41ns, wraps every 4398046511097ns
[ 0.008445] Console: colour dummy device 80x25
[ 0.012704] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=96000)
[ 0.022860] pid_max: default: 32768 minimum: 301
[ 0.027504] LSM: initializing lsm=capability,integrity
[ 0.032658] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.039935] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.048572] cacheinfo: Unable to detect cache hierarchy for CPU 0
[ 0.055045] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.061915] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.069550] rcu: Hierarchical SRCU implementation.
[ 0.074144] rcu: Max phase no-delay instances is 1000.
[ 0.080421] EFI services will not be available.
[ 0.085003] smp: Bringing up secondary CPUs ...
[ 0.089748] Detected VIPT I-cache on CPU1
[ 0.089822] GICv3: CPU1: found redistributor 100 region 0:0x0000000048060000
[ 0.089871] CPU1: Booted secondary processor 0x0000000100 [0x412fd050]
[ 0.090005] smp: Brought up 1 node, 2 CPUs
[ 0.111366] SMP: Total of 2 processors activated.
[ 0.116035] CPU features: detected: 32-bit EL0 Support
[ 0.121160] CPU features: detected: 32-bit EL1 Support
[ 0.126264] CPU features: detected: Data cache clean to the PoU not required for I/D coherence
[ 0.134845] CPU features: detected: Common not Private translations
[ 0.141078] CPU features: detected: CRC32 instructions
[ 0.146203] CPU features: detected: RCpc load-acquire (LDAPR)
[ 0.151912] CPU features: detected: LSE atomic instructions
[ 0.157458] CPU features: detected: Privileged Access Never
[ 0.163003] CPU features: detected: RAS Extension Support
[ 0.168380] CPU features: detected: Speculative Store Bypassing Safe (SSBS)
[ 0.175372] CPU: All CPU(s) started at EL2
[ 0.179385] alternatives: applying system-wide alternatives
[ 0.190888] devtmpfs: initialized
[ 0.200175] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.209689] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.225921] pinctrl core: initialized pinctrl subsystem
[ 0.232934] DMI not present or invalid.
[ 0.237066] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.243540] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.250485] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.258150] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.266013] audit: initializing netlink subsys (disabled)
[ 0.271527] audit: type=2000 audit(0.180:1): state=initialized audit_enabled=0 res=1
[ 0.271977] thermal_sys: Registered thermal governor 'step_wise'
[ 0.279036] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.285047] cpuidle: using governor menu
[ 0.295637] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.302219] ASID allocator initialised with 65536 entries
[ 0.308413] Serial: AMBA PL011 UART driver
[ 0.312317] imx mu driver is registered.
[ 0.316151] imx rpmsg driver is registered.
[ 0.327094] imx93-pinctrl 443c0000.pinctrl: initialized IMX pinctrl driver
[ 0.340851] platform 4ae10000.dsi: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/panel@0/port/endpoint
[ 0.350608] platform 4ae30000.lcd-controller: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/ports/port@0/endpoint
[ 0.364221] Modules: 24048 pages in range for non-PLT usage
[ 0.364235] Modules: 515568 pages in range for PLT usage
[ 0.370532] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.382351] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.388589] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.395348] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.401588] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.408347] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.414588] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.421347] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.429622] ACPI: Interpreter disabled.
[ 0.434188] iommu: Default domain type: Translated
[ 0.438746] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.445203] SCSI subsystem initialized
[ 0.449064] usbcore: registered new interface driver usbfs
[ 0.454309] usbcore: registered new interface driver hub
[ 0.459601] usbcore: registered new device driver usb
[ 0.465642] mc: Linux media interface: v0.10
[ 0.469700] videodev: Linux video capture interface: v2.00
[ 0.475165] pps_core: LinuxPPS API ver. 1 registered
[ 0.480049] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.489155] PTP clock support registered
[ 0.493212] EDAC MC: Ver: 3.0.0
[ 0.496790] scmi_core: SCMI protocol bus registered
[ 0.502063] FPGA manager framework
[ 0.505272] Advanced Linux Sound Architecture Driver Initialized.
[ 0.511921] Bluetooth: Core ver 2.22
[ 0.515261] NET: Registered PF_BLUETOOTH protocol family
[ 0.520532] Bluetooth: HCI device and connection manager initialized
[ 0.526856] Bluetooth: HCI socket layer initialized
[ 0.531704] Bluetooth: L2CAP socket layer initialized
[ 0.536740] Bluetooth: SCO socket layer initialized
[ 0.542014] vgaarb: loaded
[ 0.545299] clocksource: Switched to clocksource arch_sys_counter
[ 0.551443] VFS: Disk quotas dquot_6.6.0
[ 0.555137] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.562117] pnp: PnP ACPI: disabled
[ 0.570786] NET: Registered PF_INET protocol family
[ 0.575626] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.583994] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.592344] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.599989] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.607930] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.615766] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.622179] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.628740] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.635955] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.641876] RPC: Registered named UNIX socket transport module.
[ 0.647546] RPC: Registered udp transport module.
[ 0.652213] RPC: Registered tcp transport module.
[ 0.656891] RPC: Registered tcp-with-tls transport module.
[ 0.662353] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.669622] PCI: CLS 0 bytes, default 64
[ 0.673599] kvm [1]: IPA Size Limit: 40 bits
[ 0.677632] kvm [1]: GICv3: no GICV resource entry
[ 0.682375] kvm [1]: disabling GICv2 emulation
[ 0.686811] kvm [1]: GIC system register CPU interface enabled
[ 0.692630] kvm [1]: vgic interrupt IRQ9
[ 0.696526] kvm [1]: VHE mode initialized successfully
[ 0.702784] Initialise system trusted keyrings
[ 0.707212] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.713722] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.719617] NFS: Registering the id_resolver key type
[ 0.724459] Key type id_resolver registered
[ 0.728567] Key type id_legacy registered
[ 0.732573] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.739236] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.746612] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.752901] 9p: Installing v9fs 9p2000 file system support
[ 0.780607] Key type asymmetric registered
[ 0.784442] Asymmetric key parser 'x509' registered
[ 0.789349] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.796663] io scheduler mq-deadline registered
[ 0.801178] io scheduler kyber registered
[ 0.805190] io scheduler bfq registered
[ 0.814277] EINJ: ACPI disabled.
[ 0.822442] Bus freq driver module loaded
[ 0.832571] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.850821] printk: console [ttyLP0] enabled0x44380010 (irq = 17, base_baud = 1500000) is a FSL_LPUART
[ 0.850821] printk: console [ttyLP0] enabled
[ 0.859244] printk: bootconsole [lpuart32] disabled
[ 0.859244] printk: bootconsole [lpuart32] disabled
[ 0.884765] loop: module loaded
[ 0.889395] megasas: 07.725.01.00-rc1
[ 0.898961] tun: Universal TUN/TAP device driver, 1.6
[ 0.904892] thunder_xcv, ver 1.0
[ 0.908185] thunder_bgx, ver 1.0
[ 0.911430] nicpf, ver 1.0
[ 0.915254] pps pps0: new PPS source ptp0
[ 0.920267] fec 42890000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 0.927108] fec 42890000.ethernet: Using random MAC address: de:86:74:8b:ea:31
[ 0.935737] mdio_bus 42890000.ethernet-1: MDIO device at address 2 is missing.
[ 0.943546] fec 42890000.ethernet eth0: registered PHC device 0
[ 0.951233] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 0.958488] hns3: Copyright (c) 2017 Huawei Corporation.
[ 0.963849] hclge is initializing
[ 0.967211] e1000: Intel(R) PRO/1000 Network Driver
[ 0.972084] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 0.977845] e1000e: Intel(R) PRO/1000 Network Driver
[ 0.982804] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 0.988731] igb: Intel(R) Gigabit Ethernet Network Driver
[ 0.994124] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 0.999704] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.005983] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.012126] sky2: driver version 1.30
[ 1.016318] usbcore: registered new device driver r8152-cfgselector
[ 1.022619] usbcore: registered new interface driver r8152
[ 1.028693] VFIO - User Level meta-driver version: 0.3
[ 1.036180] usbcore: registered new interface driver uas
[ 1.041545] usbcore: registered new interface driver usb-storage
[ 1.047610] usbcore: registered new interface driver usbserial_generic
[ 1.054152] usbserial: USB Serial support registered for generic
[ 1.060159] usbcore: registered new interface driver ftdi_sio
[ 1.065903] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.073213] usbcore: registered new interface driver usb_serial_simple
[ 1.079792] usbserial: USB Serial support registered for carelink
[ 1.085895] usbserial: USB Serial support registered for flashloader
[ 1.092250] usbserial: USB Serial support registered for funsoft
[ 1.098255] usbserial: USB Serial support registered for google
[ 1.104180] usbserial: USB Serial support registered for hp4x
[ 1.109929] usbserial: USB Serial support registered for kaufmann
[ 1.116023] usbserial: USB Serial support registered for libtransistor
[ 1.122548] usbserial: USB Serial support registered for moto_modem
[ 1.128813] usbserial: USB Serial support registered for motorola_tetra
[ 1.135426] usbserial: USB Serial support registered for nokia
[ 1.141265] usbserial: USB Serial support registered for novatel_gps
[ 1.147624] usbserial: USB Serial support registered for siemens_mpi
[ 1.153982] usbserial: USB Serial support registered for suunto
[ 1.159900] usbserial: USB Serial support registered for vivopay
[ 1.165906] usbserial: USB Serial support registered for zio
[ 1.171574] usbcore: registered new interface driver usb_ehset_test
[ 1.181396] input: 44440000.bbnsm:pwrkey as /devices/platform/soc@0/44000000.bus/44440000.bbnsm/44440000.bbnsm:pwrkey/input/input0
[ 1.196817] bbnsm_rtc 44440000.bbnsm:rtc: registered as rtc0
[ 1.203161] bbnsm_rtc 44440000.bbnsm:rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
[ 1.212590] i2c_dev: i2c /dev entries driver
[ 1.219178] qoriq_thermal 44482000.tmu: invalid range data.
[ 1.226297] imx7ulp-wdt 42490000.watchdog: imx93 wdt probe
[ 1.260685] Bluetooth: HCI UART driver ver 2.3
[ 1.265179] Bluetooth: HCI UART protocol H4 registered
[ 1.270313] Bluetooth: HCI UART protocol BCSP registered
[ 1.275638] Bluetooth: HCI UART protocol LL registered
[ 1.280764] Bluetooth: HCI UART protocol ATH3K registered
[ 1.286167] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.292603] Bluetooth: HCI UART protocol Broadcom registered
[ 1.298273] Bluetooth: HCI UART protocol QCA registered
[ 1.305001] sdhci: Secure Digital Host Controller Interface driver
[ 1.311224] sdhci: Copyright(c) Pierre Ossman
[ 1.316108] Synopsys Designware Multimedia Card Interface Driver
[ 1.322592] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.329815] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.337172] fsl-se-fw se-fw2: assigned reserved memory node ele-reserved@a4120000
[ 1.346704] fsl-se-fw se-fw2: Successfully registered ele-trng
[ 1.352666] random: crng init done
[ 1.352992] fsl-se-fw se-fw2: i.MX secure-enclave: mu2 interface to firmware, configured.
[ 1.364344] mmc0: SDHCI controller on 42850000.mmc [42850000.mmc] using ADMA
[ 1.364475] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.378221] usbcore: registered new interface driver usbhid
[ 1.383838] usbhid: USB HID core driver
[ 1.390054] mxc-isi_v1 4ae40000.isi: mxc_isi.0 registered successfully
[ 1.398936] ethosu ethosu: assigned reserved memory node ethosu_region@C0000000
[ 1.445842] hw perfevents: enabled with armv8_cortex_a55 PMU driver, 7 counters available
[ 1.456614] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.464977] optee: probing for conduit method.
[ 1.469537] optee: revision 4.0 (a303fc80)
[ 1.470143] optee: dynamic shared memory is enabled
[ 1.479504] optee: initialized driver
[ 1.487779] NET: Registered PF_LLC protocol family
[ 1.492703] u32 classifier
[ 1.495424] input device check on
[ 1.499080] Actions configured
[ 1.499092] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 1.502946] NET: Registered PF_INET6 protocol family
[ 1.509499] mmcblk0: mmc0:0001 DA6016 14.7 GiB
[ 1.514728] Segment Routing with IPv6
[ 1.522117] In-situ OAM (IOAM) with IPv6
[ 1.522486] mmcblk0boot0: mmc0:0001 DA6016 4.00 MiB
[ 1.526192] NET: Registered PF_PACKET protocol family
[ 1.532237] mmcblk0boot1: mmc0:0001 DA6016 4.00 MiB
[ 1.536078] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 1.542037] mmcblk0rpmb: mmc0:0001 DA6016 4.00 MiB, chardev (234:0)
[ 1.554070] Bluetooth: RFCOMM TTY layer initialized
[ 1.565036] Bluetooth: RFCOMM socket layer initialized
[ 1.570185] Bluetooth: RFCOMM ver 1.11
[ 1.573939] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.579243] Bluetooth: BNEP filters: protocol multicast
[ 1.584467] Bluetooth: BNEP socket layer initialized
[ 1.589427] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.595341] Bluetooth: HIDP socket layer initialized
[ 1.600647] 8021q: 802.1Q VLAN Support v1.8
[ 1.604876] lib80211: common routines for IEEE802.11 drivers
[ 1.610585] 9pnet: Installing 9P2000 support
[ 1.615001] Key type dns_resolver registered
[ 1.632494] registered taskstats version 1
[ 1.636947] Loading compiled-in X.509 certificates
[ 1.668910] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[ 1.677339] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[ 1.699727] imx9_init_soc 47510000.efuse:imx93-soc: error -EINVAL: failed to register SoC device
[ 1.708551] imx9_init_soc: probe of 47510000.efuse:imx93-soc failed with error -22
[ 1.717987] mipi-dsi 4ae10000.dsi.0: Fixed dependency cycle(s) with /soc@0/dsi@4ae10000/ports/port@1/endpoint
[ 1.728793] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 1.736832] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ 1.746936] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[ 1.756855] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
[ 1.769033] imx-dwmac 428a0000.ethernet: IRQ eth_lpi not found
[ 1.775979] imx-dwmac 428a0000.ethernet: User ID: 0x10, Synopsys ID: 0x52
[ 1.782802] imx-dwmac 428a0000.ethernet: DWMAC4/5
[ 1.787586] imx-dwmac 428a0000.ethernet: DMA HW capability register supported
[ 1.794706] imx-dwmac 428a0000.ethernet: RX Checksum Offload Engine supported
[ 1.801829] imx-dwmac 428a0000.ethernet: TX Checksum insertion supported
[ 1.808519] imx-dwmac 428a0000.ethernet: Wake-Up On Lan supported
[ 1.814672] imx-dwmac 428a0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.822327] imx-dwmac 428a0000.ethernet: device MAC address de:9d:60:72:47:bb
[ 1.829473] imx-dwmac 428a0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 1.836255] imx-dwmac 428a0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.843037] imx-dwmac 428a0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 1.850599] imx-dwmac 428a0000.ethernet: Using 32/32 bits DMA host/device width
[ 1.868771] remoteproc remoteproc0: imx-rproc is available
[ 1.885706] st_lsm6dsx_i2c 0-006a: supply vdd not found, using dummy regulator
[ 1.893093] st_lsm6dsx_i2c 0-006a: supply vddio not found, using dummy regulator
[ 1.957428] st_lsm6dsx_i2c 0-006a: failed to read whoami register
[ 1.963743] st_lsm6dsx_i2c: probe of 0-006a failed with error -5
[ 1.970129] i2c i2c-0: LPI2C adapter registered
[ 1.976661] pca953x 1-0022: supply vcc not found, using dummy regulator
[ 1.983441] pca953x 1-0022: using AI
[ 1.987130] pca953x 1-0022: failed writing register
[ 1.992176] pca953x: probe of 1-0022 failed with error -5
[ 1.997940] adp5585 1-0034: Failed to read reg 0x00, ret is -5
[ 2.003776] adp5585: probe of 1-0034 failed with error -5
[ 2.009280] i2c i2c-1: LPI2C adapter registered
[ 2.015058] i2c 2-0050: Fixed dependency cycle(s) with /soc@0/usb@4c100000/port/endpoint
[ 2.023493] tcpci: probe of 2-0050 failed with error -5
[ 2.028898] i2c 2-0051: Fixed dependency cycle(s) with /soc@0/usb@4c200000/port/endpoint
[ 2.038005] adp5585 2-0034: Failed to read reg 0x00, ret is -5
[ 2.043868] adp5585: probe of 2-0034 failed with error -5
[ 2.049494] i2c 2-003c: Fixed dependency cycle(s) with /soc@0/bus@42800000/camera/csi@4ae00000/port/endpoint
[ 2.059587] i2c i2c-2: LPI2C adapter registered
[ 2.066492] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.074503] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ 2.084604] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[ 2.094535] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
[ 2.119149] dwc-mipi-csi2-host 4ae00000.csi: lanes: 2, name: mxc-mipi-csi2.0
[ 2.119405] sdhci-esdhc-imx 42860000.mmc: Got CD GPIO
[ 2.137766] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector
[ 2.146518] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector
[ 2.155227] OF: graph: no port node found in /soc@0/bus@42000000/i2c@42530000/tcpc@51/connector
[ 2.164407] mmc1: SDHCI controller on 42860000.mmc [42860000.mmc] using ADMA
[ 2.175564] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.183579] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ 2.193686] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[ 2.203635] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
[ 2.227268] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.235374] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ 2.245481] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[ 2.252130] mmc1: host does not support reading read-only switch, assuming write-enable
[ 2.263396] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
[ 2.286155] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.290257] mmc1: new ultra high speed SDR104 SDHC card at address 0001
[ 2.295753] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.301144] mmcblk1: mmc1:0001 SD16G 14.8 GiB
[ 2.306374] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.311171] clk: Disabling unused clocks
[ 2.319328] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.324525] mmcblk1: p1 p2
[ 2.331180] ALSA device list:
[ 2.336738] No soundcards found.
[ 2.336794] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.348116] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ 2.358229] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[ 2.368182] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
[ 2.400406] EXT4-fs (mmcblk1p2): recovery complete
[ 2.406511] EXT4-fs (mmcblk1p2): mounted filesystem 0ff2bc0a-e3a2-498e-8b3f-84260506d66a r/w with ordered data mode. Quota mode: none.
[ 2.418709] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 2.430013] devtmpfs: mounted
[ 2.434944] Freeing unused kernel memory: 3904K
[ 2.439653] Run /sbin/init as init process
[ 2.982741] systemd[1]: System time before build time, advancing clock.
[ 3.051177] systemd[1]: systemd 245.4-4ubuntu3.22 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=hybrid)
[ 3.074300] systemd[1]: Detected architecture arm64.
Welcome to Ubuntu 20.04.6 LTS!
[ 3.143473] systemd[1]: Set hostname to <localhost.localdomain>.
[ 3.184576] systemd[1]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set
[ 3.732941] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 3.754627] systemd[1]: Created slice system-modprobe.slice.
[ OK ] Created slice system-modprobe.slice.
[ 3.778653] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 3.802484] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.825808] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 3.849625] systemd[1]: Condition check resulted in Arbitrary Executable File Formats File System Automount Point being skipped.
[ 3.861479] systemd[1]: Reached target User and Group Name Lookups.
[ OK ] Reached target User and Group Name Lookups.
[ 3.885489] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.905441] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 3.925467] systemd[1]: Reached target Mounting snaps.
[ OK ] Reached target Mounting snaps.
[ 3.945432] systemd[1]: Reached target Mounted snaps.
[ OK ] Reached target Mounted snaps.
[ 3.965470] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 3.985883] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.010357] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 4.034026] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.058120] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.078154] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.101947] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.137874] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 4.162448] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.191321] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.213912] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[ 4.242134] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.262024] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
[ 4.279706] systemd[1]: Starting Load Kernel Module chromeos_pstore...
Starting Load Kernel Module chromeos_pstore...
[ 4.313778] systemd[1]: Condition check resulted in Load Kernel Module drm being skipped.
[ 4.322329] systemd[1]: Condition check resulted in Load Kernel Module efi_pstore being skipped.
[ 4.350253] systemd[1]: Starting Load Kernel Module pstore_blk...
Starting Load Kernel Module pstore_blk...
[ 4.398074] systemd[1]: Starting Load Kernel Module pstore_zone...
Starting Load Kernel Module pstore_zone...
[ 4.426080] systemd[1]: Starting Load Kernel Module ramoops...
Starting Load Kernel Module ramoops...
[ 4.451617] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.
[ 4.482092] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.508433] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.550123] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ 4.574546] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Finished Load Kernel Module chromeos_pstore.
[ OK ] Finished Load Kernel Module pstore_blk.
[ OK ] Finished Load Kernel Module pstore_zone.
[ OK ] Finished Load Kernel Module ramoops.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Finished Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Load/Save Random Seed...
Starting Apply Kernel Variables...
[ 4.914648] systemd-journald[138]: Received client request to flush runtime journal.
Starting Create System Users...
[ OK ] Mounted Kernel Configuration File System.
[ 5.031203] systemd-journald[138]: File /var/log/journal/f5fb6edf91414bdcbd789249cb473871/system.journal corrupted or uncleanly shut down, renaming and replacing.
[ OK ] Finished udev Coldplug all Devices.
[ OK ] Finished Load/Save Random Seed.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create System Users.
Starting Create Static Device Nodes in /dev...
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
[ OK ] Reached target Local File Systems.
Starting Tell Plymouth To Write Out Runtime Data...
Starting udev Kernel Device Manager...
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Tell Plymouth To Write Out Runtime Data.
Starting Create Volatile Files and Directories...
[ OK ] Finished Create Volatile Files and Directories.
Starting Network Name Resolution...
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Finished Update UTMP about System Boot/Shutdown.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ OK ] Reached target Local Encrypted Volumes.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ OK ] Started CUPS Scheduler.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Paths.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Trigger anacron every hour.
[ OK ] Started Daily apt download activities.
[ OK ] Started Daily apt upgrade and clean activities.
[ OK ] Started Periodic ext4 Onli…ata Check for All Filesystems.
[ OK ] Started Discard unused blocks once a week.
[ OK ] Started Refresh fwupd metadata regularly.
[ OK ] Started Daily man-db regeneration.
[ OK ] Started Message of the Day.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on CUPS Scheduler.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Socket activation for snappy daemon.
[ OK ] Started Network Name Resolution.
[ OK ] Listening on Socket activation for snappy daemon.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Accounts Service...
[ OK ] Started Run anacron jobs.
Starting LSB: automatic crash report generation...
Starting Avahi mDNS/DNS-SD Stack...
Starting Bluetooth management mechanism...
[ OK ] Started Regular background program processing daemon.
[ OK ] Started CUPS Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Network Manager...
Starting Remove Stale Onli…t4 Metadata Check Snapshots...
Starting Initialize hardware monitoring sensors...
Starting Dispatcher daemon for systemd-networkd...
[ OK ] Started Set the CPU Frequency Scaling governor.
Starting Authorization Manager...
Starting Restore /etc/reso… the ppp link was shut down...
[ OK ] Reached target Login Prompts (Pre).
Starting Snap Daemon...
Starting Switcheroo Control Proxy service...
Starting Login Service...
Starting WPA supplicant...
[ OK ] Finished Restore /etc/reso…re the ppp link was shut down.
[ OK ] Finished Initialize hardware monitoring sensors.
[ OK ] Started LSB: automatic crash report generation.
[ OK ] Started Login Service.
[ OK ] Started WPA supplicant.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Switcheroo Control Proxy service.
[ OK ] Started Make remote CUPS printers available locally.
[ OK ] Started Authorization Manager.
Starting Modem Manager...
[ OK ] Started Network Manager.
[ OK ] Reached target Network.
Starting Network Manager Wait Online...
Starting Permit User Sessions...
[ OK ] Started Unattended Upgrades Shutdown.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Accounts Service.
Starting Light Display Manager...
Starting Hold until boot process finishes up...
Starting Hostname Service...
[ OK ] Finished Hold until boot process finishes up.
[ OK ] Started Getty on tty1.
[ OK ] Started Hostname Service.
[ OK ] Started Light Display Manager.
[ OK ] Started Modem Manager.
Starting Network Manager Script Dispatcher Service...
[ OK ] Finished Remove Stale Onli…ext4 Metadata Check Snapshots.
[ OK ] Started Network Manager Script Dispatcher Service.
[ OK ] Started Snap Daemon.
[ OK ] Started Dispatcher daemon for systemd-networkd.
Starting Wait until snapd is fully seeded...
Starting Time & Date Service...
[ OK ] Started Time & Date Service.
[ 12.440938] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ OK ] Finished Wait until [ 12.470227] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
snapd is fully seeded.
[ 12.504731] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
[ OK ] Found device /dev/ttyLP0.
[ OK ] Started Serial Getty on ttyLP0.
[ OK ] Reached target Login Prompts.
Ubuntu 20.04.6 LTS localhost.localdomain ttyLP0
localhost login:
The critical error is as follows:
[ 2.336794] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 2.348116] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[ 2.358229] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[ 2.368182] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517
Hi, @5454ty
I have tested your issue on my site, and also add the log on the probe function, when the board boot, i can see the log output.
I think you can use the latest BSP code for test, and the driver file is "linux-imx/drivers/gpu/drm/panel/panel-raydium-rm67191.c"
B.R
HI, @5454ty
What is your BSP version?
Hi, @5454ty
Could you please share all of your test step? Also our i.mx93 do not support ubuntu OS.
B.R
您好,
张工,我可以用中文嘛
我是用TF卡来烧写的,
其实我暂时没有接我自己的新屏,我是这么想的,我首先在软件层次把RM67199跑起来,至少保证流程没错把,可是我加载了后,发现没有RM67191或者是RM67199的信息,PROBE函数加了打印也没有打
这个是我TF卡的内容
我TF卡里面有Image和imx93-11x11-evk-rm67199.dtb,
其他另外个分区是文件系统
我的UBOOT信息如下:
u-boot=>
u-boot=> print
arch=arm
auth_os=auth_cntr ${cntr_addr}
baudrate=115200
board=imx93_evk
board_name=11X11_EVK
board_rev=iMX93
boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefix}${script}; source ${scriptaddr}
boot_efi_binary=load ${devtype} ${devnum}:${distro_bootpart} ${kernel_addr_r} efi/boot/bootaa64.efi; if fdt addr -q ${fdt_addr_r}; then bootefi ${kernel_addr_r} ${fdt_addr_r};else bootefi ${kernel_addr_r} ${fdtcontroladdr};fi
boot_efi_bootmgr=if fdt addr -q ${fdt_addr_r}; then bootefi bootmgr ${fdt_addr_r};else bootefi bootmgr;fi
boot_extlinux=sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scriptaddr} ${prefix}${boot_syslinux_conf}
boot_fit=no
boot_net_usb_start=usb start
boot_os=booti ${loadaddr} - ${fdt_addr_r};
boot_prefixes=/ /boot/
boot_script_dhcp=boot.scr.uimg
boot_scripts=boot.scr.uimg boot.scr
boot_syslinux_conf=extlinux/extlinux.conf
boot_targets=mmc0 mmc1 usb0
bootargs=console=ttyLP0,115200 earlycon root=/dev/mmcblk1p2 rootwait rw
bootcmd=run sr_ir_v2_cmd;run distro_bootcmd;run bsp_bootcmd
bootcmd_mfg=run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot auto; fi;
bootcmd_mmc0=devnum=0; run mmc_boot
bootcmd_mmc1=devnum=1; run mmc_boot
bootcmd_usb0=devnum=0; run usb_boot
bootdelay=2
bootfstype=fat
bootm_size=0x10000000
bootscript=echo Running bootscript from mmc ...; source
bsp_bootcmd=echo Running BSP bootcmd ...; mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if test ${sec_boot} = yes; then if run loadcntr; then run mmcboot; else run netboot; fi; else if run loadimage; then run mmcboot; else run netboot; fi; fi; fi; fi;
cntr_addr=0x98000000
cntr_file=os_cntr_signed.bin
console=ttyLP0,115200 earlycon
cpu=armv8
distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done
distro_bootpart_uuid=076c4a2a-01
efi_dtb_prefixes=/ /dtb/ /dtb/current/
emmc_dev=0
eth1addr=16:5c:70:e4:6d:96
ethact=ethernet@428a0000
ethprime=eth1
fastboot_dev=mmc1
fdt_addr=0x83000000
fdt_addr_r=0x83000000
fdt_file=imx93-11x11-evk-rm67199.dtb
fdt_high=0xffffffffffffffff
fdtaddr=83000000
fdtcontroladdr=fced2890
fdtfile=imx93-11x11-evk-rm67199.dtb
fileaddr=80400000
filesize=2163200
ftdfile=imx93-11x11-evk-rm67199.dtb
image=Image
initrd_addr=0x83800000
initrd_high=0xffffffffffffffff
jh_mmcboot=setenv fdtfile ${jh_root_dtb}; setenv jh_clk clk_ignore_unused mem=1248MB kvm-arm.mode=nvhe; if run loadimage; then run mmcboot;else run jh_netboot; fi;
jh_netboot=setenv fdtfile ${jh_root_dtb}; setenv jh_clk clk_ignore_unused mem=1248MB kvm-arm.mode=nvhe; run netboot;
jh_root_dtb=imx93-11x11-evk-root.dtb
kboot=booti
kernel_addr_r=0x80400000
load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix}${efi_fdtfile}
loadaddr=0x80400000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadcntr=fatload mmc ${mmcdev}:${mmcpart} ${cntr_addr} ${cntr_file}
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr_r} ${fdtfile}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc clk_ignore_unused
mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi
mmcargs=setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot}
mmcautodetect=yes
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${sec_boot} = yes; then if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if run loadfdt; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk1p2 rootwait rw
netargs=setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; if test ${sec_boot} = yes; then ${get_cmd} ${cntr_addr} ${cntr_file}; if run auth_os; then run boot_os; else echo ERR: failed to authenticate; fi; else ${get_cmd} ${loadaddr} ${image}; if test ${boot_fit} = yes || test ${boot_fit} = try; then bootm ${loadaddr}; else if ${get_cmd} ${fdt_addr_r} ${fdtfile}; then run boot_os; else echo WARN: Cannot load the DT; fi; fi;fi;
nodes=/usbg1 /usbg2 /wdt-reboot /rm67199_panel /dsi-host /display-subsystem /soc@0/bus@44000000/dma-controller@44000000 /soc@0/bus@44000000/sai@443b0000 /soc@0/bus@44000000/mqs1 /soc@0/bus@44000000/bbnsm@44440000 /soc@0/bus@44000000/system-controller@44460000 /soc@0/bus@44000000/tmu@44482000 /soc@0/bus@44000000/micfil@44520000 /soc@0/bus@42000000/dma-controller@42000000 /soc@0/bus@44000000/i3c-master@44330000 /soc@0/bus@42000000/i3c-master@42520000 /soc@0/bus@42000000/sai@42650000 /soc@0/bus@42000000/sai@42660000 /soc@0/bus@42000000/mqs2 /soc@0/bus@42000000/xcvr@42680000 /soc@0/bus@42000000/flexio@425c0000 /soc@0/bus@42800000/epxp@4ae20000 /soc@0/bus@42800000/camera /soc@0/efuse@47510000 /soc@0/system-controller@4ac10000 /soc@0/ldb@4ac10020 /soc@0/phy@4ac10024 /soc@0/ele-mu /soc@0/dsi@4ae10000 /soc@0/lcd-controller@4ae30000 /soc@0/blk-ctrl@4e010000 /soc@0/memory-controller@4e300000 /soc@0/bus@44000000/i2c@44350000/pmic@25 /imx93-lpm
prepare_mcore=setenv mcore_clk clk-imx93.mcore_booted;
scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for prefix in ${boot_prefixes}; do run scan_dev_for_extlinux; run scan_dev_for_scripts; done;run scan_dev_for_efi;
scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env exists devplist || setenv devplist 1; for distro_bootpart in ${devplist}; do if fstype ${devtype} ${devnum}:${distro_bootpart} bootfstype; then part uuid ${devtype} ${devnum}:${distro_bootpart} distro_bootpart_uuid ; run scan_dev_for_boot; fi; done; setenv devplist
scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; for prefix in ${efi_dtb_prefixes}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${efi_fdtfile}; then run load_efi_dtb; fi;done;run boot_efi_bootmgr;if test -e ${devtype} ${devnum}:${distro_bootpart} efi/boot/bootaa64.efi; then echo Found EFI removable media binary efi/boot/bootaa64.efi; run boot_efi_binary; echo EFI LOAD FAILED: continuing...; fi; setenv efi_fdtfile
scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${boot_syslinux_conf}; then echo Found ${prefix}${boot_syslinux_conf}; run boot_extlinux; echo EXTLINUX FAILED: continuing...; fi
scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${script}; then echo Found U-Boot script ${prefix}${script}; run boot_a_script; echo SCRIPT FAILED: continuing...; fi; done
scriptaddr=0x83500000
sd_dev=1
sec_boot=no
serial#=2134e7f964370db9
soc=imx9
soc_type=imx93
splashimage=0x90000000
sr_ir_v2_cmd=cp.b ${fdtcontroladdr} ${fdt_addr_r} 0x10000;fdt addr ${fdt_addr_r};fdt resize 0x400;fdt set /soc@0/bus@44000000/i2c@44350000/gpio@34 compatible adi,adp5585;for i in ${nodes}; do fdt rm ${i}; done
usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_part; fi
vendor=freescale
video_link=2
Environment size: 7341/16380 bytes
u-boot=>
然后我也尝试过setenv fdtfile imx93-11x11-evk-rm67199.dtb
然后saveenv
仍然是不行,张工,能否看看,
老哥,我也是自己添加了屏幕,跟你报一样的错,请问是最后是怎么解决的啊?