Hi
Who can help me?
SDK:Android Q10.0.0_2.2.0_AUTO
nvp6324 connect 4 cameras
The evs function of the product mek_8q_car-userdebug has been adjusted, but the camera apk cannot be used to open the camera.
Therefore, I switched the product to mek_8q-userdebug to test the traditional method of using the camera, and I am currently experiencing problems:
The camera apk opens and previews no content.
Core video information
mek_8q:/ # ls sys/class/video4linux/
v4l-subdev0 v4l-subdev2 v4l-subdev4 video0 video12 video2
v4l-subdev1 v4l-subdev3 v4l-subdev5 video1 video13 video3
mek_8q:/ # cat sys/class/video4linux/video0/name
mxc_isi.0.capture
mek_8q:/ # cat sys/class/video4linux/video1/name
mxc_isi.1.capture
mek_8q:/ # cat sys/class/video4linux/video12/name
vpu decoder
mek_8q:/ # cat sys/class/video4linux/video13/name
vpu encoder
mek_8q:/ # cat sys/class/video4linux/video2/name
mxc_isi.2.capture
mek_8q:/ # cat sys/class/video4linux/video3/name
mxc_isi.3.capture
mek_8q:/ #
main error log
03-26 02:12:12.937 433 2408 E Camera3-Stream: getBuffer: wait for output buffer return timed out after 8000ms (max_buffers 2)
03-26 02:12:12.938 433 2408 V Camera3-Stream: getBuffer: Already dequeued max output buffers (2), wait for next returned one.
logcat_boot.log is the log of Android boot。
logcat_preview.log is the log of camera apk preview.
Hi
Can you offer the kernel log?
BR
Zhiming
Hi
The error happened in CameraHAL.Failed in below command.You need see if your camera support VIDIOC_DBG_G_CHIP_IDENT.
ret = ioctl(fd, VIDIOC_DBG_G_CHIP_IDENT, &vidChip);
Please help to see how to solve it。
Here is the main problem
ret = ioctl(mDev, VIDIOC_S_PARM, ¶m);
if (ret < 0) {
ALOGE("%s: VIDIOC_S_PARM Failed: %s", __func__, strerror(errno));
return ret;
}
error log
E FslCameraHAL: onDeviceConfigureLocked: VIDIOC_S_PARM Failed: Not a typewriter
E FslCameraHAL: handleConfigureLocked onDeviceConfigure failed
in the kernel
//vendor/nxp-opensource/kernel_imx/drivers/staging/media/imx/imx8-isi-cap.c
static int mxc_isi_cap_s_parm(struct file *file, void *fh,
struct v4l2_streamparm *a)
{
struct mxc_isi_cap_dev *isi_cap = video_drvdata(file);
struct v4l2_subdev *sd;
sd = mxc_get_remote_subdev(isi_cap, __func__);
if (!sd)
return -ENODEV;
return v4l2_s_parm_cap(video_devdata(file), sd, a);
}
Did not call nvp6324_s_parm。
The following three functions are called
.enum_frame_size = nvp6324_enum_framesizes,
.get_fmt = nvp6324_get_fmt,
.set_fmt = nvp6324_set_fmt,
I will consult with software team.
Hi nxf65025
Is there any good news?
Best wishes
thank you very much
The relevant documents are as follows:
//HAL
//vendor/nxp-opensource/imx/libcamera3/ImxCamera.cpp
ImxCamera::ImxCameraDMAStream::onDeviceConfigureLocked()
ret = ioctl(mDev, VIDIOC_S_PARM, ¶m);
if (ret < 0) {
ALOGE("%s: VIDIOC_S_PARM Failed: %s", __func__, strerror(errno));
return ret;
}
//kernel
//vendor/nxp-opensource/kernel_imx/drivers/staging/media/imx/imx8-isi-cap.c
static int mxc_isi_cap_s_parm(struct file *file, void *fh,
struct v4l2_streamparm *a)
{
struct mxc_isi_cap_dev *isi_cap = video_drvdata(file);
struct v4l2_subdev *sd;
sd = mxc_get_remote_subdev(isi_cap, __func__);
if (!sd)
return -ENODEV;
return v4l2_s_parm_cap(video_devdata(file), sd, a);
}
//vendor/nxp-opensource/kernel_imx/drivers/media/platform/imx8/nvp6324/nvp6324_video.c
static int nvp6324_s_parm(struct v4l2_subdev *sd, struct v4l2_streamparm *a)
{
......
}
I saw another problem I was trying to solve
E FslCameraHAL: onDeviceConfigureLocked: VIDIOC_S_PARM Failed: Not a typewriter
E FslCameraHAL: handleConfigureLocked onDeviceConfigure failed
I have solved this problem,
ioctl(fd, VIDIOC_DBG_G_CHIP_IDENT, &vidChip)
--- a/android_build/vendor/nxp-opensource/kernel_imx/drivers/staging/media/imx/imx8-isi-cap.c
+++ b/android_build/vendor/nxp-opensource/kernel_imx/drivers/staging/media/imx/imx8-isi-cap.c
@@ -1170,6 +1170,15 @@ static int mxc_isi_cap_s_selection(struct file *file, void *fh,
return 0;
}
+static int mxc_isi_cap_g_chip_ident(struct file *file, void *fh,
+ struct v4l2_dbg_chip_ident *chip)
+{
+ chip->match.type = V4L2_CHIP_MATCH_I2C_DRIVER;
+ strcpy(chip->match.name, "nvp6324_mipi_camera");
+
+ return 0;
+}
+
static int mxc_isi_cap_enum_framesizes(struct file *file, void *priv,
struct v4l2_frmsizeenum *fsize)
{
@@ -1285,6 +1294,7 @@ static const struct v4l2_ioctl_ops mxc_isi_capture_ioctl_ops = {
.vidioc_g_selection = mxc_isi_cap_g_selection,
.vidioc_s_selection = mxc_isi_cap_s_selection,
+ .vidioc_g_chip_ident = mxc_isi_cap_g_chip_ident,
.vidioc_enum_framesizes = mxc_isi_cap_enum_framesizes,
.vidioc_enum_frameintervals = mxc_isi_cap_enum_frameintervals,
The preview interface still has no content。