imx8mp PCIE EP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp PCIE EP

2,357件の閲覧回数
qwerqq
Contributor I

I am currently using version 5.4.70 of imx8mp, and now I am using PCIE on two development boards. One does RC, the other does EP mode, now I can detect the device, the printing information is as follows:

root@OK8MP:~# lspci

00:00.0 PCI bridge: Synopsys, Inc. DWC_usb3 (rev 01)

01:00.0 Non-VGA unclassified device: Synopsys, Inc. DWC_usb3 (rev 01)

I now recognize the device, but I did not generate the corresponding device node in the /dev/directory because I still lack the corresponding device driver?Looking forward to your reply

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,320件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please refer this 

0 件の賞賛
返信

2,308件の閲覧回数
qwerqq
Contributor I

Following the actions in the documentation, the following error occurs:

    Image_20231127162613.png

Also, if the EP end is detected, will a node be generated under /dev/?

0 件の賞賛
返信