imx8mp EVK board reboot to bootloader while loading kernel of android-13

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mp EVK board reboot to bootloader while loading kernel of android-13

1,007 次查看
kalarav_p
Contributor II

 

 

We have imx8mp custom board and we are trying to load kernel of android-13, While loading kernel of android-13 reboot to bootloader every time. 

Below are kernel loading logs.


Starting kernel ...

[ 0.000000][ T0] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000][ T0] Linux version 6.1.25 (kalarav@falcon) (Android (10087095, +pgo, +bolt, +lto, -mlgo, based on r487747c) clang version 17.0.2 (https://android.googlesource.com/toolchain/llvm-project 3
[ 0.000000][ T0] Machine model: NXP i.MX8MPlus EVK board
[ 0.000000][ T0] Stack Depot is disabled
[ 0.000000][ T0] efi: UEFI not found.
[ 0.000000][ T0] Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
[ 0.000000][ T0] OF: reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
[ 0.000000][ T0] NUMA: No NUMA configuration found
[ 0.000000][ T0] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000][ T0] NUMA: NODE_DATA [mem 0xbfb2d980-0xbfb2ffff]
[ 0.000000][ T0] kvm [0]: Reserved 16 MiB at 0xbea00000
[ 0.000000][ T0] Zone ranges:
[ 0.000000][ T0] DMA32 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000][ T0] Normal empty
[ 0.000000][ T0] Movable zone start for each node
[ 0.000000][ T0] Early memory node ranges
[ 0.000000][ T0] node 0: [mem 0x0000000040000000-0x00000000923fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000092400000-0x00000000943fffff]
[ 0.000000][ T0] node 0: [mem 0x0000000094400000-0x00000000bfffffff]
[ 0.000000][ T0] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
[ 0.000000][ T0] cma: Reserved 800 MiB at 0x0000000060000000
[ 0.000000][ T0] psci: probing for conduit method from DT.
[ 0.000000][ T0] psci: PSCIv1.1 detected in firmware.
[ 0.000000][ T0] psci: Using standard PSCI v0.2 function IDs
[ 0.000000][ T0] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000][ T0] psci: SMC Calling Convention v1.2
[ 0.000000][ T0] Load bootconfig: 933 bytes 61 nodes
[ 0.000000][ T0] percpu: Embedded 30 pages/cpu s84712 r8192 d29976 u122880
[ 0.000000][ T0] Detected VIPT I-cache on CPU0
[ 0.000000][ T0] CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
[ 0.000000][ T0] CPU features: detected: GIC system register CPU interface
[ 0.000000][ T0] CPU features: detected: ARM erratum 845719
[ 0.000000][ T0] alternatives: applying boot alternatives
[ 0.000000][ T0] Fallback order for Node 0: 0
[ 0.000000][ T0] Built 1 zonelists, mobility grouping on. Total pages: 516096
[ 0.000000][ T0] Policy zone: DMA32
[ 0.000000][ T0] Kernel command line: console=ttynull stack_depot_disable=on cgroup_disable=pressure kasan.page_alloc.sample=10 kasan.stacktrace=off kvm-arm.mode=protected bootconfig ioremap_guard cg
[ 0.000000][ T0] cgroup: Disabling pressure control group feature
[ 0.000000][ T0] Unknown kernel command line parameters "buildvariant=eng", will be passed to user space.
[ 0.000000][ T0] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000][ T0] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000][ T0] mem auto-init: stack:all(zero), heap alloc:on, heap free:off
[ 0.000000][ T0] Memory: 1119512K/2097152K available (27328K kernel code, 3010K rwdata, 14488K rodata, 1984K init, 763K bss, 158440K reserved, 819200K cma-reserved)
[ 0.000000][ T0] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000][ T0] trace event string verifier disabled
[ 0.000000][ T0] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000][ T0] rcu: RCU event tracing is enabled.
[ 0.000000][ T0] rcu: RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
[ 0.000000][ T0] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000][ T0] Trampoline variant of Tasks RCU enabled.
[ 0.000000][ T0] Tracing variant of Tasks RCU enabled.
[ 0.000000][ T0] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000][ T0] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000][ T0] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000][ T0] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000][ T0] GICv3: 160 SPIs implemented
[ 0.000000][ T0] GICv3: 0 Extended SPIs implemented
[ 0.000000][ T0] Root IRQ handler: gic_handle_irq
[ 0.000000][ T0] GICv3: GICv3 features: 16 PPIs
[ 0.000000][ T0] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000][ T0] ITS: No ITS available, not enabling LPIs
[ 0.000000][ T0] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000][ T0] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000][ T0] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000000][ T0] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000976][ T0] kfence: initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
[ 0.001154][ T0] Console: colour dummy device 80x25
[ 0.001265][ T0] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.001275][ T0] pid_max: default: 32768 minimum: 301
[ 0.001551][ T0] LSM: Security Framework initializing
[ 0.001627][ T0] SELinux: Initializing.
[ 0.001996][ T0] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.002008][ T0] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.004154][ T1] cblist_init_generic: Setting adjustable number of callback queues.
[ 0.004165][ T1] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.004266][ T1] cblist_init_generic: Setting shift to 2 and lim to 1.
[ 0.004496][ T1] rcu: Hierarchical SRCU implementation.
[ 0.004499][ T1] rcu: Max phase no-delay instances is 1000.
[ 0.005684][ T1] dyndbg: Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build
[ 0.007431][ T1] EFI services will not be available.
[ 0.007981][ T1] smp: Bringing up secondary CPUs ...
[ 0.008574][ T0] Detected VIPT I-cache on CPU1
[ 0.008667][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.008703][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.009368][ T0] Detected VIPT I-cache on CPU2
[ 0.009445][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.009466][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.010079][ T0] Detected VIPT I-cache on CPU3
[ 0.010156][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.010177][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.010252][ T1] smp: Brought up 1 node, 4 CPUs
[ 0.010260][ T1] SMP: Total of 4 processors activated.
[ 0.010264][ T1] CPU features: detected: 32-bit EL0 Support
[ 0.010267][ T1] CPU features: detected: 32-bit EL1 Support
[ 0.010271][ T1] CPU features: detected: CRC32 instructions
[ 0.010280][ T1] CPU features: detected: Protected KVM
[ 0.010342][ T1] CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
[ 0.010347][ T1] CPU: All CPU(s) started at EL2
[ 0.010368][ T1] alternatives: applying system-wide alternatives
[ 0.015049][ T1] devtmpfs: initialized
[ 0.032718][ T1] Registered cp15_barrier emulation handler
[ 0.032733][ T1] Registered setend emulation handler
[ 0.032944][ T1] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.032967][ T1] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.065054][ T1] pinctrl core: initialized pinctrl subsystem
[ 0.069326][ T1] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.079413][ T1] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.079633][ T1] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.079744][ T1] audit: initializing netlink subsys (disabled)
[ 0.080069][ T38] audit: type=2000 audit(0.072:1): state=initialized audit_enabled=0 res=1
[ 0.080894][ T1] thermal_sys: Registered thermal governor 'step_wise'
[ 0.080899][ T1] thermal_sys: Registered thermal governor 'user_space'
[ 0.080903][ T1] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.080951][ T1] cpuidle: using governor menu
[ 0.081515][ T1] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.081622][ T1] ASID allocator initialised with 65536 entries
[ 0.083180][ T1] Serial: AMBA PL011 UART driver
[ 0.083296][ T1] imx mu driver is registered.
[ 0.083322][ T1] imx rpmsg driver is registered.
[ 0.084417][ T1] printk: console [ramoops-1] enabled
[ 0.084693][ T1] pstore: Registered ramoops as persistent store backend
[ 0.084703][ T1] ramoops: using 0x100000@0x94400000, ecc: 0
[ 0.096848][ T1] imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.108245][ T1] platform 32e60000.mipi_dsi: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/adv7535@3d
[ 0.108305][ T1] platform 32e60000.mipi_dsi: Fixed dependency cycle(s) with /soc@0/bus@32c00000/lcd-controller@32e80000
[ 0.108900][ T1] platform 32e90000.lcd-controller: Fixed dependency cycle(s) with /soc@0/bus@32c00000/ldb@32ec005c
[ 0.110503][ T1] platform 32c00000.bus:ldb@32ec005c: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/lvds-to-hdmi-bridge@4c
[ 0.113133][ T1] platform 32e40000.csi: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/os08a20_mipi@36
[ 0.113513][ T1] platform 32e50000.csi: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a40000/os08a20_mipi@36
[ 0.118253][ T1] platform 32fc6000.lcd-controller: Fixed dependency cycle(s) with /soc@0/bus@30c00000/hdmi@32fd8000
[ 0.128057][ T1] platform cbtl04gp: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 0.129211][ T1] KASLR disabled due to lack of seed
[ 0.159269][ T1] ACPI: Interpreter disabled.
[ 0.160720][ T1] iommu: Default domain type: Translated
[ 0.160740][ T1] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.161497][ T1] SCSI subsystem initialized
[ 0.161890][ T1] usbcore: registered new interface driver usbfs
[ 0.161938][ T1] usbcore: registered new interface driver hub
[ 0.161975][ T1] usbcore: registered new device driver usb
[ 0.163796][ T1] mc: Linux media interface: v0.10
[ 0.163852][ T1] videodev: Linux video capture interface: v2.00
[ 0.163961][ T1] pps_core: LinuxPPS API ver. 1 registered
[ 0.163972][ T1] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.163992][ T1] PTP clock support registered
[ 0.164276][ T1] EDAC MC: Ver: 3.0.0
[ 0.166411][ T1] FPGA manager framework
[ 0.166550][ T1] Advanced Linux Sound Architecture Driver Initialized.
[ 0.167299][ T1] Bluetooth: Core ver 2.22
[ 0.167351][ T1] NET: Registered PF_BLUETOOTH protocol family
[ 0.167360][ T1] Bluetooth: HCI device and connection manager initialized
[ 0.167374][ T1] Bluetooth: HCI socket layer initialized
[ 0.167386][ T1] Bluetooth: L2CAP socket layer initialized
[ 0.167407][ T1] Bluetooth: SCO socket layer initialized
[ 0.167770][ T1] nfc: nfc_init: NFC Core ver 0.1
[ 0.167847][ T1] NET: Registered PF_NFC protocol family
[ 0.169013][ T1] clocksource: Switched to clocksource arch_sys_counter
[ 0.169480][ T1] VFS: Disk quotas dquot_6.6.0
[ 0.169541][ T1] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.169823][ T1] pnp: PnP ACPI: disabled
[ 0.179328][ T1] NET: Registered PF_INET protocol family
[ 0.179506][ T1] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.181198][ T1] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.181316][ T1] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.181402][ T1] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.181591][ T1] TCP bind hash table entries: 16384 (order: 7, 524288 bytes, linear)
[ 0.182003][ T1] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.182141][ T1] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.182197][ T1] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.182415][ T1] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.183009][ T1] NET: Registered PF_XDP protocol family
[ 0.183026][ T1] PCI: CLS 0 bytes, default 64
[ 0.183288][ T55] Trying to unpack rootfs image as initramfs...
[ 0.193226][ T1] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.194317][ T1] kvm [1]: IPA Size Limit: 40 bits
[ 0.228362][ T1] kvm [1]: GICv3: no GICV resource entry
[ 0.228407][ T1] kvm [1]: disabling GICv2 emulation
[ 0.228432][ T1] kvm [1]: GIC system register CPU interface enabled
[ 0.228643][ T1] kvm [1]: vgic interrupt IRQ9
[ 0.229171][ T1] kvm [1]: Protected nVHE mode initialized successfully
[ 0.231218][ T1] Initialise system trusted keyrings
[ 0.231665][ T1] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.244524][ T1] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.244986][ T1] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.246134][ T1] fuse: init (API version 7.37)
[ 0.246839][ T1] 9p: Installing v9fs 9p2000 file system support
[ 0.285267][ T1] Key type asymmetric registered
[ 0.285304][ T1] Asymmetric key parser 'x509' registered
[ 0.285448][ T1] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 235)
[ 0.285681][ T1] io scheduler mq-deadline registered
[ 0.285694][ T1] io scheduler kyber registered
[ 0.285917][ T1] io scheduler bfq registered
[ 0.297584][ T1] EINJ: ACPI disabled.
[ 0.297608][ T67] acpi_thermal_pm (67) used greatest stack depth: 14224 bytes left
[ 0.315235][ T1] mxs-dma 33000000.dma-apbh: initialized
[ 0.333044][ T1] SoC: i.MX8MP revision 1.1
[ 0.334085][ T1] imx8m-blk-ctrl 32ec0000.blk-ctrl: BLK CTRL use normal mode
[ 0.335889][ T1] ------------[ cut here ]------------
[ 0.335915][ T1] WARNING: CPU: 3 PID: 1 at drivers/trusty/trusty.c:78 trusty_fast_call32+0x4c/0x6c
[ 0.335938][ T1] Modules linked in:
[ 0.335951][ T1] CPU: 3 PID: 1 Comm: swapper/0 Not tainted 6.1.25 #4
[ 0.335963][ T1] Hardware name: NXP i.MX8MPlus EVK board (DT)
[ 0.335972][ T1] pstate: a0400005 (NzCv daif +PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 0.335985][ T1] pc : trusty_fast_call32+0x4c/0x6c
[ 0.335997][ T1] lr : imx8m_blk_ctrl_probe+0x558/0x5bc
[ 0.336010][ T1] sp : ffff80000aeeb6f0
[ 0.336018][ T1] x29: ffff80000aeeb6f0 x28: 0000000000000000 x27: 0000000000000000
[ 0.336036][ T1] x26: 0000000000000000 x25: ffff00007fb7a090 x24: ffff0000069d3410
[ 0.336053][ T1] x23: ffff80000a097e48 x22: ffff000007c06680 x21: ffff0000069c9c00
[ 0.336070][ T1] x20: ffff0000069c9c10 x19: ffff000007c06640 x18: ffff80000aeb5098
[ 0.336087][ T1] x17: 00000000fbe1d510 x16: 00000000fbe1d510 x15: ffff800009a71b5c
[ 0.336103][ T1] x14: ffff80000a37ee48 x13: 0000000000000000 x12: 0000000000000008
[ 0.336120][ T1] x11: 0000000000000000 x10: 0000000000000001 x9 : e014c5086973c600
[ 0.336137][ T1] x8 : 0000000000000000 x7 : 7f7f7f7f7f7f7f7f x6 : 6d67ff7873727471
[ 0.336154][ T1] x5 : 0000000000000001 x4 : 0000000000000000 x3 : 0000000000000000
[ 0.336170][ T1] x2 : 0000000000000000 x1 : 00000000b7000000 x0 : 00000000fffffffe
[ 0.336187][ T1] Call trace:
[ 0.336196][ T1] trusty_fast_call32+0x4c/0x6c
[ 0.336208][ T1] imx8m_blk_ctrl_probe+0x558/0x5bc
[ 0.336221][ T1] platform_probe+0xcc/0xf8
[ 0.336236][ T1] really_probe+0x19c/0x390
[ 0.336249][ T1] __driver_probe_device+0xc0/0xf0
[ 0.336262][ T1] driver_probe_device+0x4c/0x228
[ 0.336274][ T1] __driver_attach+0x110/0x1e0
[ 0.336287][ T1] bus_for_each_dev+0xa0/0xf4
[ 0.336299][ T1] driver_attach+0x2c/0x40
[ 0.336311][ T1] bus_add_driver+0x118/0x208
[ 0.336322][ T1] driver_register+0x80/0x124
[ 0.336335][ T1] __platform_driver_register+0x2c/0x40
[ 0.336349][ T1] imx8m_blk_ctrl_driver_init+0x24/0x38
[ 0.336365][ T1] do_one_initcall+0xe4/0x334
[ 0.336379][ T1] do_initcall_level+0xd0/0x1ac
[ 0.336393][ T1] do_initcalls+0x5c/0xa0
[ 0.336406][ T1] do_basic_setup+0x24/0x34
[ 0.336418][ T1] kernel_init_freeable+0xf4/0x170
[ 0.336431][ T1] kernel_init+0x28/0x1b4
[ 0.336445][ T1] ret_from_fork+0x10/0x20
[ 0.336458][ T1] ---[ end trace 0000000000000000 ]---
[ 0.336472][ T1] imx8m-blk-ctrl 38330000.blk-ctl: BLK CTRL use normal mode
[ 0.340189][ T1] Bus freq driver module loaded
[ 0.350754][ T1] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 17, base_baud = 5000000) is a IMX
[ 0.351629][ T1] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 18, base_baud = 5000000) is a IMX
[ 0.352402][ T1] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 19, base_baud = 1500000) is a IMX
[ 0.423776][ T55] Freeing initrd memory: 18976K
[ 0.431122][ T1] printk: console [ttymxc1] enabled
[ 0.437355][ T66] imx-sdma 30bd0000.dma-controller: firmware found.
[ 1.973326][ T1] printk: console [ttynull0] enabled
[ 1.973503][ T66] imx-sdma 30bd0000.dma-controller: loaded firmware 4.6
[ 2.002463][ T1] brd: module loaded
[ 2.018635][ T1] loop: module loaded
[ 2.023042][ T1] zram: Added device: zram0
[ 2.030642][ T1] megasas: 07.719.03.00-rc1
[ 2.042664][ T1] spi-nor spi0.0: unrecognized JEDEC id bytes: 00 00 00 00 00 00
[ 2.052179][ T1] wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information.
[ 2.060741][ T1] wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld <Jason@zx2c4.com>. All Rights Reserved.
[ 2.071808][ T1] MACsec IEEE 802.1AE
[ 2.078798][ T1] tun: Universal TUN/TAP device driver, 1.6
[ 2.084815][ T1] vcan: Virtual CAN interface driver
[ 2.089981][ T1] slcan: serial line CAN interface driver
[ 2.095571][ T1] CAN device driver interface
[ 2.101440][ T1] thunder_xcv, ver 1.0
[ 2.105422][ T1] thunder_bgx, ver 1.0
[ 2.109476][ T1] nicpf, ver 1.0
[ 2.116372][ T1] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 2.124327][ T1] hns3: Copyright (c) 2017 Huawei Corporation.
[ 2.130411][ T1] hclge is initializing
[ 2.134454][ T1] e1000: Intel(R) PRO/1000 Network Driver
[ 2.140041][ T1] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 2.146542][ T1] e1000e: Intel(R) PRO/1000 Network Driver
[ 2.152216][ T1] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 2.158906][ T1] igb: Intel(R) Gigabit Ethernet Network Driver
[ 2.165015][ T1] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 2.171340][ T1] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 2.178316][ T1] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 2.185252][ T1] sky2: driver version 1.30
[ 2.191341][ T1] PPP generic driver version 2.4.2
[ 2.196513][ T1] PPP BSD Compression module registered
[ 2.201940][ T1] PPP Deflate Compression module registered
[ 2.207722][ T1] PPP MPPE Compression module registered
[ 2.213222][ T1] NET: Registered PF_PPPOX protocol family
[ 2.218898][ T1] PPTP driver version 0.8.5
[ 2.223478][ T1] usbcore: registered new interface driver rtl8150
[ 2.229887][ T1] usbcore: registered new interface driver r8152
[ 2.236137][ T1] usbcore: registered new interface driver cdc_ether
[ 2.242721][ T1] usbcore: registered new interface driver cdc_eem
[ 2.249170][ T1] usbcore: registered new interface driver cdc_ncm
[ 2.255579][ T1] usbcore: registered new interface driver aqc111
[ 2.261917][ T1] usbcore: registered new interface driver r8153_ecm
[ 2.268800][ T1] VFIO - User Level meta-driver version: 0.3
[ 2.277252][ T1] platform 38100000.usb: Fixed dependency cycle(s) with /soc@0/bus@30800000/i2c@30a30000/tcpc@50
[ 2.294608][ T1] usbcore: registered new interface driver cdc_acm
[ 2.301011][ T1] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.309967][ T1] usbcore: registered new interface driver uas
[ 2.316045][ T1] usbcore: registered new interface driver usb-storage
[ 2.322854][ T1] usbcore: registered new interface driver usbserial_generic
[ 2.330114][ T1] usbserial: USB Serial support registered for generic
[ 2.336880][ T1] usbcore: registered new interface driver ftdi_sio
[ 2.343357][ T1] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 2.351414][ T1] usbcore: registered new interface driver usb_serial_simple
[ 2.358670][ T1] usbserial: USB Serial support registered for carelink
[ 2.365489][ T1] usbserial: USB Serial support registered for zio
[ 2.371877][ T1] usbserial: USB Serial support registered for funsoft
[ 2.378619][ T1] usbserial: USB Serial support registered for flashloader
[ 2.385702][ T1] usbserial: USB Serial support registered for google
[ 2.392363][ T1] usbserial: USB Serial support registered for libtransistor
[ 2.399634][ T1] usbserial: USB Serial support registered for vivopay
[ 2.406369][ T1] usbserial: USB Serial support registered for moto_modem
[ 2.413363][ T1] usbserial: USB Serial support registered for motorola_tetra
[ 2.420703][ T1] usbserial: USB Serial support registered for nokia
[ 2.427264][ T1] usbserial: USB Serial support registered for novatel_gps
[ 2.434344][ T1] usbserial: USB Serial support registered for hp4x
[ 2.440820][ T1] usbserial: USB Serial support registered for suunto
[ 2.447469][ T1] usbserial: USB Serial support registered for siemens_mpi
[ 2.454572][ T1] usbcore: registered new interface driver usb_ehset_test
[ 2.465831][ T1] usbcore: registered new interface driver xpad
[ 2.473154][ T1] i2c_dev: i2c /dev entries driver
[ 2.480552][ T1] gspca_main: v2.14.0 registered
[ 2.485427][ T1] usbcore: registered new interface driver uvcvideo
[ 2.493161][ T1] __power_supply_register: Expected proper parent device for 'battery'
[ 2.501847][ T1] __power_supply_register: Expected proper parent device for 'usb'
[ 2.512214][ T1] trusty trusty: failed to get version: -1
[ 2.517939][ T1] trusty trusty: selected api version: 0 (requested 5)
[ 2.525133][ T1] trusty trusty: trusty-share not supported on secure side, error=-1
[ 2.533108][ T1] trusty trusty: Trusty-Sched_Share API not available.
[ 2.542302][ T80] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
[ 2.542330][ T81] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
[ 2.550139][ T82] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
[ 2.550161][ T83] trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
[ 2.550569][ T1] trusty trusty: trusty-log not supported on secure side.
[ 2.551068][ T1] trusty-virtio trusty:trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1)
[ 2.551076][ T1] trusty-virtio trusty:trusty-virtio: failed (-19) to load device descr
[ 2.551110][ T1] trusty-virtio trusty:trusty-virtio: Failed to add virtio devices
[ 2.553469][ T1] device-mapper: uevent: version 1.0.3
[ 2.553849][ T1] device-mapper: ioctl: 4.47.0-ioctl (2022-07-28) initialised: dm-devel@redhat.com
[ 2.554445][ T1] Bluetooth: HCI UART driver ver 2.3
[ 2.554453][ T1] Bluetooth: HCI UART protocol H4 registered
[ 2.554457][ T1] Bluetooth: HCI UART protocol BCSP registered
[ 2.554485][ T1] Bluetooth: HCI UART protocol LL registered
[ 2.554489][ T1] Bluetooth: HCI UART protocol ATH3K registered
[ 2.554512][ T1] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.554808][ T1] Bluetooth: HCI UART protocol Broadcom registered
[ 2.554832][ T1] Bluetooth: HCI UART protocol QCA registered
[ 2.555164][ T1] EDAC MC: ECC not enabled
[ 2.565921][ T1] sdhci: Secure Digital Host Controller Interface driver
[ 2.680633][ T1] sdhci: Copyright(c) Pierre Ossman
[ 2.687123][ T1] Synopsys Designware Multimedia Card Interface Driver
[ 2.695007][ T1] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.707032][ T1] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.714915][ T1] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 2.722153][ T1] hid: raw HID events driver (C) Jiri Kosina
[ 2.730303][ T1] usbcore: registered new interface driver usbhid
[ 2.736605][ T1] usbhid: USB HID core driver
[ 2.737022][ T55] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 2.742783][ T1] mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using dummy regulator
[ 2.758632][ T1] : mipi_csis_imx8mp_phy_reset, No remote pad found!
[ 2.765254][ T1] mxc-mipi-csi2-sam 32e40000.csi: lanes: 4, hs_settle: 16, clk_settle: 2, wclk: 1, freq: 266000000
[ 2.776067][ T1] mxc-mipi-csi2-sam 32e50000.csi: supply mipi-phy not found, using dummy regulator
[ 2.785695][ T1] : mipi_csis_imx8mp_phy_reset, No remote pad found!
[ 2.792296][ T1] mxc-mipi-csi2-sam 32e50000.csi: lanes: 4, hs_settle: 16, clk_settle: 2, wclk: 1, freq: 266000000
[ 2.805648][ T1] ashmem: initialized
[ 2.816224][ T1] cs_system_cfg: CoreSight Configuration manager initialised
[ 2.826482][ T1] gnss: GNSS driver registered with major 494
[ 2.835778][ T1] Galcore version 6.4.11.p1.658245
[ 2.860636][ T1] [drm] Initialized vivante 1.0.0 20170808 for 40000000.mix_gpu_ml on minor 0
[ 2.870758][ T1] vpu driver probe fail! nr=0xb7000000 ret=-1. Use normal mode.
[ 2.879285][ T1] hantrodec 0 : module inserted. Major = 493
[ 2.885869][ T1] vpu driver probe fail! nr=0xb7000000 ret=-1. Use normal mode.
[ 2.893600][ T1] hantrodec 1 : module inserted. Major = 493
[ 2.900668][ T1] mxc_hantro_vc8000e 38320000.vpu_vc8000e: hantro_enc: get trusty_dev node, use Trusty mode.
[ 2.910705][ T1] hantro_enc driver probe fail! nr=0xb8000000 ret=-1. Use normal mode.
[ 2.919423][ T1] hantroenc: HW at base <0000000038320000> with ID <0x80006200>
[ 2.927060][ T1] hx280enc: module inserted. Major <492>
[ 2.935792][ T1] usbcore: registered new interface driver snd-usb-audio
[ 2.951498][ T1] imx-hdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 2.959246][ T1] NET: Registered PF_LLC protocol family
[ 2.964811][ T1] GACT probability NOT on
[ 2.969023][ T1] Mirror/redirect action on
[ 2.973413][ T1] netem: version 1.3
[ 2.977295][ T1] u32 classifier
[ 2.980702][ T1] input device check on
[ 2.985075][ T1] Actions configured
[ 2.990358][ T1] xt_time: kernel timezone is -0000
[ 2.995543][ T1] ipip: IPv4 and MPLS over IPv4 tunneling driver
[ 3.002199][ T1] gre: GRE over IPv4 demultiplexor driver
[ 3.007791][ T1] ip_gre: GRE over IPv4 tunneling driver
[ 3.014612][ T1] IPv4 over IPsec tunneling driver
[ 3.021169][ T1] Initializing XFRM netlink socket
[ 3.026189][ T1] IPsec XFRM device driver
[ 3.031187][ T1] NET: Registered PF_INET6 protocol family
[ 3.040791][ T1] Segment Routing with IPv6
[ 3.045232][ T1] In-situ OAM (IOAM) with IPv6
[ 3.050061][ T1] mip6: Mobile IPv6
[ 3.055003][ T1] ip6_gre: GRE over IPv6 tunneling driver
[ 3.061130][ T1] NET: Registered PF_PACKET protocol family
[ 3.066902][ T1] NET: Registered PF_KEY protocol family
[ 3.072521][ T1] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 3.086191][ T1] can: controller area network core
[ 3.091384][ T1] NET: Registered PF_CAN protocol family
[ 3.096890][ T1] can: raw protocol
[ 3.100568][ T1] can: broadcast manager protocol
[ 3.105472][ T1] can: netlink gateway - max_hops=1
[ 3.111721][ T1] Bluetooth: RFCOMM TTY layer initialized
[ 3.117333][ T1] Bluetooth: RFCOMM socket layer initialized
[ 3.123208][ T1] Bluetooth: RFCOMM ver 1.11
[ 3.127677][ T1] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 3.133699][ T1] Bluetooth: BNEP filters: protocol multicast
[ 3.139638][ T1] Bluetooth: BNEP socket layer initialized
[ 3.145314][ T1] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 3.151945][ T1] Bluetooth: HIDP socket layer initialized
[ 3.158604][ T1] l2tp_core: L2TP core driver, V2.0
[ 3.163692][ T1] l2tp_ppp: PPPoL2TP kernel driver, V2.0
[ 3.169194][ T1] 8021q: 802.1Q VLAN Support v1.8
[ 3.174147][ T1] tipc: Activated (version 2.0.0)
[ 3.179223][ T1] NET: Registered PF_TIPC protocol family
[ 3.184912][ T1] tipc: Started in single node mode
[ 3.190109][ T1] 9pnet: Installing 9P2000 support
[ 3.195398][ T1] NET: Registered PF_IEEE802154 protocol family
[ 3.202527][ T1] NET: Registered PF_VSOCK protocol family
[ 3.211157][ T1] imx-lcdifv3 32e80000.lcd-controller: lcdif: failed to get response of echo. Use normal mode.
[ 3.225536][ T1] snvs_pwrkey 30370000.snvs:snvs-powerkey: snvs pwkey: trusty driver failed to probe! nr=0xb5000000 error=-1. Use normal mode.
[ 3.239037][ T1] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 3.254196][ T1] snvs_rtc 30370000.snvs:snvs-rtc-lp: snvs rtc: trusty snvs driver failed to probe! nr=0xb5000000 ret=-1. Use normal mode.
[ 3.267599][ T1] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 3.274519][ T1] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:24 UTC (24)
[ 3.286798][ T1] registered taskstats version 1
[ 3.291681][ T1] Loading compiled-in X.509 certificates
[ 3.300538][ T1] Loaded X.509 cert 'Build time autogenerated kernel key: a69189a425a3d7ad300ae73888c59e771653092e'
[ 3.311268][ T1] page_owner is disabled
[ 3.315637][ T1] Key type .fscrypt registered
[ 3.320276][ T1] Key type fscrypt-provisioning registered
[ 3.326948][ T1] pstore: Using crash dump compression: deflate
[ 3.428206][ T55] nxp-pca9450 0-0025: pca9450bc probed.
[ 3.433766][ T55] i2c i2c-0: IMX I2C adapter registered
[ 3.440737][ T55] adv7511 1-003d: supply avdd not found, using dummy regulator
[ 3.448323][ T55] adv7511 1-003d: supply dvdd not found, using dummy regulator
[ 3.455824][ T55] adv7511 1-003d: supply pvdd not found, using dummy regulator
[ 3.463280][ T55] adv7511 1-003d: supply a2vdd not found, using dummy regulator
[ 3.470824][ T55] adv7511 1-003d: supply v3p3 not found, using dummy regulator
[ 3.478297][ T55] adv7511 1-003d: supply v1p2 not found, using dummy regulator
[ 3.545290][ T55] i2c i2c-1: IMX I2C adapter registered
[ 3.552513][ T55] pca953x 2-0020: supply vcc not found, using dummy regulator
[ 3.559982][ T55] pca953x 2-0020: using no AI
[ 3.565512][ T55] pca953x 2-0020: failed writing register
[ 3.572065][ T55] i2c i2c-2: IMX I2C adapter registered
[ 3.578832][ T55] imx8mp-ldb 32c00000.bus:ldb@32ec005c: Failed to create device link (0x180) with 32c00000.bus:phy@32ec0128
[ 3.590647][ T55] imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator
[ 3.600123][ T55] imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator
[ 3.612469][ T55] pwm-backlight lvds_backlight: supply power not found, using dummy regulator
[ 3.613702][ T53] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 3.629183][ T53] imx6q-pcie 33800000.pcie: IO 0x001ff80000..0x001ff8ffff -> 0x0000000000
[ 3.638127][ T53] imx6q-pcie 33800000.pcie: MEM 0x0018000000..0x001fefffff -> 0x0018000000
[ 3.641806][ T100] imx-sdma 30e10000.dma-controller: firmware found.
[ 3.648042][ T55] dwhdmi-imx 32fd8000.hdmi: Detected HDMI TX controller v2.13a with HDCP (samsung_dw_hdmi_phy2)
[ 3.666015][ T55] dwhdmi-imx 32fd8000.hdmi: registered DesignWare HDMI I2C bus driver
[ 3.668389][ T53] phy phy-32f00000.pcie-phy.4: phy poweron failed --> -110
[ 3.680799][ T55] pps pps0: new PPS source ptp0
[ 3.681104][ T53] imx6q-pcie 33800000.pcie: waiting for PHY ready timeout!
[ 3.681190][ T53] imx6q-pcie: probe of 33800000.pcie failed with error -110
[ 3.898477][ T55] fec 30be0000.ethernet eth0: registered PHC device 0
[ 3.906338][ T55] imx-dwmac 30bf0000.ethernet: IRQ eth_lpi not found
[ 3.914031][ T55] imx-dwmac 30bf0000.ethernet: User ID: 0x10, Synopsys ID: 0x51
[ 3.921552][ T55] imx-dwmac 30bf0000.ethernet: DWMAC4/5
[ 3.927057][ T55] imx-dwmac 30bf0000.ethernet: DMA HW capability register supported
[ 3.934908][ T55] imx-dwmac 30bf0000.ethernet: RX Checksum Offload Engine supported
[ 3.942759][ T55] imx-dwmac 30bf0000.ethernet: Wake-Up On Lan supported
[ 3.949650][ T55] imx-dwmac 30bf0000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 3.958024][ T55] imx-dwmac 30bf0000.ethernet: Enabled L3L4 Flow TC (entries=8)
[ 3.965526][ T55] imx-dwmac 30bf0000.ethernet: Enabled RFS Flow TC (entries=10)
[ 3.973052][ T55] imx-dwmac 30bf0000.ethernet: Enabling HW TC (entries=256, max_off=256)
[ 3.981338][ T55] imx-dwmac 30bf0000.ethernet: Using 34/40 bits DMA host/device width
[ 4.181749][ T55] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 4.188016][ T55] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 4.196730][ T55] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220fe6d hci version 0x110 quirks 0x0000002001010010
[ 4.206892][ T55] xhci-hcd xhci-hcd.1.auto: irq 223, io mem 0x38200000
[ 4.213800][ T55] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 4.220006][ T55] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 4.228379][ T55] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 4.235781][ T55] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 6.01
[ 4.244761][ T55] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.252698][ T55] usb usb1: Product: xHCI Host Controller
[ 4.258288][ T55] usb usb1: Manufacturer: Linux 6.1.25 xhci-hcd
[ 4.264397][ T55] usb usb1: SerialNumber: xhci-hcd.1.auto
[ 4.271210][ T55] hub 1-0:1.0: USB hub found
[ 4.275709][ T55] hub 1-0:1.0: 1 port detected
[ 4.280745][ T55] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 4.289665][ T55] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 6.01
[ 4.298647][ T55] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.306596][ T55] usb usb2: Product: xHCI Host Controller
[ 4.312188][ T55] usb usb2: Manufacturer: Linux 6.1.25 xhci-hcd
[ 4.318302][ T55] usb usb2: SerialNumber: xhci-hcd.1.auto
[ 4.325042][ T55] hub 2-0:1.0: USB hub found
[ 4.329552][ T55] hub 2-0:1.0: 1 port detected
[ 4.335832][ T55] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 7 mkt segment 2 supported-hw 0x80 0x4
[ 4.349296][ T8] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 4.372033][ T55] input: audio-hdmi HDMI Jack as /devices/platform/sound-hdmi/sound/card0/input1
[ 4.390844][ T8] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 4.393575][ T55] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 4.407297][ T55] imx-drm display-subsystem: bound imx-lcdifv3-crtc.1 (ops lcdifv3_crtc_ops)
[ 4.415985][ T55] imx-drm display-subsystem: bound imx-lcdifv3-crtc.2 (ops lcdifv3_crtc_ops)
[ 4.424811][ T55] imx_sec_dsim_drv 32e60000.mipi_dsi: version number is 0x1060200
[ 4.432535][ T55] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e60000 to encoder DSI-40: -19
[ 4.444829][ T55] imx_sec_dsim_drv 32e60000.mipi_dsi: Failed to attach bridge: 32e60000.mipi_dsi
[ 4.453817][ T55] imx_sec_dsim_drv 32e60000.mipi_dsi: failed to bind sec dsim bridge: -19
[ 4.462184][ T55] imx-drm display-subsystem: bound 32e60000.mipi_dsi (ops imx_sec_dsim_ops)
[ 4.470816][ T55] imx-drm display-subsystem: bound 32c00000.bus:ldb@32ec005c (ops imx8mp_ldb_ops)
[ 4.479926][ T55] imx-drm display-subsystem: bound 32fd8000.hdmi (ops dw_hdmi_imx_ops)
[ 4.489076][ T55] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[ 4.497677][ T55] imx-drm display-subsystem: [drm] Cannot find any crtc or sizes
[ 4.507022][ T55] wm8960 2-001a: Failed to issue reset
[ 4.516277][ T55] rpmsg-codec-wm8960 2-001a: Failed to issue reset
[ 4.525841][ T55] debugfs: File 'Playback' in directory 'dapm' already present!
[ 4.533384][ T55] debugfs: File 'Capture' in directory 'dapm' already present!
[ 4.545039][ T71] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 4.548084][ T1] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 4.563121][ T1] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 4.570503][ T100] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 4.578743][ T1] ALSA device list:
[ 4.579833][ T100] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 4.583538][ T1] #0: audio-hdmi
[ 4.595560][ T1] #1: micfil-audio
[ 4.599340][ T1] #2: imx-audio-xcvr
[ 4.603299][ T1] #3: bt-sco-audio
[ 4.607994][ T1] Freeing unused kernel memory: 1984K
[ 4.613455][ T1] Run /init as init process
[ 4.623352][ T24] mmc1: host does not support reading read-only switch, assuming write-enable
[ 4.645494][ T1] init: init first stage started!
[ 4.652097][ T1] init: Loading module /lib/modules/imx_dsp_rproc.ko with args ''
[ 4.660093][ T1] imx_dsp_rproc: module verification failed: signature and/or required key missing - tainting kernel
[ 4.673944][ T1] remoteproc remoteproc0: imx-dsp-rproc is available
[ 4.680930][ T1] init: Loaded kernel module /lib/modules/imx_dsp_rproc.ko
[ 4.688189][ T1] init: Loading module /lib/modules/goodix_ts.ko with args ''
[ 4.697162][ T1] init: Loaded kernel module /lib/modules/goodix_ts.ko
[ 4.704041][ T1] init: Loading module /lib/modules/synaptics_dsx_i2c.ko with args ''
[ 4.705208][ T24] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 4.720145][ T1] init: Loaded kernel module /lib/modules/synaptics_dsx_i2c.ko
[ 4.720824][ T24] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 4.727801][ T1] init: Loading module /lib/modules/basler-camera-driver-vvcam.ko with args ''
[ 4.741799][ T1] basler_camera_driver_vvcam: loading out-of-tree module taints kernel.
[ 4.751583][ T1] init: Loaded kernel module /lib/modules/basler-camera-driver-vvcam.ko
[ 4.760078][ T1] init: Loading module /lib/modules/vvcam-dwe.ko with args ''
[ 4.769094][ T1] enter viv_dwe_init_module
[ 4.773813][ T71] usb 1-1: New USB device found, idVendor=0bda, idProduct=5411, bcdDevice= 1.04
[ 4.774139][ T1] enter dwe_hw_probe
[ 4.782715][ T71] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.782721][ T71] usb 1-1: Product: 4-Port USB 2.0 Hub
[ 4.787186][ T1] vvcam dewarp driver probed
[ 4.794433][ T71] usb 1-1: Manufacturer: Generic
[ 4.800312][ T1] init: Loaded kernel module /lib/modules/vvcam-dwe.ko
[ 4.815905][ T1] init: Loading module /lib/modules/vvcam-video.ko with args ''
[ 4.824552][ T24] mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16
[ 4.832559][ T1] enter viv_video_init_module
[ 4.840881][ T1] init: Loaded kernel module /lib/modules/vvcam-video.ko
[ 4.848050][ T1] init: Loading module /lib/modules/vvcam-isp.ko with args ''
[ 4.848160][ T71] hub 1-1:1.0: USB hub found
[ 4.860444][ T71] hub 1-1:1.0: 4 ports detected
[ 4.860610][ T1] enter viv_isp_init_module
[ 4.869967][ T1] enter isp_hw_probe
[ 4.875072][ T1] vvcam isp driver registered
[ 4.879816][ T1] enter isp_hw_probe
[ 4.883893][ T96] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd
[ 4.885382][ T1] vvcam isp driver registered
[ 4.896158][ T1] init: Loaded kernel module /lib/modules/vvcam-isp.ko
[ 4.903125][ T1] init: Loading module /lib/modules/imx8-media-dev.ko with args ''
[ 4.910974][ T1] imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned.
[ 4.923435][ T96] usb 2-1: New USB device found, idVendor=0bda, idProduct=0411, bcdDevice= 1.04
[ 4.924615][ T1] init: Loaded kernel module /lib/modules/imx8-media-dev.ko
[ 4.932338][ T96] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.932345][ T96] usb 2-1: Product: 4-Port USB 3.0 Hub
[ 4.932350][ T96] usb 2-1: Manufacturer: Generic
[ 4.957918][ T1] init: Loaded 8 kernel modules took 306 ms
[ 4.960459][ T96] hub 2-1:1.0: USB hub found
[ 4.963806][ T1] init: /first_stage_ramdisk/system/bin/snapuserd already exists and it can be executed
[ 4.969550][ T96] hub 2-1:1.0: 4 ports detected
[ 4.978130][ T1] init: Switching root to '/first_stage_ramdisk'
[ 4.989538][ T1] init: [libfs_mgr]ReadFstabFromDt(): failed to read fstab from dt
[ 5.000358][ T1] init: Using Android DT directory /proc/device-tree/firmware/android/
[ 5.152548][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found in /sys, waiting for their uevent(s): boot_a, dtbo_a, init_boot_a, metadataa
[ 15.074759][ T24] platform sound-wm8960: deferred probe pending
[ 15.182612][ T1] init: Wait for partitions returned after 10010ms
[ 15.189092][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout: boot_a, dtbo_a, init_boot_a, metadata, super, vbmetaa
[ 15.207536][ T1] init: Failed to mount required partitions early ...
[ 15.215924][ T1] init: InitFatalReboot: signal 6
[ 15.226800][ T1] init: #00 pc 000000000012f1fc /system/bin/init
[ 15.233195][ T1] init: #01 pc 00000000000c1b90 /system/bin/init
[ 15.239502][ T1] init: #02 pc 0000000000017560 /system/lib64/libbase.so (android::base::SetAborter(std::__1::function<void (char const*)>&&)::$_3::__invoke(char const*)+80)
[ 15.255343][ T1] init: #03 pc 0000000000016a84 /system/lib64/libbase.so (android::base::LogMessage::~LogMessage()+356)
[ 15.266412][ T1] init: #04 pc 00000000000ed424 /system/bin/init
[ 15.272718][ T1] init: #05 pc 00000000000ae110 /system/bin/init
[ 15.279022][ T1] init: #06 pc 000000000004b730 /system/lib64/libc.so (__libc_init+96)
[ 15.287247][ T1] init: Reboot ending, jumping to kernel
[ 15.292868][ T100] cfg80211: failed to load regulatory.db
[ 15.298395][ T1] kvm: exiting hardware virtualization
[ 15.324967][ T1] reboot: Restarting system with command 'bootloader'



0 项奖励
回复
1 回复

977 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

From the logs, there seems to be some issues with the images flashed, please double check that those were built/flashed correctly.

[ 13.491510][ T1] init: bool android::init::BlockDevInitializer::InitDevices(std::set<std::string>): partition(s) not found after polling timeout: boot_a, dtbo_a, init_boot_a, metadata, super, vbmetaa

Saludos,
Aldo.

0 项奖励
回复