Hi :
When we testing L5.4.70-2.3.0_images_MX8MMEVK ,and found that it could not burn to imx8mm evk board。
image:L5.4.70-2.3.0_images_MX8MMEVK.zip
EVK board:
cpu board:"SCH47712 REV A1 " "700-47712 REV X2" "8MMINILPD4-CPU2"
base board:“TDA6971" "8MMINI-BB" "SCH-31407 REV C2"
uuu release 1:uuu 1.2.91 2:uuu 1.4.95
(it's no problem when burn in android11)
LOG(uuu 1.2.91 ):
U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 04 2020 - 00:28:49 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Downloading file of size 2097152 to 0x40400000... done
Downloading file of size 1069344 to 0x00200000... "Error" handler, esr 0xbf000002
elr: 00000000007e697c lr : 00000000007ee49c
x 0: 0000000000200000 x 1: 0000000042201341
x 2: 0000000000000400 x 3: 0000000000000001
x 4: 0000000000200000 x 5: 0000000000000000
x 6: 0000000000000000 x 7: 0000000000004000
x 8: 0000000042200450 x 9: 0000000000000002
x10: 00000000422004d0 x11: 0000000000000001
x12: 0000000000000000 x13: 0000000000000000
x14: 000000000090e558 x15: 0000000000013da4
x16: 00000000007ea6e4 x17: 0000000000000005
x18: 000000000091de80 x19: 00000000422005c0
x20: 0000000000000400 x21: 00000000007f8338
x22: 00000000422008c0 x23: 0000000042200350
x24: 0000000042201340 x25: 0000000042200398
x26: 0000000042200040 x27: 00000000007f83d8
x28: 0000000000000440 x29: 000000000091dc00
Code: f2400863 54000120 aa0003e4 d2800003 (eb03005f)
Resetting CPU ...
resetting ...
log(uuu 1.4.95):
U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 04 2020 - 00:28:49 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Are you following the steps in the user's guide to program the image?
You may try the latest version from here
HI Jimmychan:
Thanks for reply.
I did following the step in the user's guide. And actually, I'm success on download Android11.
I will try the newest version.
But version L5.4.70 should be ok too, have you try verion L5.4.70 ? I worried that it's the problem of my pc or driver or something else.
Best Regards.
HI Jimmychan:
I 100% understand that the image has been tested , and it' no problem.
But as I know , there is several version of EVK board, and with difference PMIC or some other things.
So, I worried about my EVK board is not compatible with this(L5.4.70) version. And if it's not compatible, I want to know which part will effect the download.