Excuse me, have you tested keystroke wakeup on the 5.1 kernel again?I am currently using the gpio_keys.c driver which won't wake up the device, but it will work on the 4.1 kernel.Specific kernel version:Linux imx8mmevk 5.10.52-1.0,The following is the configuration of my device tree
Hi @yzg,
Please try testing the GPIO wakeup with the latest kernel available!
Thanks & Regards,
Dhruvit.
I can confirm that my gpio is fine, I have tested the wake up function in 4.1 kernel and it works perfectly
Hi
Thank you for your reply. At present, my kernel version is Linux imx8mmevk 5.10.52-1.0. Is there any patch available?
Hi @yzg,
No currently, there are no patches available for Linux 5.10.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Best regards,
Dhruvit.