Imx8mm evk android hdmi shows some small white horizontal lines in a solid background. For example, you can open the clock application, then slide the mouse to see some small white lines.
However, in Linux I repeatedly tested the above problems, I compared the mipi2hdmi driver, this part is consistent, the difference is that the display part of the android added the fence synchronization mechanism, I do not know whether this is caused by the difference Phenomenon, can you help me?
Hello
I suggest upgrading to the newest Android version Android P9.0.2.3.0. I have tested with that version and I could not find any problem.
Best regards,
Diego.
Hi Diego,
Thanks for your suggestion. I will try 2.3.0 later.
On the other hand, I checked the release notes in 2.3.0. It says that the release quality for imx8m mini evk is "Post-GA".
May I know what the different between "GA" and "Post-GA"?
Thank you
BR
Brian
Hello,
That normally happens because of a malfunction of the HDMI cable. Have you tried testing with another HDMI cable?
Best regards,
Diego.
Hi,
thanks for the reply, I don't think this is the problem caused by the HDMI cable, because I use the same imx8mm evk hardware, there is no problem using the linux image. Moreover, this HDMI cable has been used for a long time and is normal on other platforms.
Do you have imx8mm evk hardware on hand? If so, please help me test, I am using the image in android_p9.0.0_2.0.0-ga_image_8mmevk
thanks.
Hello
I apologize for the delay,
Do you have any image with the problem?
Furthermore, the output log could help me to find where is the problem.
Best regards,
Diego