I am trying to configure ADC2 channels 6 and 7 on a custom imx6 ul board.
Given below is updated imx6ul.dtsi section for adc:
adc2: adc@0219c000 {
compatible = "fsl,imx6ul-adc", "fsl,vf610-adc";
reg = <0x0219c000 0x4000>;
interrupts = <GIC_SPI 101 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_ADC2>;
num-channels = <2>;
clock-names = "adc";
status = "disabled";
};
Given below are dts updates:
pinctrl_adc2: adc2grp {
fsl,pins = <
MX6UL_PAD_GPIO1_IO06__GPIO1_IO06 0xb0
MX6UL_PAD_GPIO1_IO07__GPIO1_IO07 0xb0
>;
};&adc2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_adc2>;
interrupts = <GIC_SPI 101 IRQ_TYPE_LEVEL_HIGH>;
vref-supply = <®_vref_3v3>;
num-channels = <2>;
status = "okay";
};
Rearranged the channel sequence in file as given below:
static const struct iio_chan_spec vf610_adc_iio_channels[] = {
+ VF610_ADC_CHAN(6, IIO_VOLTAGE),
+ VF610_ADC_CHAN(7, IIO_VOLTAGE),
VF610_ADC_CHAN(0, IIO_VOLTAGE),
VF610_ADC_CHAN(1, IIO_VOLTAGE),
VF610_ADC_CHAN(2, IIO_VOLTAGE),
VF610_ADC_CHAN(3, IIO_VOLTAGE),
VF610_ADC_CHAN(4, IIO_VOLTAGE),
VF610_ADC_CHAN(5, IIO_VOLTAGE),
- VF610_ADC_CHAN(6, IIO_VOLTAGE),
- VF610_ADC_CHAN(7, IIO_VOLTAGE),
VF610_ADC_CHAN(8, IIO_VOLTAGE),
VF610_ADC_CHAN(9, IIO_VOLTAGE),
VF610_ADC_CHAN(10, IIO_VOLTAGE),
I am getting following message in kernel boot log:
vf610-adc 219c000.adc: Timeout for adc calibration
in_voltage6_raw and in_voltage7_raw are listed under /sys/bus/iio/devices/iio:device0
When I try to read value from ADC2 channel 6 and 7, system hangs for sometime and then kernel panic.
root@imx6ulboard:/sys/bus/iio/devices/iio:device0# cat in_voltage7_raw
INFO: rcu_preempt self-detected stall on CPU
0: (2100 ticks this GP) idle=68d/140000000000002/0 softirq=4518/4518 fqs=0
(t=2100 jiffies g=1106 c=1105 q=6)
rcu_preempt kthread starved for 2100 jiffies!
Task dump for CPU 0:
cat R running 0 352 245 0x00000002
[<80015d78>] (unwind_backtrace) from [<8001271c>] (show_stack+0x10/0x14)
[<8001271c>] (show_stack) from [<8007617c>] (rcu_dump_cpu_stacks+0x94/0xd4)
[<8007617c>] (rcu_dump_cpu_stacks) from [<80079c34>] (rcu_check_callbacks+0x4fc/0x8ec)
[<80079c34>] (rcu_check_callbacks) from [<8007c2e8>] (update_process_times+0x38/0x64)
[<8007c2e8>] (update_process_times) from [<8008c598>] (tick_sched_timer+0x54/0x98)
[<8008c598>] (tick_sched_timer) from [<8007cf8c>] (__run_hrtimer+0x44/0xd4)
[<8007cf8c>] (__run_hrtimer) from [<8007d384>] (hrtimer_interrupt+0x12c/0x310)
[<8007d384>] (hrtimer_interrupt) from [<8002072c>] (mxc_timer_interrupt+0x2c/0x34)
[<8002072c>] (mxc_timer_interrupt) from [<8006de54>] (handle_irq_event_percpu+0x78/0x134)
[<8006de54>] (handle_irq_event_percpu) from [<8006df4c>] (handle_irq_event+0x3c/0x5c)
[<8006df4c>] (handle_irq_event) from [<80070c08>] (handle_fasteoi_irq+0xe0/0x198)
[<80070c08>] (handle_fasteoi_irq) from [<8006d4f4>] (generic_handle_irq+0x2c/0x3c)
[<8006d4f4>] (generic_handle_irq) from [<8006d7ac>] (__handle_domain_irq+0x7c/0xec)
[<8006d7ac>] (__handle_domain_irq) from [<8000944c>] (gic_handle_irq+0x24/0x5c)
[<8000944c>] (gic_handle_irq) from [<80013200>] (__irq_svc+0x40/0x74)
Exception stack(0x88823ce8 to 0x88823d30)
3ce0: 00000000 809cd9fc 80bc9040 00000000 00000202 00000000
3d00: 00000010 88822000 00000001 80b5e080 88006000 00000001 0000002a 88823d30
3d20: 80038988 80038998 20070113 ffffffff
[<80013200>] (__irq_svc) from [<80038998>] (__do_softirq+0xa4/0x238)
[<80038998>] (__do_softirq) from [<80038df4>] (irq_exit+0xc0/0xfc)
[<80038df4>] (irq_exit) from [<8006d7b0>] (__handle_domain_irq+0x80/0xec)
[<8006d7b0>] (__handle_domain_irq) from [<8000944c>] (gic_handle_irq+0x24/0x5c)
[<8000944c>] (gic_handle_irq) from [<80013200>] (__irq_svc+0x40/0x74)
Exception stack(0x88823db8 to 0x88823e00)
3da0: 883ad2c8 0000000a
3dc0: 00000001 cccccccd 883ad000 883ad2c8 88823e60 808640c8 883ad194 88782000
3de0: 883ad2c4 00000001 00000000 88823e00 805f2f18 807e1be0 20070013 ffffffff
[<80013200>] (__irq_svc) from [<807e1be0>] (wait_for_common+0x14/0x144)
[<807e1be0>] (wait_for_common) from [<805f2f18>] (vf610_read_raw+0xf8/0x1a8)
[<805f2f18>] (vf610_read_raw) from [<805ef854>] (iio_read_channel_info+0x94/0x98)
[<805ef854>] (iio_read_channel_info) from [<8037f0b0>] (dev_attr_show+0x1c/0x48)
[<8037f0b0>] (dev_attr_show) from [<8014b3d8>] (sysfs_kf_seq_show+0x88/0xf4)
[<8014b3d8>] (sysfs_kf_seq_show) from [<8010a4cc>] (seq_read+0x1e4/0x484)
[<8010a4cc>] (seq_read) from [<800ea138>] (__vfs_read+0x1c/0xd0)
[<800ea138>] (__vfs_read) from [<800ea920>] (vfs_read+0x7c/0x108)
[<800ea920>] (vfs_read) from [<800eb1b8>] (SyS_read+0x44/0x9c)
[<800eb1b8>] (SyS_read) from [<8000f480>] (ret_fast_syscall+0x0/0x3c)
ADC2 pins 0 to 4, Interrupt pin GIC_SPI 101 and ADC2 Clock are configured for Touch Screen Controller node tsc in imx6ul.dtsi as given below:
tsc: tsc@02040000 {
compatible = "fsl,imx6ul-tsc";
reg = <0x02040000 0x4000>, <0x0219c000 0x4000>;
interrupts = <GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 101 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6UL_CLK_IPG>,
<&clks IMX6UL_CLK_ADC2>;
clock-names = "tsc", "adc";
status = "disabled";
};
Is the configuration for ADC Pins 6 & 7 made for custom board are OK?
Please suggest if any change is required.
Solved! Go to Solution.
Hi Arunachalam
one can look at similar issue
is it working without dts modifications.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The same problem as yours, has the problem been solved?
Thanks, Igor.
I was able to make it work.
Regards,
Arun
Hi, Arunachalam Ramaswamy.
Can you tell me the details what you have done
thanks
YU
Hi Arunachalam
one can look at similar issue
is it working without dts modifications.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------