Hello
I want to configure the ENET1_TX_CLK pin as ENET1_REF_CLK1 with 50Mhz for the phy. In u-boot it works. But not in kernel.
DTS config:
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
pinctrl-assert-gpios = <&gpio1 10 GPIO_ACTIVE_HIGH>, <&gpio1 10 GPIO_ACTIVE_LOW>;
phy-mode = "rmii";
status = "okay";
};
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6SX_PAD_ENET1_MDIO__ENET1_MDIO 0xa0b1
MX6SX_PAD_ENET1_MDC__ENET1_MDC 0xa0b1
MX6SX_PAD_ENET1_CRS__ENET1_CRS 0xa0b1
MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0051
MX6SX_PAD_RGMII1_TD0__ENET1_TX_DATA_0 0xa0b1
MX6SX_PAD_RGMII1_TD1__ENET1_TX_DATA_1 0xa0b1
MX6SX_PAD_RGMII1_TX_CTL__ENET1_TX_EN 0xa0b1
MX6SX_PAD_RGMII1_RD0__ENET1_RX_DATA_0 0x3081
MX6SX_PAD_RGMII1_RD1__ENET1_RX_DATA_1 0x3081
>;
};
I change in the mach-imx6sx.c file IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK to "1"
static void __init imx6sx_enet_clk_sel(void)
{
struct regmap *gpr;
gpr = syscon_regmap_lookup_by_compatible("fsl,imx6sx-iomuxc-gpr");
if (!IS_ERR(gpr)) {
regmap_update_bits(gpr, IOMUXC_GPR1,
IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK, 0);
regmap_update_bits(gpr, IOMUXC_GPR1,
IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, 1);
} else {
pr_err("failed to find fsl,imx6sx-iomux-gpr regmap\n");
}
}
What should I do?
Peter
已解决! 转到解答。
Hi
Yes it do :smileylaugh: I found the problems with the devregs tool. Here my patch. May be helpful for someone.
Index: kernel-source/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h
===================================================================
--- kernel-source.orig/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h 2015-12-05 09:54:09.201580469 +0100
+++ kernel-source/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h 2015-12-05 09:54:15.237580459 +0100
@@ -397,9 +397,9 @@
#define IMX6SX_GPR1_VADC_SW_RST_MASK (0x1 << 19)
#define IMX6SX_GPR1_VADC_SW_RST_RESET (0x1 << 19)
#define IMX6SX_GPR1_VADC_SW_RST_RELEASE (0x0 << 19)
-#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK (0x3 << 13)
-#define IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK (0x3 << 17)
-#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_EXT (0x3 << 13)
+#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK (0x1 << 13)
+#define IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK (0x1 << 17)
+#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_EXT (0x1 << 13)
#define IMX6SX_GPR2_MQS_OVERSAMPLE_MASK (0x1 << 26)
#define IMX6SX_GPR2_MQS_OVERSAMPLE_SHIFT (26)
Index: kernel-source/arch/arm/mach-imx/mach-imx6sx.c
===================================================================
--- kernel-source.orig/arch/arm/mach-imx/mach-imx6sx.c 2015-12-05 09:53:51.685580497 +0100
+++ kernel-source/arch/arm/mach-imx/mach-imx6sx.c 2015-12-05 10:08:39.025579056 +0100
@@ -211,7 +211,7 @@
regmap_update_bits(gpr, IOMUXC_GPR1,
IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK, 0);
regmap_update_bits(gpr, IOMUXC_GPR1,
- IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, 0);
+ IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK);
} else {
pr_err("failed to find fsl,imx6sx-iomux-gpr regmap\n");
}
Index: kernel-source/arch/arm/mach-imx/clk-imx6sx.c
===================================================================
--- kernel-source.orig/arch/arm/mach-imx/clk-imx6sx.c 2015-12-05 09:53:51.661580497 +0100
+++ kernel-source/arch/arm/mach-imx/clk-imx6sx.c 2015-12-05 09:54:15.237580459 +0100
@@ -615,8 +615,8 @@
imx_clk_set_parent(clks[IMX6SX_CLK_ENET_PRE_SEL], clks[IMX6SX_CLK_PLL2_PFD2]);
imx_clk_set_parent(clks[IMX6SX_CLK_ENET_SEL], clks[IMX6SX_CLK_ENET_PODF]);
imx_clk_set_rate(clks[IMX6SX_CLK_ENET_PODF], 200000000);
- imx_clk_set_rate(clks[IMX6SX_CLK_ENET_REF], 125000000);
- imx_clk_set_rate(clks[IMX6SX_CLK_ENET2_REF], 125000000);
+ imx_clk_set_rate(clks[IMX6SX_CLK_ENET_REF], 50000000);
+ imx_clk_set_rate(clks[IMX6SX_CLK_ENET2_REF], 50000000);
/* Audio clocks */
imx_clk_set_rate(clks[IMX6SX_CLK_PLL4_AUDIO_DIV], 393216000);
Index: kernel-source/arch/arm/boot/dts/imx6sx-pinfunc.h
===================================================================
--- kernel-source.orig/arch/arm/boot/dts/imx6sx-pinfunc.h 2015-12-05 09:53:51.409580498 +0100
+++ kernel-source/arch/arm/boot/dts/imx6sx-pinfunc.h 2015-12-05 09:54:15.237580459 +0100
@@ -316,7 +316,7 @@
#define MX6SX_PAD_ENET1_RX_CLK__VDEC_DEBUG_35 0x008C 0x03D4 0x0000 0x8 0x0
#define MX6SX_PAD_ENET1_RX_CLK__PCIE_CTRL_DEBUG_29 0x008C 0x03D4 0x0000 0x9 0x0
#define MX6SX_PAD_ENET1_TX_CLK__ENET1_TX_CLK 0x0090 0x03D8 0x0000 0x0 0x0
-#define MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0090 0x03D8 0x0760 0x1 0x1
+#define MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0090 0x03D8 0x0760 0x11 0x1
#define MX6SX_PAD_ENET1_TX_CLK__AUDMUX_AUD4_RXD 0x0090 0x03D8 0x0644 0x2 0x1
#define MX6SX_PAD_ENET1_TX_CLK__UART1_DTR_B 0x0090 0x03D8 0x0000 0x3 0x0
#define MX6SX_PAD_ENET1_TX_CLK__SPDIF_SR_CLK 0x0090 0x03D8 0x0000 0x4 0x0
Hi,
Just to double check, if you configure the pin in uboot but you do not try to reconfigure it in Linux, Does it work?
Have you used the memtool application found in the /unit_tests folder? that can help to check the register configurations of the IOMUXC. Please use that and check that the IOMUXC is configured correctly.
Best Regards,
Alejandro
Hi
Yes it do :smileylaugh: I found the problems with the devregs tool. Here my patch. May be helpful for someone.
Index: kernel-source/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h
===================================================================
--- kernel-source.orig/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h 2015-12-05 09:54:09.201580469 +0100
+++ kernel-source/include/linux/mfd/syscon/imx6q-iomuxc-gpr.h 2015-12-05 09:54:15.237580459 +0100
@@ -397,9 +397,9 @@
#define IMX6SX_GPR1_VADC_SW_RST_MASK (0x1 << 19)
#define IMX6SX_GPR1_VADC_SW_RST_RESET (0x1 << 19)
#define IMX6SX_GPR1_VADC_SW_RST_RELEASE (0x0 << 19)
-#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK (0x3 << 13)
-#define IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK (0x3 << 17)
-#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_EXT (0x3 << 13)
+#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK (0x1 << 13)
+#define IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK (0x1 << 17)
+#define IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_EXT (0x1 << 13)
#define IMX6SX_GPR2_MQS_OVERSAMPLE_MASK (0x1 << 26)
#define IMX6SX_GPR2_MQS_OVERSAMPLE_SHIFT (26)
Index: kernel-source/arch/arm/mach-imx/mach-imx6sx.c
===================================================================
--- kernel-source.orig/arch/arm/mach-imx/mach-imx6sx.c 2015-12-05 09:53:51.685580497 +0100
+++ kernel-source/arch/arm/mach-imx/mach-imx6sx.c 2015-12-05 10:08:39.025579056 +0100
@@ -211,7 +211,7 @@
regmap_update_bits(gpr, IOMUXC_GPR1,
IMX6SX_GPR1_FEC_CLOCK_MUX_SEL_MASK, 0);
regmap_update_bits(gpr, IOMUXC_GPR1,
- IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, 0);
+ IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK, IMX6SX_GPR1_FEC_CLOCK_PAD_DIR_MASK);
} else {
pr_err("failed to find fsl,imx6sx-iomux-gpr regmap\n");
}
Index: kernel-source/arch/arm/mach-imx/clk-imx6sx.c
===================================================================
--- kernel-source.orig/arch/arm/mach-imx/clk-imx6sx.c 2015-12-05 09:53:51.661580497 +0100
+++ kernel-source/arch/arm/mach-imx/clk-imx6sx.c 2015-12-05 09:54:15.237580459 +0100
@@ -615,8 +615,8 @@
imx_clk_set_parent(clks[IMX6SX_CLK_ENET_PRE_SEL], clks[IMX6SX_CLK_PLL2_PFD2]);
imx_clk_set_parent(clks[IMX6SX_CLK_ENET_SEL], clks[IMX6SX_CLK_ENET_PODF]);
imx_clk_set_rate(clks[IMX6SX_CLK_ENET_PODF], 200000000);
- imx_clk_set_rate(clks[IMX6SX_CLK_ENET_REF], 125000000);
- imx_clk_set_rate(clks[IMX6SX_CLK_ENET2_REF], 125000000);
+ imx_clk_set_rate(clks[IMX6SX_CLK_ENET_REF], 50000000);
+ imx_clk_set_rate(clks[IMX6SX_CLK_ENET2_REF], 50000000);
/* Audio clocks */
imx_clk_set_rate(clks[IMX6SX_CLK_PLL4_AUDIO_DIV], 393216000);
Index: kernel-source/arch/arm/boot/dts/imx6sx-pinfunc.h
===================================================================
--- kernel-source.orig/arch/arm/boot/dts/imx6sx-pinfunc.h 2015-12-05 09:53:51.409580498 +0100
+++ kernel-source/arch/arm/boot/dts/imx6sx-pinfunc.h 2015-12-05 09:54:15.237580459 +0100
@@ -316,7 +316,7 @@
#define MX6SX_PAD_ENET1_RX_CLK__VDEC_DEBUG_35 0x008C 0x03D4 0x0000 0x8 0x0
#define MX6SX_PAD_ENET1_RX_CLK__PCIE_CTRL_DEBUG_29 0x008C 0x03D4 0x0000 0x9 0x0
#define MX6SX_PAD_ENET1_TX_CLK__ENET1_TX_CLK 0x0090 0x03D8 0x0000 0x0 0x0
-#define MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0090 0x03D8 0x0760 0x1 0x1
+#define MX6SX_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x0090 0x03D8 0x0760 0x11 0x1
#define MX6SX_PAD_ENET1_TX_CLK__AUDMUX_AUD4_RXD 0x0090 0x03D8 0x0644 0x2 0x1
#define MX6SX_PAD_ENET1_TX_CLK__UART1_DTR_B 0x0090 0x03D8 0x0000 0x3 0x0
#define MX6SX_PAD_ENET1_TX_CLK__SPDIF_SR_CLK 0x0090 0x03D8 0x0000 0x4 0x0