imx6sl: avaibility of 32kHz Clock through REF_CLK_32K pad in Deep Sleep ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sl: avaibility of 32kHz Clock through REF_CLK_32K pad in Deep Sleep ?

ソリューションへジャンプ
801件の閲覧回数
ArnaudMouiche
Contributor II

Hi,

REF_CLK_32K pad signal is usefull to feed a RTC clocking to external component requiring a RTC clock, without adding extra quartz (bluetooth, etc...)

Yet, I'm wondering if it is still possible for the imx6SL to output this signal when the imx6SL goes in "Deep Sleep Mode" ?

Regards,

Arnaud

ラベル(3)
タグ(4)
0 件の賞賛
返信
1 解決策
696件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ArnaudMouiche

yes REF_CLK_32K signal is available

in Deep Sleep Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
697件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ArnaudMouiche

yes REF_CLK_32K signal is available

in Deep Sleep Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信