imx6sl: avaibility of 32kHz Clock through REF_CLK_32K pad in Deep Sleep ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sl: avaibility of 32kHz Clock through REF_CLK_32K pad in Deep Sleep ?

Jump to solution
1,281 Views
ArnaudMouiche
Contributor II

Hi,

REF_CLK_32K pad signal is usefull to feed a RTC clocking to external component requiring a RTC clock, without adding extra quartz (bluetooth, etc...)

Yet, I'm wondering if it is still possible for the imx6SL to output this signal when the imx6SL goes in "Deep Sleep Mode" ?

Regards,

Arnaud

Labels (3)
Tags (4)
0 Kudos
Reply
1 Solution
1,176 Views
igorpadykov
NXP Employee
NXP Employee

Hi ArnaudMouiche

yes REF_CLK_32K signal is available

in Deep Sleep Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,177 Views
igorpadykov
NXP Employee
NXP Employee

Hi ArnaudMouiche

yes REF_CLK_32K signal is available

in Deep Sleep Mode.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply