imx6q music play crash in surfaceflinger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q music play crash in surfaceflinger

1,049 次查看
zhanxiaozhang
Contributor III

imx6q player music crash ,does anyone meet the situation,here is the log

11-06 03:41:11.389 F/libc ( 123): Fatal signal 11 (SIGSEGV) at 0x000000dc (code=1), thread 123 (surfaceflinger)
11-06 03:41:11.399 F/libc ( 782): Fatal signal 11 (SIGSEGV) at 0x562de050 (code=2), thread 782 (zs11mediaplayer)
11-06 03:41:11.499 I/DEBUG ( 122): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
11-06 03:41:11.499 I/DEBUG ( 122): Build fingerprint: 'MG/mg_zsq/mg_zsq:4.4.3/MG_ZS11/20181026-1512:eng/dev-keys'
11-06 03:41:11.499 I/DEBUG ( 122): Revision: '0'
11-06 03:41:11.499 I/DEBUG ( 122): pid: 123, tid: 123, name: surfaceflinger >>> /system/bin/surfaceflinger <<<
11-06 03:41:11.499 I/DEBUG ( 122): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 000000dc
11-06 03:41:11.509 W/NativeCrashListener( 434): Couldn't find ProcessRecord for pid 123
11-06 03:41:11.529 I/DEBUG ( 122): r0 000000c8 r1 00000003 r2 00000000 r3 00000002
11-06 03:41:11.529 I/DEBUG ( 122): AM write failure (32 / Broken pipe)
11-06 03:41:11.529 I/DEBUG ( 122): r4 000000c8 r5 78af2374 r6 87392933 r7 78c7055c
11-06 03:41:11.529 I/DEBUG ( 122): r8 78c71c1c r9 00000258 sl 78c71cfc fp 00000000
11-06 03:41:11.529 I/DEBUG ( 122): ip 78c71c7c sp 7e961570 lr 76df5057 pc 76df1270 cpsr 000f0030
11-06 03:41:11.529 I/DEBUG ( 122): d0 0000000000000000 d1 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d2 0000000000000000 d3 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d4 0000000000000000 d5 0000000800000002
11-06 03:41:11.529 I/DEBUG ( 122): d6 0000000800000002 d7 3b5a740e497ffff0
11-06 03:41:11.529 I/DEBUG ( 122): d8 0000000000000000 d9 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d10 0000000000000000 d11 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d12 0000000000000000 d13 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d14 0000000000000000 d15 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d16 0000000000000000 d17 0000025800000400
11-06 03:41:11.529 I/DEBUG ( 122): d18 0000000000000000 d19 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d20 0000000000000001 d21 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d22 0000000000000000 d23 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d24 0000000000000000 d25 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d26 0000000000000001 d27 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d28 0000000000000000 d29 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): d30 0000000000000001 d31 0000000000000000
11-06 03:41:11.529 I/DEBUG ( 122): scr 80000010
11-06 03:41:11.529 I/DEBUG ( 122):
11-06 03:41:11.529 I/DEBUG ( 122): backtrace:
11-06 03:41:11.529 I/DEBUG ( 122): #00 pc 00020270 /system/lib/libGLES_trace.so
11-06 03:41:11.529 I/DEBUG ( 122): #01 pc 00024053 /system/lib/libGLES_trace.so (android::gltrace::GLTrace_glGetShaderInfoLog(unsigned int, int, int*, char*)+100)
11-06 03:41:11.529 I/DEBUG ( 122): #02 pc 00012837 /system/lib/libutils.so
11-06 03:41:11.529 I/DEBUG ( 122):
11-06 03:41:11.529 I/DEBUG ( 122): stack:
11-06 03:41:11.529 I/DEBUG ( 122): 7e961530 7e961658 [stack]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961534 768f1528 /system/lib/egl/libEGL_VIVANTE.so
11-06 03:41:11.529 I/DEBUG ( 122): 7e961538 78c7055c [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e96153c 768f0e30 /system/lib/egl/libEGL_VIVANTE.so
11-06 03:41:11.529 I/DEBUG ( 122): 7e961540 ffffffff
11-06 03:41:11.529 I/DEBUG ( 122): 7e961544 78a621ac [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961548 78af2374 [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e96154c 00000000
11-06 03:41:11.529 I/DEBUG ( 122): 7e961550 ffffffff
11-06 03:41:11.529 I/DEBUG ( 122): 7e961554 78a621ac [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961558 78af4c14 [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e96155c 78c7055c [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961560 78c71c1c [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961564 00000000
11-06 03:41:11.529 I/DEBUG ( 122): 7e961568 78a62714 [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e96156c 78af2374 [heap]
11-06 03:41:11.529 I/DEBUG ( 122): #00 7e961570 78a62714 [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961574 78af2374 [heap]
11-06 03:41:11.529 I/DEBUG ( 122): 7e961578 87392933
11-06 03:41:11.529 I/DEBUG ( 122): 7e96157c 76df5057 /system/lib/libGLES_trace.so (android::gltrace::GLTrace_glGetShaderInfoLog(unsigned int, int, int*, char*)+104)
11-06 03:41:11.529 I/DEBUG ( 122): #01 7e961580 00000001
11-06 03:41:11.529 I/DEBUG ( 122): 7e961584 00000000
11-06 03:41:11.529 I/DEBUG ( 122): 7e961588 7e961600 [stack]
11-06 03:41:11.529 I/DEBUG ( 122): 7e96158c 00000002
11-06 03:41:11.529 I/DEBUG ( 122): 7e961590 00000000
11-06 03:41:11.529 I/DEBUG ( 122): 7e961594 76ec5cd1 /system/lib/libc.so (malloc+12)
11-06 03:41:11.539 I/DEBUG ( 122): 7e961598 00000400
11-06 03:41:11.539 I/DEBUG ( 122): 7e96159c 78c71d6c [heap]
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615a0 78af2374 [heap]
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615a4 76e918b1 /system/lib/libutils.so (android::VectorImpl::_grow(unsigned int, unsigned int)+140)
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615a8 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615ac 76e91523 /system/lib/libutils.so (android::VectorImpl::itemLocation(unsigned int) const+10)
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615b0 7e9616d8 [stack]
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615b4 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615b8 00000001
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615bc 76e91917 /system/lib/libutils.so (android::VectorImpl::insertAt(void const*, unsigned int, unsigned int)+44)
11-06 03:41:11.539 I/DEBUG ( 122): ........ ........
11-06 03:41:11.539 I/DEBUG ( 122): #02 7e961628 76e94742 /system/lib/libutils.so
11-06 03:41:11.539 I/DEBUG ( 122): 7e96162c 6e48eb71 /system/lib/egl/libGLESv2_VIVANTE.so
11-06 03:41:11.539 I/DEBUG ( 122): 7e961630 6e48eb6d /system/lib/egl/libGLESv2_VIVANTE.so
11-06 03:41:11.539 I/DEBUG ( 122): 7e961634 768eb485 /system/lib/egl/libEGL_VIVANTE.so (eglSwapBuffers+72)
11-06 03:41:11.539 I/DEBUG ( 122): 7e961638 7e9616d8 [stack]
11-06 03:41:11.539 I/DEBUG ( 122): 7e96163c 76d5ab5b /system/lib/libui.so
11-06 03:41:11.539 I/DEBUG ( 122): 7e961640 7e9616b8 [stack]
11-06 03:41:11.539 I/DEBUG ( 122): 7e961644 76d5b4d3 /system/lib/libui.so
11-06 03:41:11.539 I/DEBUG ( 122): 7e961648 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 7e96164c 7e961684 [stack]
11-06 03:41:11.539 I/DEBUG ( 122): 7e961650 00000007
11-06 03:41:11.539 I/DEBUG ( 122): 7e961654 76d5ba37 /system/lib/libui.so (android::Region::boolean_operation(int, android::Region&, android::Region const&, android::Region const&, int, int)+92)
11-06 03:41:11.539 I/DEBUG ( 122): 7e961658 78e73ae8 [heap]
11-06 03:41:11.539 I/DEBUG ( 122): 7e96165c 00000001
11-06 03:41:11.539 I/DEBUG ( 122): 7e961660 00000001
11-06 03:41:11.539 I/DEBUG ( 122): 7e961664 78c6c628 [heap]
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near r5:
11-06 03:41:11.539 I/DEBUG ( 122): 78af2354 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78af2364 00000000 00000000 00000143 00000138
11-06 03:41:11.539 I/DEBUG ( 122): 78af2374 444c4745 00000000 01df5e76 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78af2384 00000001 0000007b 76f68154 00000023
11-06 03:41:11.539 I/DEBUG ( 122): 78af2394 78af24b4 78a6219c 78a621ac 78c7055c
11-06 03:41:11.539 I/DEBUG ( 122): 78af23a4 78af4c14 78e2bcec 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78af23b4 00000001 78af37e0 00000010 00000011
11-06 03:41:11.539 I/DEBUG ( 122): 78af23c4 00000012 78a621bc 76e2cb1d 76e2cc21
11-06 03:41:11.539 I/DEBUG ( 122): 78af23d4 00000000 00000044 00000000 6c080028
11-06 03:41:11.539 I/DEBUG ( 122): 78af23e4 47456269 49565f4c 544e4156 6f732e45
11-06 03:41:11.539 I/DEBUG ( 122): 78af23f4 00000000 0000206c 00000000 00000060
11-06 03:41:11.539 I/DEBUG ( 122): 78af2404 00000000 6c080028 4c476269 615f5345
11-06 03:41:11.539 I/DEBUG ( 122): 78af2414 6f72646e 732e6469 0000006f 0000206d
11-06 03:41:11.539 I/DEBUG ( 122): 78af2424 00000000 00000080 00000000 6c080030
11-06 03:41:11.539 I/DEBUG ( 122): 78af2434 4c476269 31765345 5f4d435f 41564956
11-06 03:41:11.539 I/DEBUG ( 122): 78af2444 2e45544e 00006f73 00000000 0000206e
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near r6:
11-06 03:41:11.539 I/DEBUG ( 122): 87392910 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392920 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392930 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392940 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392950 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392960 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392970 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392980 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392990 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 873929a0 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 873929b0 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 873929c0 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 873929d0 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 873929e0 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 873929f0 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122): 87392a00 ffffffff ffffffff ffffffff ffffffff
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near r7:
11-06 03:41:11.539 I/DEBUG ( 122): 78c7053c 73656e74 00000000 5649565f 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c7054c 7269645f 00000000 00001813 00001808
11-06 03:41:11.539 I/DEBUG ( 122): 78c7055c 534c4745 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c7056c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c7057c 00000000 00000000 00000000 00000001
11-06 03:41:11.539 I/DEBUG ( 122): 78c7058c 00000400 00000258 01df5e76 00000001
11-06 03:41:11.539 I/DEBUG ( 122): 78c7059c 01df5e76 00000000 00000000 01df5e76
11-06 03:41:11.539 I/DEBUG ( 122): 78c705ac 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c705bc 00000000 01df5e76 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c705cc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c705dc 00000000 00000000 00000000 78c72a34
11-06 03:41:11.539 I/DEBUG ( 122): 78c705ec 00000000 000000d4 76884980 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c705fc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c7060c 00000000 00000000 00000000 00000020
11-06 03:41:11.539 I/DEBUG ( 122): 78c7061c 0000309a 00000000 00000020 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c7062c 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near r8:
11-06 03:41:11.539 I/DEBUG ( 122): 78c71bfc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c0c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c1c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c2c 00000000 00000000 78c6d6d0 78c71d6c
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c3c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c4c 00000000 00000000 00000001 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c5c 00000300 00000001 78c6d7f0 78c722e0
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c6c 78c721e0 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c7c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c8c 00000400 00000258 00000003 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c9c 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cac 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cbc 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71ccc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cdc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cec 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near sl:
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cdc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cec 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cfc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d0c 00000000 00000000 00000000 78c720b8
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d1c 78c72150 78c6d6d0 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d2c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d3c 00000000 78c70644 00000400 00000258
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d4c 78c72a34 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d5c 78c6d8ac 6e48cc79 000002c3 000002b8
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d6c 46525553 00000000 00000006 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d7c 00000132 00000001 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d8c 00000400 00000258 00000400 00000258
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d9c 00000000 00000020 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71dac 00000000 00000000 00000000 00001000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71dbc 00258000 00258000 00258000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71dcc 00000000 00000000 00000000 00000008
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near ip:
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c5c 00000300 00000001 78c6d7f0 78c722e0
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c6c 78c721e0 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c7c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c8c 00000400 00000258 00000003 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71c9c 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cac 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cbc 00000000 00000400 00000258 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71ccc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cdc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cec 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71cfc 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d0c 00000000 00000000 00000000 78c720b8
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d1c 78c72150 78c6d6d0 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d2c 00000000 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d3c 00000000 78c70644 00000400 00000258
11-06 03:41:11.539 I/DEBUG ( 122): 78c71d4c 78c72a34 00000000 00000000 00000000
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): memory near sp:
11-06 03:41:11.539 I/DEBUG ( 122): 7e961550 ffffffff 78a621ac 78af4c14 78c7055c
11-06 03:41:11.539 I/DEBUG ( 122): 7e961560 78c71c1c 00000000 78a62714 78af2374
11-06 03:41:11.539 I/DEBUG ( 122): 7e961570 78a62714 78af2374 87392933 76df5057
11-06 03:41:11.539 I/DEBUG ( 122): 7e961580 00000001 00000000 7e961600 00000002
11-06 03:41:11.539 I/DEBUG ( 122): 7e961590 00000000 76ec5cd1 00000400 78c71d6c
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615a0 78af2374 76e918b1 00000000 76e91523
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615b0 7e9616d8 00000000 00000001 76e91917
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615c0 00000000 00000000 00000400 00000258
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615d0 76e69e1f 78c6c430 00000001 768e1941
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615e0 78a626d4 76d5b843 7e9615f7 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 7e9615f0 78c6c4b0 00000001 78d8e6f8 76d5dee0
11-06 03:41:11.539 I/DEBUG ( 122): 7e961600 78c6c4b0 78d8e700 00000000 768f1528
11-06 03:41:11.539 I/DEBUG ( 122): 7e961610 78c7055c 768f0e30 78af2374 00000000
11-06 03:41:11.539 I/DEBUG ( 122): 7e961620 0000000c 76e94839 76e94742 6e48eb71
11-06 03:41:11.539 I/DEBUG ( 122): 7e961630 6e48eb6d 768eb485 7e9616d8 76d5ab5b
11-06 03:41:11.539 I/DEBUG ( 122): 7e961640 7e9616b8 76d5b4d3 00000000 7e961684
11-06 03:41:11.539 I/DEBUG ( 122):
11-06 03:41:11.539 I/DEBUG ( 122): code around pc:
11-06 03:41:11.539 I/DEBUG ( 122): 76df1250 e1a02003 ebffff44 e1a03000 e1a00003
11-06 03:41:11.539 I/DEBUG ( 122): 76df1260 e24bd004 e8bd8800 0002ddac 4604b570
11-06 03:41:11.539 I/DEBUG ( 122): 76df1270 460e6943 42936982 6905d117 00581c59
11-06 03:41:11.539 I/DEBUG ( 122): 76df1280 bfb84288 61a04608 f7ff0080 6963ee76
11-06 03:41:11.539 I/DEBUG ( 122): 76df1290 009a4629 f7ff6120 f104ee76 4295021c
11-06 03:41:11.539 I/DEBUG ( 122): 76df12a0 b115d003 f7ff4628 6960ee74 1c436921
11-06 03:41:11.539 I/DEBUG ( 122): 76df12b0 6020f841 bd706163 4604b570 460e6b03
11-06 03:41:11.539 I/DEBUG ( 122): 76df12c0 42936b42 6ac5d117 00581c59 bfb84288
11-06 03:41:11.539 I/DEBUG ( 122): 76df12d0 63604608 f7ff0080 6b23ee50 009a4629
11-06 03:41:11.539 I/DEBUG ( 122): 76df12e0 f7ff62e0 f104ee50 42950238 b115d003
11-06 03:41:11.539 I/DEBUG ( 122): 76df12f0 f7ff4628 6b20ee4e 1c426ae1 0380eb01
11-06 03:41:11.539 I/DEBUG ( 122): 76df1300 6322601e b570bd70 f8d04604 460e308c
11-06 03:41:11.549 I/DEBUG ( 122): 76df1310 2090f8d0 d1194293 5088f8d0 00581c59
11-06 03:41:11.549 I/DEBUG ( 122): 76df1320 bfb84288 f8c44608 f7ff0090 4629ee26
11-06 03:41:11.549 I/DEBUG ( 122): 76df1330 208cf8d4 0088f8c4 ee24f7ff 0094f104
11-06 03:41:11.549 I/DEBUG ( 122): 76df1340 d0034285 4628b115 ee22f7ff 308cf8d4
11-06 03:41:11.549 I/DEBUG ( 122):
11-06 03:41:11.549 I/DEBUG ( 122): code around lr:
11-06 03:41:11.549 I/DEBUG ( 122): 76df5034 f7fc6084 4630f919 f98ff7fc f8d04651
11-06 03:41:11.549 I/DEBUG ( 122): 76df5044 730530c8 0203f043 f8c06084 f7fc20c8
11-06 03:41:11.549 I/DEBUG ( 122): 76df5054 4630f90b f981f7fc f8d04649 730530c8
11-06 03:41:11.549 I/DEBUG ( 122): 76df5064 0203f043 f8c06084 f7fc20c8 4630f8fd
11-06 03:41:11.549 I/DEBUG ( 122): 76df5074 f973f7fc f8d04641 730530c8 f0436084
11-06 03:41:11.549 I/DEBUG ( 122): 76df5084 f8c00503 f7fc50c8 2001f8ef ef8af7fb
11-06 03:41:11.549 I/DEBUG ( 122): 76df5094 20034604 f7fb460d 464aef86 ec414643
11-06 03:41:11.549 I/DEBUG ( 122): 76df50a4 6b780b18 f8d04651 4658c3f8 200347e0
11-06 03:41:11.549 I/DEBUG ( 122): 76df50b4 ef78f7fb 20014682 f7fb468b aa08ef74
11-06 03:41:11.549 I/DEBUG ( 122): 76df50c4 9207462b 8b02ed8d e9cd4622 9606ab04
11-06 03:41:11.549 I/DEBUG ( 122): 76df50d4 9020f8cd 8024f8cd 0100e9cd f01e4638
11-06 03:41:11.549 I/DEBUG ( 122): 76df50e4 4638f908 f01c4631 4630fc51 fd82f01f
11-06 03:41:11.549 I/DEBUG ( 122): 76df50f4 ecbdb01f e8bd8b02 e92d8ff0 ed2d4ff0
11-06 03:41:11.549 I/DEBUG ( 122): 76df5104 b09f8b02 4683ae0a 46984691 468a4630
11-06 03:41:11.549 I/DEBUG ( 122): 76df5114 fe78f01e f01c2400 9b1dfb1b 911121bb
11-06 03:41:11.549 I/DEBUG ( 122): 76df5124 f0434607 901d0008 f7fc4630 4659f916
11-06 03:41:11.629 I/DEBUG ( 122): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
11-06 03:41:11.629 I/DEBUG ( 122): Build fingerprint: 'MG/mg_zsq/mg_zsq:4.4.3/MG_ZS11/20181026-1512:eng/dev-keys'
11-06 03:41:11.629 I/DEBUG ( 122): Revision: '0'
11-06 03:41:11.629 I/DEBUG ( 122): pid: 782, tid: 782, name: zs11mediaplayer >>> com.shinco.zs11mediaplayer <<<
11-06 03:41:11.629 I/DEBUG ( 122): signal 11 (SIGSEGV), code 2 (SEGV_ACCERR), fault addr 562de050
11-06 03:41:11.629 W/SurfaceComposerClient( 629): ComposerService remote (surfaceflinger) died [0x55a52cb8]
11-06 03:41:11.629 W/SurfaceComposerClient( 685): ComposerService remote (surfaceflinger) died [0x556b5f10]
11-06 03:41:11.629 I/ServiceManager( 119): service 'SurfaceFlinger' died
11-06 03:41:11.629 W/SurfaceComposerClient( 434): ComposerService remote (surfaceflinger) died [0x54f64f98]
11-06 03:41:11.629 E/DisplayEventReceiver( 434): Display event receiver pipe was closed or an error occurred. events=0x9
11-06 03:41:11.629 E/DisplayEventReceiver( 434): Display event receiver pipe was closed or an error occurred. events=0x9
11-06 03:41:11.639 E/DisplayEventReceiver( 434): Display event receiver pipe was closed or an error occurred. events=0x9
11-06 03:41:11.639 E/DisplayEventReceiver( 434): Display event receiver pipe was closed or an error occurred. events=0x9
11-06 03:41:11.639 E/DisplayEventReceiver( 685): Display event receiver pipe was closed or an error occurred. events=0x9
11-06 03:41:11.639 E/DisplayEventReceiver( 629): Display event receiver pipe was closed or an error occurred. events=0x9
11-06 03:41:11.649 I/ServiceManager( 119): service 'media.audio_flinger' died
11-06 03:41:11.649 I/ServiceManager( 119): service 'media.player' died
11-06 03:41:11.649 I/ServiceManager( 119): service 'media.camera' died
11-06 03:41:11.649 I/ServiceManager( 119): service 'media.audio_policy' died

标签 (1)
0 项奖励
回复
2 回复数

903 次查看
zhanxiaozhang
Contributor III

thx!

but i did not find any crash info app(java apk) related,it only show libui.so  libEGL_VIVANTE.so.

0 项奖励
回复

903 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi zhangxiaozhang,

Your application is accessing memory outside of its address space. This is most likely an invalid pointer access. SIGSEGV. You may still see some stack trace information in the logcat if you look around a bit after the application process crashes. It will not tell you the line number within the file, but will tell you which object files and addresses were in use in the call chain. From there you can often figure out which area of the code is problematic. You can also setup a gdb native connection to the target process and catch it in the debugger.

Regards

0 项奖励
回复