I have an IMX6 sabre SD board running Linux version 3.0.35.
The USB OTG port works find in host mode (when used with an OTG cable), but does not respond in device mode when the board is connected to a PC. lsusb on the PC shows no sign of the imx6 board.
I probed the D+ and D- lines on the board and neither is moves when the host cable is plugged in, so it is not responding properly as a device. A high speed device is suppose to drive D+ high and a low speed device is suppose to drive D- high.
Anybody have this working and know what's wrong?
已解决! 转到解答。
To use the gadget drivers you need to load them first. This is what I was missing and why my iMX6 board never worked in device mode.
The gadget functions are not complied directly into the kernel, but are modules stored here:
/lib/modules/3.0.35-.../kernel/drivers/usb/gadget
To get the iMX6 to act like an OTG device you must load a module before connecting to a USB host.
modprobe g_serial.ko
To unload the module
modprobe -r g_serial.ko
Alternatively you can change your kernel config file to load the module on startup.
This option requires you to load the module from the command line as shown above:
CONFIG_USB_G_SERIAL=m
If you change it
CONFIG_USB_G_SERIAL=y
Now the gadget serial driver is present in the kernel and does not need to be loaded from the command line.
To use the gadget drivers you need to load them first. This is what I was missing and why my iMX6 board never worked in device mode.
The gadget functions are not complied directly into the kernel, but are modules stored here:
/lib/modules/3.0.35-.../kernel/drivers/usb/gadget
To get the iMX6 to act like an OTG device you must load a module before connecting to a USB host.
modprobe g_serial.ko
To unload the module
modprobe -r g_serial.ko
Alternatively you can change your kernel config file to load the module on startup.
This option requires you to load the module from the command line as shown above:
CONFIG_USB_G_SERIAL=m
If you change it
CONFIG_USB_G_SERIAL=y
Now the gadget serial driver is present in the kernel and does not need to be loaded from the command line.
Hi,
modprobe g_serial works for me but I tried to add CONFIG_USB_G_SERIAL=y to my config file (it didn't appear at all) and the port didn't recognized... there is something else i need to add to make it work on startup?
Thanks,
Tzipi
Hi j b
most simple way to check usb device mode is to try connect to MFG Tool or
run SDK (it has usb device mode example)
SABRE Platform for Smart Devices Based on the i.MX 6 Series - Quick Start Guide
In Freescale Linux BSP peripheral mode-supports MSC, and CDC (Communication Devices Class) drivers
which include ethernet and serial support.
However you should first load necessary driver (like g_file_storage) and perform
other actions (specific for each mode), to make i.MX6 work in device mode.
One can check L3.0.35_4.1.0_LINUX_DOCS
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The OTG port works in device mode with the the MFG_TOOL. It connects to the computer and the D+ line responds.
However, OTG in device mode is not working with my custom kernel.
Have I set something wrong in the configuration? I'm pasting my configuration file below.
****************************************************************************************************************
#
# Automatically generated make config: don't edit
# LTIB version: 8.1.2
#
CONFIG_CONFIG_TITLE="Freescale iMX6x Based Boards"
CONFIG_PLATFORM_COMMENT="Freescale iMX6x Based Boards"
CONFIG_VENDOR="Freescale"
CONFIG_PLATFORM="imx6q"
CONFIG_PLATFORM_SUBDIR="imx"
CONFIG_GNUTARCH="arm"
CONFIG_LINTARCH="arm"
CONFIG_CFGHOST="arm-linux"
CONFIG_ARMEABI_ARCH=y
CONFIG_VFP_ARCH=y
#
# LTIB settings
#
#
# System features
#
CONFIG_FEAT_CACHE_RPMS=y
CONFIG_ENDIAN="little"
#
# Choose the target C library type
#
CONFIG_GLIBC=y
# CONFIG_UCLIBC is not set
CONFIG_CHOICE_BASE_LIBS=y
# CONFIG_CHOICE_GLIBC is not set
# CONFIG_CHOICE_UCLIBC is not set
# CONFIG_LIBC_NONE is not set
# CONFIG_PKG_GLIBC is not set
# CONFIG_PKG_UCLIBC is not set
#
# Toolchain component options
#
CONFIG_PKG_BASE_LIBS=y
CONFIG_PKG_LIBC_WANT_SHARED_LIBS=y
# CONFIG_PKG_LIBC_WANT_CRT_FILES is not set
# CONFIG_PKG_LIBC_WANT_HEADERS1 is not set
# CONFIG_PKG_LIBC_WANT_STATIC_LIBS is not set
# CONFIG_PKG_LIBC_WANT_C_LOCALES is not set
CONFIG_PKG_CXX_WANT_SHARED_LIBS=y
# CONFIG_PKG_CXX_WANT_HEADERS is not set
# CONFIG_PKG_CXX_WANT_STATIC_LIBS is not set
CONFIG_PKG_GCC_WANT_LIBGCC_SHARED=y
CONFIG_DYNAMIC_LINKER="/lib/ld.so.1"
CONFIG_SYS_WANT_MMU=y
CONFIG_SYS_WANT_SHARED=y
#
# Toolchain selection.
#
CONFIG_TOOLCHAIN_ARMEABI_FSL_GCC_LINARO_MULTILIB=y
# CONFIG_TOOLCHAIN_ARMEABI_FSL_GCC_MULTILIB is not set
# CONFIG_TOOLCHAIN_ARMEABI_CODE_SOURCERY is not set
# CONFIG_TOOLCHAIN_ARMEABI_GLIBC1 is not set
# CONFIG_TOOLCHAIN_ARMEABI_CUSTOM is not set
CONFIG_TOOLCHAIN="gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm"
CONFIG_TOOLCHAIN_PATH="/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain"
CONFIG_TOOLCHAIN_PREFIX="arm-none-linux-gnueabi-"
CONFIG_TOOLCHAIN_CFLAGS="-O2 -march=armv7-a -mfpu=vfpv3 -mfloat-abi=softfp"
#
# Choose your bootloader for U-Boot
#
CONFIG_BOOTLOADER_U_BOOT=y
# CONFIG_BOOTLOADER_GIT is not set
# CONFIG_U_BOOT_DIR_BUILD is not set
# CONFIG_BOOTLOADER_NONE is not set
CONFIG_BOOTLOADER_U_BOOT_200908=y
# CONFIG_BOOTLOADER_U_BOOT_201210 is not set
#
# Choose your board for u-boot
#
# CONFIG_BOARD_MX6Q_ARM2 is not set
# CONFIG_BOARD_MX6Q_ARM2_LPDDR2 is not set
# CONFIG_BOARD_MX6Q_ARM2_LPDDR2POP is not set
# CONFIG_BOARD_MX6Q_SABRELITE is not set
# CONFIG_BOARD_MX6Q_SABREAUTO is not set
# CONFIG_BOARD_MX6Q_SABREAUTO_NAND is not set
# CONFIG_BOARD_MX6Q_SABREAUTO_WEIMNOR is not set
# CONFIG_BOARD_MX6Q_SABREAUTO_SPI-NOR is not set
# CONFIG_BOARD_MX6Q_SABRESD is not set
# CONFIG_BOARD_MX6Q_HDMIDONGLE is not set
# CONFIG_BOARD_MX6Q_HDMIDONGLE_NAND is not set
# CONFIG_BOARD_MX6DL_ARM2 is not set
# CONFIG_BOARD_MX6DL_ARM2_LPDDR2 is not set
# CONFIG_BOARD_MX6DL_SABRESD is not set
# CONFIG_BOARD_MX6DL_SABREAUTO is not set
# CONFIG_BOARD_MX6DL_SABREAUTO_NAND is not set
# CONFIG_BOARD_MX6DL_SABREAUTO_SPI-NOR is not set
# CONFIG_BOARD_MX6DL_SABREAUTO_WEIMNOR is not set
# CONFIG_BOARD_MX6DL_HDMIDONGLE is not set
# CONFIG_BOARD_MX6DL_HDMIDONGLE_NAND is not set
# CONFIG_BOARD_MX6SOLO_SABREAUTO is not set
# CONFIG_BOARD_MX6SOLO_SABREAUTO_NAND is not set
# CONFIG_BOARD_MX6SOLO_SABREAUTO_WEIMNOR is not set
# CONFIG_BOARD_MX6SOLO_SABREAUTO_SPI-NOR is not set
# CONFIG_BOARD_MX6SOLO_SABRESD is not set
CONFIG_BOARD_MX6Q_DTRA3=y
CONFIG_PKG_U_BOOT="u-boot-v2009.08"
CONFIG_PKG_U_BOOT_CONFIG_TYPE="mx6q_dtra3_config"
CONFIG_PKG_U_BOOT_BUILD_ARGS="OPTFLAGS=-Os"
CONFIG_SYSCFG_KTARG="uImage"
CONFIG_SYSCFG_BOOT_KERNEL="arch/arm/boot/uImage arch/arm/boot/zImage"
#
# Choose your Kernel
#
# CONFIG_KERNEL_3507 is not set
CONFIG_KERNEL_3035=y
# CONFIG_KERNEL_3015 is not set
# CONFIG_KERNEL_38 is not set
# CONFIG_KERNEL_35 is not set
# CONFIG_KERNEL_31 is not set
# CONFIG_KERNEL_28 is not set
# CONFIG_KERNEL_GIT is not set
# CONFIG_KERNEL_DIR_BUILD is not set
# CONFIG_KERNEL_NONE is not set
# CONFIG_PKG_KERNEL_FORCE is not set
# CONFIG_PKG_KERNEL_WANT_CSCOPE is not set
CONFIG_PKG_KERNEL="kernel-3.0.35"
CONFIG_PKG_KERNEL_WANT_HEADERS=y
# CONFIG_PKG_KERNEL_WANT_CF is not set
CONFIG_PKG_KERNEL_LEAVESRC=y
# CONFIG_PKG_KERNEL_UPDATER is not set
## CONFIG_PKG_KERNEL_PRECONFIG="mx6q_sabresd_config"
CONFIG_PKG_KERNEL_PRECONFIG="mx6q_dtra3_config"
CONFIG_DISTRO="dist/lfs-5.1"
#
# Package selection
#
#
# Package list
#
#
# Platform specific package selection
#
CONFIG_PKG_FIRMWARE_IMX=y
CONFIG_PKG_IMX_TEST=y
CONFIG_PKG_IMX_LIB=y
# CONFIG_PKG_IMX_VPU_LIB is not set
CONFIG_PKG_KOBS_NG=y
# CONFIG_PKG_LTP_IMX is not set
# CONFIG_PKG_WPA_SUPPLICANT is not set
# CONFIG_PKG_GPU_VIV_BIN_MX6Q is not set
CONFIG_PKG_UUC=y
# CONFIG_PKG_ATHEROS_WIFI is not set
# CONFIG_PKG_MTDEV is not set
# CONFIG_PKG_GPU_VIV_WL_BIN_MX6Q is not set
# CONFIG_PKG_WESTON_IMX_BIN is not set
# CONFIG_PKG_HDCP_APP_BIN is not set
#
# Freescale Multimedia Plugins/Codecs
#
# CONFIG_PKG_LIBFSLCODEC is not set
# CONFIG_PKG_LIBFSLPARSER is not set
# CONFIG_PKG_LIBFSLVPUWRAP is not set
# CONFIG_PKG_LIBFSLAACPCODEC is not set
# CONFIG_PKG_LIBFSLAC3CODEC is not set
# CONFIG_PKG_LIBFSLMSCODEC is not set
# CONFIG_PKG_LIBFSLMSPARSER is not set
# CONFIG_PKG_GST_FSL_PLUGINS is not set
# CONFIG_PKG_GST_PLUGINS_GL is not set
# CONFIG_PKG_FSL_ALSA_PLUGINS is not set
#
# Common package selection list
#
# CONFIG_PKG_ASTERISK is not set
# CONFIG_PKG_ATK is not set
# CONFIG_PKG_AUTOCONF is not set
# CONFIG_PKG_AUTOMAKE is not set
# CONFIG_PKG_ALSA_LIB is not set
# CONFIG_PKG_ALSA_UTILS is not set
CONFIG_PKG_BASH=y
CONFIG_PKG_BASH_WANT_NO_SH_SYMLINK=y
# CONFIG_PKG_BIND is not set
CONFIG_PKG_BINUTILS=y
# CONFIG_PKG_BINUTILS_BUILD_DOCS is not set
# CONFIG_PKG_BISON is not set
# CONFIG_PKG_BLUEZ_HCIDUMP is not set
# CONFIG_PKG_BLUEZ_LIBS is not set
# CONFIG_PKG_BLUEZ_UTILS is not set
# CONFIG_PKG_BOA is not set
# CONFIG_PKG_BONNIE_PLUS_PLUS is not set
# CONFIG_PKG_BRIDGE_UTILS is not set
CONFIG_PKG_BUSYBOX=y
CONFIG_PKG_BUSYBOX_PRECONFIG="busybox.config"
# CONFIG_PKG_BUSYBOX_WANT_CF is not set
# CONFIG_PKG_BZIP2 is not set
# CONFIG_PKG_CAIRO is not set
# CONFIG_PKG_CAN4LINUX is not set
# CONFIG_PKG_CANTEST is not set
# CONFIG_PKG_CCACHE is not set
# CONFIG_PKG_CHEESE is not set
# CONFIG_PKG_CLAMAV is not set
# CONFIG_PKG_CONNTRACK_TOOLS is not set
# CONFIG_PKG_COREUTILS is not set
# CONFIG_PKG_CPIO is not set
# CONFIG_PKG_CPUFREQUTILS is not set
# CONFIG_PKG_CRACKLIB is not set
# CONFIG_PKG_CRAMFS is not set
# CONFIG_PKG_CRASHME is not set
# CONFIG_PKG_CURL is not set
# CONFIG_PKG_DAEMONIZER is not set
CONFIG_PKG_DEVMEM2=y
# CONFIG_PKG_DHCP is not set
# CONFIG_PKG_DB1 is not set
# CONFIG_PKG_DB4 is not set
# CONFIG_PKG_DBUS is not set
# CONFIG_PKG_DBUS_GLIB is not set
# CONFIG_PKG_DEV is not set
# CONFIG_PKG_MDEV is not set
CONFIG_PKG_UDEV=y
# CONFIG_PKG_UDEV_WANT_AUTOMOUNT is not set
CONFIG_PKG_UDEV_WANT_NON_RAID=y
CONFIG_PKG_UDEV_WANT_IMX=y
# CONFIG_PKG_DEVFSD is not set
# CONFIG_PKG_DEV_NONE is not set
# CONFIG_PKG_DIFFUTILS is not set
# CONFIG_PKG_DIRECTFB is not set
# CONFIG_PKG_DISTCC is not set
CONFIG_PKG_DOSFSTOOLS=y
CONFIG_PKG_NEWFS_MSDOS=y
# CONFIG_PKG_DROPBEAR is not set
# CONFIG_PKG_DTC is not set
# CONFIG_PKG_DT_D is not set
CONFIG_PKG_E2FSPROGS=y
#
# Enlightenment window manager packages
#
CONFIG_CHOICE_ENLIGHTENMENT_NONE=y
# CONFIG_CHOICE_ENLIGHTENMENT is not set
# CONFIG_PKG_ED is not set
# CONFIG_PKG_EEL is not set
# CONFIG_PKG_ENCHANT is not set
# CONFIG_PKG_EOG is not set
# CONFIG_PKG_EPDFVIEW is not set
# CONFIG_PKG_ETHTOOL is not set
# CONFIG_PKG_EVOLUTION is not set
# CONFIG_PKG_EVOLUTION_DATA_SERVER is not set
# CONFIG_PKG_EVTEST is not set
# CONFIG_PKG_EXPAT is not set
# CONFIG_PKG_FAAD2 is not set
# CONFIG_PKG_FAKEROOT is not set
CONFIG_PKG_FAKE_PROVIDES=y
# CONFIG_PKG_FARSIGHT is not set
# CONFIG_PKG_FBPAN is not set
# CONFIG_PKG_FBSET is not set
# CONFIG_PKG_FBV is not set
# CONFIG_PKG_FFMPEG is not set
# CONFIG_PKG_FINDUTILS is not set
# CONFIG_PKG_FLEX is not set
# CONFIG_PKG_FMTOOLS is not set
# CONFIG_PKG_FONTCONFIG is not set
# CONFIG_PKG_FREETYPE is not set
# CONFIG_PKG_GAWK is not set
# CONFIG_PKG_GCONF_DBUS is not set
# CONFIG_PKG_GDBM is not set
CONFIG_PKG_GDB=y
CONFIG_PKG_GDB_NATIVE_WANT_ED=y
CONFIG_PKG_GDB_CROSS_WANT_ED=y
# CONFIG_PKG_GDB_XML_WANT_ED is not set
CONFIG_PKG_GDB_SERVER_WANT_ED=y
# CONFIG_PKG_GDB_BUILD_DOCS is not set
# CONFIG_PKG_GENEXT2FS is not set
# CONFIG_PKG_GENROMFS is not set
# CONFIG_PKG_GEN_INIT_CPIO is not set
# CONFIG_PKG_GETTEXT is not set
# CONFIG_PKG_GIT is not set
# CONFIG_PKG_GLIB2 is not set
# CONFIG_PKG_GMP is not set
# CONFIG_PKG_GNOME_DESKTOP is not set
# CONFIG_PKG_GNOME_MIME_DATA is not set
# CONFIG_PKG_GNOME_ICON_THEME is not set
# CONFIG_PKG_GNOME_VFS is not set
# CONFIG_PKG_GNOME_KEYRING is not set
# CONFIG_PKG_GPSD is not set
# CONFIG_PKG_GREP is not set
# CONFIG_PKG_GROFF is not set
# CONFIG_PKG_GSTREAMER_CORE is not set
# CONFIG_PKG_GST_PLUGINS_FARSIGHT is not set
# CONFIG_PKG_GTK2 is not set
# CONFIG_PKG_GTKHTML is not set
# CONFIG_PKG_HAL is not set
# CONFIG_PKG_HDPARM is not set
# CONFIG_PKG_HELLOWORLD is not set
# CONFIG_PKG_HELLOWORLD_MOD is not set
# CONFIG_PKG_HESIOD is not set
# CONFIG_PKG_HOSTAPD is not set
CONFIG_PKG_HOTPLUG=y
# CONFIG_PKG_HTTPD is not set
CONFIG_PKG_I2C_TOOLS=y
# CONFIG_PKG_IOZONE is not set
CONFIG_PKG_INPUT_UTILS=y
# CONFIG_PKG_IPROUTE is not set
# CONFIG_PKG_INETUTILS is not set
# CONFIG_PKG_IPERF is not set
# CONFIG_PKG_OPENSWAN is not set
# CONFIG_PKG_STRONGSWAN is not set
CONFIG_PKG_IPSEC_SUITE_NONE=y
# CONFIG_PKG_IPSEC_TOOLS is not set
# CONFIG_PKG_IPSECADM is not set
# CONFIG_PKG_IPTABLES is not set
# CONFIG_PKG_IPUTILS is not set
# CONFIG_PKG_IRATTACH is not set
# CONFIG_PKG_IRDADUMP is not set
# CONFIG_PKG_ISO_CODES is not set
# CONFIG_PKG_KBD is not set
# CONFIG_PKG_KEYFUZZ is not set
# CONFIG_PKG_KRB5 is not set
# CONFIG_PKG_LESS is not set
# CONFIG_PKG_LFS_UTILS is not set
# CONFIG_PKG_LIBERATION_FONTS is not set
# CONFIG_PKG_LIBART_LGPL is not set
# CONFIG_PKG_LIBBONOBO is not set
# CONFIG_PKG_LIBBONOBOUI is not set
# CONFIG_PKG_LIBGCRYPT is not set
# CONFIG_PKG_LIBGPG_ERROR is not set
# CONFIG_PKG_LIBGLADE is not set
# CONFIG_PKG_LIBGNOME is not set
# CONFIG_PKG_LIBGNOMECANVAS is not set
# CONFIG_PKG_LIBGNOMEUI is not set
# CONFIG_PKG_LIBICONV is not set
# CONFIG_PKG_LIBIDL is not set
# CONFIG_PKG_LIBID3TAG is not set
# CONFIG_PKG_LIBMAD is not set
# CONFIG_PKG_LIBMPEG2 is not set
# CONFIG_PKG_LIBNETFILTER_CONNTRACK is not set
# CONFIG_PKG_LIBNFNETLINK is not set
# CONFIG_PKG_LIBNL is not set
CONFIG_PKG_LIBJPEG=y
# CONFIG_PKG_LIBELF is not set
# CONFIG_PKG_LIBNET is not set
# CONFIG_PKG_LIBOGG is not set
# CONFIG_PKG_LIBPCAP is not set
CONFIG_PKG_LIBPNG=y
# CONFIG_PKG_LIBOIL is not set
# CONFIG_PKG_LIBRSVG is not set
# CONFIG_PKG_LIBSOUP is not set
# CONFIG_PKG_LIBTASN1 is not set
CONFIG_PKG_LIBTERMCAP=y
# CONFIG_PKG_LIBTIFF is not set
# CONFIG_PKG_LIBTOOL is not set
CONFIG_PKG_LIBUSB=y
# CONFIG_PKG_LIBXML2 is not set
# CONFIG_PKG_LINUX_ATM is not set
# CONFIG_PKG_LINUX_WLAN is not set
# CONFIG_PKG_MPFR is not set
# CONFIG_PKG_LKC is not set
CONFIG_PKG_LOGROTATE=y
# CONFIG_PKG_LTP is not set
# CONFIG_PKG_LMBENCH is not set
# CONFIG_PKG_LM_SENSORS is not set
# CONFIG_PKG_LRZSZ is not set
CONFIG_PKG_LZO=y
# CONFIG_PKG_M4 is not set
# CONFIG_PKG_MADPLAY is not set
# CONFIG_PKG_MAKE is not set
# CONFIG_PKG_MAN is not set
#
# Matchbox window manager packages
#
CONFIG_CHOICE_MATCHBOX_NONE=y
# CONFIG_CHOICE_MATCHBOX is not set
# CONFIG_PKG_MDADM is not set
CONFIG_PKG_MERGE=y
# CONFIG_PKG_MICROWINDOWS is not set
# CONFIG_PKG_MIITOOL is not set
# CONFIG_PKG_MINICOM is not set
CONFIG_PKG_MODEPS=y
# CONFIG_PKG_MODUTILS is not set
# CONFIG_PKG_MODULE_INIT_TOOLS is not set
CONFIG_MODUTILS_NONE=y
# CONFIG_PKG_MPLAYER is not set
# CONFIG_PKG_MP3PLAY is not set
CONFIG_PKG_MTD_UTILS=y
# CONFIG_PKG_MUX_SERVER is not set
# CONFIG_PKG_MYSQL is not set
# CONFIG_PKG_NAUTILUS is not set
CONFIG_PKG_NCURSES=y
CONFIG_PKG_NCURSES_WANT_REDUCED_SET=y
# CONFIG_PKG_NET_SNMP is not set
# CONFIG_PKG_NET_TOOLS is not set
# CONFIG_PKG_NETCAT is not set
# CONFIG_PKG_NETPERF is not set
# CONFIG_PKG_NFS_UTILS is not set
# CONFIG_PKG_NSS_MDNS is not set
# CONFIG_PKG_NTPCLIENT is not set
# CONFIG_PKG_OPENOBEX is not set
# CONFIG_PKG_OPENCV is not set
# CONFIG_PKG_OPENSSH is not set
# CONFIG_PKG_OPENSSL is not set
CONFIG_PKG_OPROFILE=y
# CONFIG_PKG_ORBIT2 is not set
# CONFIG_PKG_PANGO is not set
# CONFIG_PKG_PATCH is not set
CONFIG_PKG_PCIUTILS=y
# CONFIG_PKG_PCMCIAUTILS is not set
# CONFIG_PKG_PCRE is not set
# CONFIG_PKG_PERL is not set
# CONFIG_PKG_PHP is not set
# CONFIG_PKG_PIDENTD is not set
# CONFIG_PKG_PKGCONFIG is not set
# CONFIG_PKG_PLAY is not set
# CONFIG_PKG_POPPLER is not set
CONFIG_PKG_POPT=y
# CONFIG_PKG_PORTMAP is not set
# CONFIG_PKG_PPP is not set
CONFIG_PKG_PROCINFO=y
CONFIG_PKG_PROCPS=y
CONFIG_PKG_PSMISC=y
# CONFIG_PKG_PYTHON is not set
#
# Qt
#
CONFIG_QT_NONE=y
# CONFIG_PKG_QT_EMBEDDED is not set
# CONFIG_PKG_QT_X11 is not set
#
# Qtopia
#
CONFIG_QTOPIA_NONE=y
# CONFIG_PKG_QTOPIA is not set
# CONFIG_PKG_QTOPIA_4 is not set
#
# Applications
#
#
# Settings applications
#
# CONFIG_PKG_READLINE is not set
# CONFIG_PKG_RPM is not set
# CONFIG_PKG_RNG_TOOLS is not set
# CONFIG_PKG_RSYNC is not set
# CONFIG_PKG_RT_TESTS is not set
# CONFIG_PKG_RTCTEST is not set
# CONFIG_PKG_SAMBA is not set
# CONFIG_PKG_SASH is not set
# CONFIG_PKG_SCHEDUTILS is not set
# CONFIG_PKG_SCREEN is not set
# CONFIG_PKG_SED is not set
CONFIG_PKG_SEQ=y
# CONFIG_PKG_SETSERIAL is not set
# CONFIG_PKG_SIMICSFS_MOD is not set
CONFIG_PKG_SKELL=y
# CONFIG_PKG_SKELL_WANT_TERMINFO is not set
# CONFIG_PKG_SPARSE is not set
# CONFIG_PKG_STATSERIAL is not set
# CONFIG_PKG_SQLITE is not set
CONFIG_PKG_STRACE=y
CONFIG_PKG_SYSCONFIG=y
# CONFIG_PKG_SYSFSUTILS is not set
# CONFIG_PKG_SYSKLOGD is not set
# CONFIG_PKG_SYSSTAT is not set
# CONFIG_PKG_SYSVINIT is not set
# CONFIG_PKG_TAR is not set
# CONFIG_PKG_TCLAP is not set
# CONFIG_PKG_TCPDUMP is not set
# CONFIG_PKG_TCP_WRAPPERS is not set
# CONFIG_PKG_TERMCAP is not set
# CONFIG_PKG_TEXINFO is not set
# CONFIG_PKG_TIME is not set
# CONFIG_PKG_TIMEZONE is not set
# CONFIG_PKG_TINYLOGIN is not set
# CONFIG_PKG_TINYPROXY is not set
# CONFIG_PKG_TOTEM is not set
# CONFIG_PKG_TOTEM_PL_PARSER is not set
# CONFIG_PKG_TSLIB is not set
# CONFIG_PKG_TUNCTL is not set
CONFIG_PKG_USBUTILS=y
# CONFIG_PKG_UCLINUX_CKSUM is not set
CONFIG_PKG_UTIL_LINUX=y
# CONFIG_PKG_U_BOOT_TOOLS is not set
# CONFIG_PKG_UNIFDEF is not set
# CONFIG_PKG_UNZIP is not set
# CONFIG_PKG_VIM is not set
# CONFIG_PKG_VPLAY is not set
# CONFIG_PKG_VSFTPD is not set
# CONFIG_PKG_WATCHDOG is not set
# CONFIG_PKG_WGET is not set
# CONFIG_PKG_WHICH is not set
# CONFIG_PKG_WIRELESS_TOOLS is not set
# CONFIG_PKG_XFSPROGS is not set
# CONFIG_PKG_LIBXKBCOMMON is not set
# CONFIG_PKG_LIBXCB is not set
# CONFIG_PKG_LIBFFI is not set
# CONFIG_PKG_WAYLAND is not set
#
# X11
#
CONFIG_X11_NONE=y
# CONFIG_PKG_XORG_SERVER is not set
#
# X11 libraries and packages
#
# CONFIG_PKG_RANDRPROTO is not set
# CONFIG_PKG_RENDERPROTO is not set
# CONFIG_PKG_FIXESPROTO is not set
# CONFIG_PKG_DAMAGEPROTO is not set
# CONFIG_PKG_XF86DRIPROTO is not set
# CONFIG_PKG_XCMISCPROTO is not set
# CONFIG_PKG_XEXTPROTO is not set
# CONFIG_PKG_XPROTO is not set
# CONFIG_PKG_SCRNSAVERPROTO is not set
# CONFIG_PKG_BIGREQSPROTO is not set
# CONFIG_PKG_RESOURCEPROTO is not set
# CONFIG_PKG_FONTSPROTO is not set
# CONFIG_PKG_INPUTPROTO is not set
# CONFIG_PKG_KBPROTO is not set
# CONFIG_PKG_VIDEOPROTO is not set
# CONFIG_PKG_COMPOSITEPROTO is not set
# CONFIG_PKG_RECORDPROTO is not set
# CONFIG_PKG_FONTCACHEPROTO is not set
# CONFIG_PKG_XF86BIGFONTPROTO is not set
# CONFIG_PKG_XCB_PROTO is not set
# CONFIG_PKG_LIBPTHREAD_STUBS is not set
# CONFIG_PKG_LIBFONTENC is not set
# CONFIG_PKG_XTRANS is not set
# CONFIG_PKG_LIBDRM is not set
# CONFIG_PKG_PIXMAN is not set
# CONFIG_PKG_LIBXKBFILE is not set
# CONFIG_PKG_LIBXFONT is not set
# CONFIG_PKG_LIBXDMCP is not set
# CONFIG_PKG_LIBXAU is not set
# CONFIG_PKG_LIBX11 is not set
# CONFIG_PKG_LIBXEXT is not set
# CONFIG_PKG_LIBXFT is not set
# CONFIG_PKG_LIBXRANDR is not set
# CONFIG_PKG_LIBXRENDER is not set
# CONFIG_PKG_LIBXFIXES is not set
# CONFIG_PKG_LIBXDAMAGE is not set
# CONFIG_PKG_LIBPCIACCESS is not set
# CONFIG_PKG_FONTUTIL is not set
# CONFIG_PKG_LIBICE is not set
# CONFIG_PKG_LIBSM is not set
# CONFIG_PKG_LIBXPM is not set
# CONFIG_PKG_LIBXT is not set
# CONFIG_PKG_LIBXMU is not set
# CONFIG_PKG_LIBXAW is not set
# CONFIG_PKG_LIBXXF86DGA is not set
# CONFIG_PKG_XORG_X11_XKB_UTILS is not set
# CONFIG_PKG_XORG_X11_PROTO_DEVEL is not set
# CONFIG_PKG_XORG_X11_TWM is not set
# CONFIG_PKG_XTERM is not set
# CONFIG_PKG_YAFFS_UTILS is not set
# CONFIG_PKG_ZAPTEL is not set
CONFIG_PKG_ZLIB=y
#
# Additional Package selection
#
# CONFIG_PKG_LIBCGI is not set
#
# DTRA-3 Components
#
#
# Selection for DTRA-3 features
#
CONFIG_PKG_MUIMAGER=y
CONFIG_PKG_DTRA3=y
CONFIG_PKG_LIBDTRA3=y
CONFIG_PKG_LIBUSBX=y
CONFIG_PKG_PREBUILT_PYTHON=y
CONFIG_PKG_PREBUILT_PILLOW=y
CONFIG_PKG_PY_USB=y
CONFIG_PKG_SERVER=y
CONFIG_PKG_DTRA3_SUPPORT=y
#
# Target System Configuration
#
#
# Options
#
CONFIG_SYSCFG_HOSTNAME="dtra_3"
CONFIG_SYSCFG_WANT_LOGIN_TTY=y
CONFIG_SYSCFG_LOGING_TTY="::respawn:/etc/rc.d/rc_mxc.S"
CONFIG_SYSCFG_MODLIST=""
CONFIG_SYSCFG_START_UDEV=y
CONFIG_SYSCFG_START_NETWORK=y
#
# Network setup
#
#
#
#
CONFIG_SYSCFG_IFACE0=y
CONFIG_SYSCFG_NET_INTERFACE0="eth0"
CONFIG_SYSCFG_DHCPC0=y
#
#
#
# CONFIG_SYSCFG_IFACE1 is not set
#
#
#
# CONFIG_SYSCFG_IFACE2 is not set
#
#
#
# CONFIG_SYSCFG_IFACE3 is not set
#
#
#
# CONFIG_SYSCFG_IFACE4 is not set
CONFIG_SYSCFG_DHCPC_CMD="udhcpc -b -i "
# CONFIG_SYSCFG_SETTIME is not set
CONFIG_SYSCFG_START_SYSLOG=y
CONFIG_SYSCFG_START_INETD=y
CONFIG_SYSCFG_INETD_ARGS=""
#
# Target Image Generation
#
#
# Options
#
#
# Choose your root filesystem image type
#
CONFIG_DEPLOYMENT_JFFS2=y
# CONFIG_DEPLOYMENT_UBIFS is not set
# CONFIG_DEPLOYMENT_RAMDISK is not set
# CONFIG_DEPLOYMENT_CRAMFS is not set
# CONFIG_DEPLOYMENT_INITRAMFS is not set
# CONFIG_DEPLOYMENT_ROMFS is not set
# CONFIG_DEPLOYMENT_NFS is not set
CONFIG_SYSCFG_DEPLOYMENT_STYLE="JFFS2"
# CONFIG_WANT_POST_BUILD_SCRIPT is not set
CONFIG_DEPLOYMENT_ERASE_BLOCK_SIZE="512"
# CONFIG_SYSCFG_READONLY_FS is not set
CONFIG_SYSCFG_TMPFS_SIZE="4m"
CONFIG_SYSCFG_RAM_DIRS="/tmp /var"
CONFIG_DEPLOYMENT_ROOTFS_DIR=""
# CONFIG_DEPLOYMENT_ROOTFS_KEEPSTAGE is not set
# CONFIG_DEPLOYMENT_HL2SL is not set
CONFIG_DEPLOYMENT_RM_DOCS=y
# CONFIG_DEPLOYMENT_RM_BOOT is not set
CONFIG_DEPLOYMENT_RM_USR_SRC=y
CONFIG_DEPLOYMENT_RM_USR_INCLUDE=y
CONFIG_DEPLOYMENT_RM_LOCALES=y
CONFIG_DEPLOYMENT_RM_USER_DIRS="/opt/qt /usr/share/man /usr/man /u /usr/arm-linux /usr/lib/fonts"
CONFIG_DEPLOYMENT_RM_USER_FILES="/usr/lib/libqte* /usr/include/q* /usr/include/jri*.h /usr/include/npapi.h /usr/include/npupp.h"
# CONFIG_DEPLOYMENT_RM_STATIC_LIBS is not set
CONFIG_DEPLOYMENT_RM_RPMDB="/var/lib/rpm"
# CONFIG_DEPLOYMENT_STRIP is not set
# CONFIG_DEPLOYMENT_PADDING_EN is not set
CONFIG_DEPLOYMENT_PAGESIZE_KB="4"
CONFIG_ERASE_BLOCK_SIZE="64"
CONFIG_CAP_UCLIBC=y
CONFIG_CAP_GLIBC=y
CONFIG_CAP_LFS_5_1=y
CONFIG_CAP_HAS_MMU=y
CONFIG_CAP_HAS_SHARED=y
CONFIG_PKG_GCC_NAME="nobuild"
CONFIG_SYSCFG_TMPFS="tmpfs"
CONFIG_INITTAB_LINE="::respawn:-/sbin/getty -L console 0 screen"
CONFIG_UCLIBC_DYNAMIC_LINKER="/lib/ld-uClibc.so.0"
CONFIG_GLIBC_DYNAMIC_LINKER="/lib/ld.so.1"
CONFIG_SYSCFG_BAUD="115200"
CONFIG_SYSCFG_CONSOLEDEV="ttyS0"
CONFIG_SYSCFG_BOOTLOADER="u-boot"
CONFIG_U_BOOT_IMAGE_TYPE="ppc"
CONFIG_SYSCFG_RUNKERNELADDR="0x0"
CONFIG_SYSCFG_LOADKERNELADDR="0x800000"
CONFIG_SYSCFG_LOADDTBADDR="0x9F0000"
CONFIG_SYSCFG_LOADRAMADDR="0xB00000"
CONFIG_SYSCFG_CUTARG="zImage"
CONFIG_CAP_FSL_EXT=y
CONFIG_LTIB_RELEASE="8.1.2"
Hi Hi j b
first, if board connects to MFG Tools then i.MX6 usb device mode
works well
then second - what are you trying to test now ?
regarding Linux - you can start with Demo images
L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I'm booting the board from an SD card. On the SD card is my customized version of u-boot and the kernel. The board boots successfully and I can use the OTG port in host mode, but the board does not respond when I use the OTG port in device mode (ie connected to a computer). Since the OTG port worked in device mode with the MFG TOOL this suggests that I have configured something incorrectly in my kernel. I pasted my configuration file in the previous post. Have I somehow disabled OTG device mode?
Even all is good: board, linux configurations, all that will not work
until you do not understand how to test it: what one should do
and what results he should see.
For usb device mode links below may help
Linux Software User Manual (i.MX6) - BlueWiki
http://www.armadeus.com/wiki/index.php?title=USB_Gadget
https://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:usb-gadget:file-backed_storage