Dear Community
i have a question about PMU_REG_CORE register on imx6d
i want change REG1_TARG value
change PMU_REG_CORE log |
---|
root@imx6qdlsolo:/unit_tests# ./memtool -32 0x020c8140 1 E Reading 0x1 count starting at address 0x020C8140
0x020C8140: 004C000B
root@imx6qdlsolo:/unit_tests# ./memtool -32 0x020c8140=0x004c200b Writing 32-bit value 0x4C200B to address 0x020C8140 root@imx6qdlsolo:/unit_tests# root@imx6qdlsolo:/unit_tests# ./memtool -32 0x020c8140 1 E Reading 0x1 count starting at address 0x020C8140
0x020C8140: 004C200B
root@imx6qdlsolo:/unit_tests# ./autorun-vpu.sh Checking for devnode: /dev/mxc_vpu autorun-vpu.sh: PASS devnode found: /dev/mxc_vpu
Running test case: ./mxc_vpu_test.out -C config_dec [INFO] VPU test program built on Sep 16 2016 00:25:03 [INFO] Product Info: i.MX6Q/D/S [INFO] VPU firmware version: 3.1.1_r46072 [INFO] VPU library version: 5.4.35 [INFO] Format: STD_MPEG4 [INFO] MPEG4 class: MPEG4 [INFO] Input file "akiyo.mp4" opened. [INFO] bitstreamMode 0, chromaInterleave 0, mapType 0, tiled2LinearEnable 0 [INFO] Mpeg4 Profile: 0 Level: 3 Interlaced: 0 [INFO] Aspect Ratio Table index: 1 [INFO] Decoder: width = 176, height = 144, frameRateRes = 15, frameRateDiv = 4294967295, count = 4 [INFO] CROP left/top/right/bottom 0 0 0 0 [INFO] v4l output to /dev/video17 [INFO] Display to 1024 768, top offset 0, left offset 0 [INFO] Display fps will be 30
^C[WARN] Ctrl-C received [INFO] 100 frames took 3238842 microseconds [INFO] dec fps = 2109.48 [INFO] total fps= 30.88 autorun-vpu.sh: PASS test case: ./mxc_vpu_test.out -C config_dec
^C root@imx6qdlsolo:/unit_tests# ./memtool -32 0x020c8140 1 E Reading 0x1 count starting at address 0x020C8140 0x020C8140: 004C000B |
PMU_REG_CORE register value is restored after vpu test script
i wonder that why that value is restored ?
how can i setting PMU_REG_CORE vaule
Thanks BR