imx6 read emmc via JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 read emmc via JTAG

1,722 Views
Alex_Smart
Contributor II

I was looking for solution for reading/witing eemc contents with JTAG interface, and no luck so far. There are several similar topics without an answer

https://community.nxp.com/t5/i-MX-Processors/eMMC-programming-with-JTAG-interface-iMX-6SX/m-p/137414...

 

Here they are usung u-boot

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Bring-up-i-MX6-via-JTAG/ta-p/1124954

Labels (2)
0 Kudos
Reply
4 Replies

1,701 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Alex_Smart 

I hope you are doing very well.

Unfortunately, the JTAG interface is not designed to do what you need/want. 

NXP provides a solution to flash the eMMC thorough UUU tool. Also, you can use this UUU tool with SDP/fastboot to communicate partitions of any device on the board (SD/eMMC).

 

Best regards!

Salas.

 

 

0 Kudos
Reply

1,685 Views
Alex_Smart
Contributor II
Well thats weird. Im new to this particular CPU, how do you guys debug code on eMMC? What IDE are you using?
0 Kudos
Reply

1,662 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

1,651 Views
Alex_Smart
Contributor II

I see. So in that case Linux uploaded via ssh. I have a several questions if its nit too much trouble:

Is it possible to write some kind of microcode, load it to RAM and perform read/write operations in emmc?
Is it possible to read eFuse via JTAG?

Is it possible to read emmc via uuu tool?

0 Kudos
Reply