HW: imx6q
SW: yocto linux 3.14.28
bsp compile: bitbake fsl-image-qt5
video: 1080P MV , attch file
root@imx6qsabresd:/var/volatile/log# fbset
mode "1920x1080-60"
# D: 148.500 MHz, H: 67.500 kHz, V: 60.000 Hz
geometry 1920 1080 1920 1088 16
timings 6734 148 88 36 4 44 5
hsync high
vsync high
rgba 5/11,6/5,5/0,0/0
endmode
root@imx6qsabresd:/var/volatile/log#
player tool: imx player, video player
When I play the video, the speed is about twice as fast? how i do?
Hello,
Would you please upload the video stream for analyzer?
Regards,
Play 1080p movies will be like this
Your seetings look correct. Have you checked other 1080p streams, all play as 2x speed or only this streams play as 2x speed? If it's only this stream which is being reproduced at 2X, it may be a stream issue. Could you could upload this stream?
Is is very possible that the problem resides on the display configuration. Since it's set as 60 fps it's twice faster than the common play and that would make the video look twice as fast. Would you please try with 30 fps configuration and let us know your findings?
I have configured it, but the result is the same.
configuration parameter:
setenv bootargs_mmc 'setenv bootargs; setenv bootargs ${bootargs_base} root=${mmcroot} video=mxcfb0:dev=hdmi,1920x1080M@30,if=RGB24'; run bootcmd_mmc