What's the best BSP for imx28 available now?
I've tried the 2.6.35_1.1.0_130130 BSP, but it have a lot of missing or broken packages.
Maybe is possible to use yocto?
Hi Marco,
Yes you can use Yocto to get the best out of the i.MX28. Here is the machine config file:
meta-fsl-arm/imx28evk.conf at master · Freescale/meta-fsl-arm · GitHub
Note that it is using linux-fslc which is the community kernel based on the Linux kernel 4.1.
meta-fsl-arm/mxs-base.inc at master · Freescale/meta-fsl-arm · GitHub
meta-fsl-arm/linux-fslc_4.1.bb at master · Freescale/meta-fsl-arm · GitHub
Regards,
Gary
HI Marco
one can look at i.MX28 community BSPs
Public images - fsl-community-bsp/master/526/x11
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------