imx25 USB: Full speed only

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx25 USB: Full speed only

823 Views
rohith1z
Contributor III

I want to be able to run the OTG USB port on imx25 in Full speed only mode. What's the best way to do it?

I'm using the on-board UTMI phy.

The reference manual says that:

Software-configurable for full-speed / low-speed interface for Serial transceiver

The only reference I found was bit 24(PFSC) of PORTSCx register.

Is that the recommended method?

Tags (2)
0 Kudos
Reply
1 Reply

745 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Look at the following https://community.nxp.com/message/262460 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply