The default configuration of the bootlet code for the latest i.MX233 support a hardware configuration that has both a LiIon battery configuration. For other configurations though such as a VDD5V connection only or a DCDC_BATT/Battery connection only, some additional changes need to be done.
I'm designing a board with the i.M233 and VDD5V connection with no battery.
What are the additional changes in boot_prep recommended to work this way?
The bootloader also checks the adc to decide which load chain use, based on pressed keys. How could I disable this feature?
Could anyone help me?
Thanks
已解决! 转到解答。
Thank you.
I've not seen the revc schematics till now (only revb).
My problem was that in my board, the DC_DC_BAT and BATT pins were not connected.
By placing a 1K pull-up resistor to 4.2V and a 33uF capacitor to ground to both pins connected together, all starts OK without any change in software.
Thank you.
I've not seen the revc schematics till now (only revb).
My problem was that in my board, the DC_DC_BAT and BATT pins were not connected.
By placing a 1K pull-up resistor to 4.2V and a 33uF capacitor to ground to both pins connected together, all starts OK without any change in software.
You may want to look at U-Boot as it has got MX233 support; the code is much easier to follow and hack than bootlets.
The first version with support for MX233 will be 2013.04 but current GIT has it already; other fixes and improvements (as USB support) has been posted today in mailing list.
There's some patches for i.MX28 available for this kind of setup. As it's quite similar to i.MX233, it may provide some guidelines on how to do this.