imx_rel_3.14.52_1.1.0_ga not support fixed link phy feature?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx_rel_3.14.52_1.1.0_ga not support fixed link phy feature?

910 次查看
wenmingfeng
Contributor III

HI ,

I used imx_rel_3.14.52_1.1.0_ga and when I open menuconfig the item "Driver for MDIOS Bus/PHY emulation with fixed speed/link PHY". I got a compiler error,"error: implicit declaration of function ‘fixed_phy_register’ [-Werror=implicit-function-declaration]
return fixed_phy_register(PHY_POLL, &status, np);" I grep the function not implement any where.

Does somebody have patch for that?

Thanks!

Wenming

标签 (2)
0 项奖励
回复
1 回复

755 次查看
b36401
NXP Employee
NXP Employee

Please refer this conversation. It may help.

https://community.nxp.com/message/538494

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复