iRAM area is not accessible with JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iRAM area is not accessible with JTAG

616件の閲覧回数
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic

JTAG

Debugger

 

Question.  The iRAM area(0x1FFE_0000) is not accessible with JTAG (RV-ICE).

 

Answer. 

1. Please check if ARM core of the i.MX51 is in supervisor mode, when using JTAG. Say, sometimes it may be in thumb one, since internal bootloader uses the thumb mode.

 

2. "Strange" behavior may be detected, if some i.MX51 fuses are "unexpectedly" burned because of power up sequence violation. Let me remind, VDD_FUSE is recommended be floated and grounded.

 

3.After watchdog reset internal memory IRAM is not accessible. Note, internal and UART / USB bootloader start watchdog.

 

 Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

タグ(1)
0 件の賞賛
返信
0 返答(返信)