I have an iMX93EVK, running the supplied factory image and a RPI-CAM-MIPI board.
I have followed the instructions contained within
https://docs.nxp.com/bundle/UM11933/page/topics/getting_started.html
and I get the following error when trying to load the firmware.
[ 2.654564] ap1302_mipi 2-003c: AP1302 Chip ID is 0x265
[ 2.659861] ap1302_mipi 2-003c: Direct firmware load for imx/camera/ap1302.fw
failed with error -2
[ 2.662449] ap1302_mipi 2-003c: Write reg error: reg=0x5058, val=0x186
[ 2.668994] ap1302_mipi 2-003c: Falling back to sysfs fallback for: imx/camera/ap1302.fw
[ 2.675340] ap1302_mipi 2-003c: AP1302 is found
[ 6.530463] ap1302_mipi 2-003c: Fail to write AP1302 firware window ret=-151
[ 8.923634] mx8-img-md: Registered mxc_isi.0.capture as /dev/video0
[ 8.974938] mxc-md 42800000.bus:camera: Entity type for entity ap1302_mipi 2-003c was not initialized!
[ 8.985246] mx8-img-md: Registered sensor subdevice: ap1302_mipi 2-003c (1)
[ 8.992296] mx8-img-md: created link [mxc_isi.0] => [mxc_isi.0.capture]
[ 9.002628] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.0]
[ 9.012548] mx8-img-md: created link [ap1302_mipi 2-003c] => [mxc-mipi-csi2.0]
As a result of the above error I am unable to grab any images from the camera.
Any help would be appreciated.
Maybe you can refer to my previous debug note:
https://community.nxp.com/t5/i-MX-Processors/where-to-get-imx8mp-airobot-ap1302-camre-fw/m-p/1719461...
I am seeing the same error using iMX8MP with an AP1302 on a custom board,
[ 1.824349] ap1302_mipi 3-003c: AP1302 Chip ID is 0x265
[ 1.829670] ap1302_mipi 3-003c: Direct firmware load for imx/camera/ap1302.fw failed with error -2
[ 1.838661] ap1302_mipi 3-003c: AP1302 is found
[ 1.848020] ap1302_mipi 3-003c: Falling back to sysfs fallback for: imx/camera/ap1302.fw
[ 6.180342] ap1302_mipi 3-003c: Failed to request_firmware
In addition to the AP1302 I also see an error with loading the sdma-imx firmware
[ 0.165676] imx-sdma 30bd0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 1.829670] ap1302_mipi 3-003c: Direct firmware load for imx/camera/ap1302.fw failed with error -2
I have seen community responses regarding sdma-imx firmware error being casued by the driver being intialised before the rootfs is available, I was wondering if the issue with the AP1302 firmware is the same.
I have already downloaded that file, renamed it and placed it in /lib/firmware/imx/camera as directed in the document.
The file is found but there is an error programming it
Hello,
You have to download the ap1302 firmware from ONSemiconductor, and rename it as ap1302.fw
Please check it:
https://www.nxp.com/docs/en/application-note/AN13917.pdf
Regards