Hi,
I have an iMX8m Nano flashed with Yocto image:
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.47-2.2.0.xmlimx-manifest - i.MX Release Manifest
DISTRO=fsl-imx-xwayland MACHINE=imx8mnevk source imx-setup-release.sh -b build_nano
I've tested a openCL benchmark on the board and I'm only getting 2 GLOPs compared to the 9.6 GLOPs in the board specifications. I've performed the same test on the quad-max board, getting 20 GLOPs compared to the 32 theoretical GLOPs. As a rule of thumb, I should get around 6 GLOPs on the iMX8m Nano based on the quad-max results.
I can see that the freq of the GPU core and shader is well set to 600 MHz, but the performance is low.
Is there any configurations that I might be missing?
Thanks
Hi,
Any update on this issue?
Best regards
Hello Miguel,
Please share your sample code in order to check it.
Regards
Here it is the benchmark: https://github.com/ekondis/mixbench
I have followed the openCL benchmark. The results come from the mixbench-ocl-ro binary.
The mixbench-ocl-alt binary runs on the imx8 quad-max but does not in the imx8m nano.
Thanks for your time
PD: I'd be interested to know whether you have any Vulkan benchmark to test on my machine.