Hi,
I have a problem recently. I am using USB Camera with iMX8qm-mek board for Android 9 Automotive. USB camera is not detecting and usb camera using uvc driver. I checked the kernel side,
CONFIG_MEDIA_USB_SUPPORT=y
CONFIG_USB_VIDEO_CLASS=y
Thanks & Regards,
VinothS,
Solved! Go to Solution.
Hi,
finally, I fixed this problem in the lib side,
vendor/nxp-opensource/imx/libcamera3/CameraHAL.cpp
configure this mCameraCount flag as 1 in handleCameraConnected function
Thanks & Regards,
VinothS,
Hi,
finally, I fixed this problem in the lib side,
vendor/nxp-opensource/imx/libcamera3/CameraHAL.cpp
configure this mCameraCount flag as 1 in handleCameraConnected function
Thanks & Regards,
VinothS,
Hi,
I Unable to access the camera.
FslCameraHAL: getNodeName open dev path:/dev/video0 failed:No such file or directory
Do I have to give the permission to access the device ?
Thanks & Regards,
VinothS,
Hi,
Camera detected successfully. But. I got some of the following error
mek_8q:/ $ [ 43.526628] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 43.531563] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 43.555484] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 43.561159] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 43.567966] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 43.575204] usb usb1: Product: EHCI Host Controller
[ 43.580094] usb usb1: Manufacturer: Linux 4.14.98-dirty ehci_hcd
[ 43.586117] usb usb1: SerialNumber: ci_hdrc.0
[ 43.593894] hub 1-0:1.0: USB hub found
[ 43.597698] hub 1-0:1.0: 1 port detected
[ 43.935478] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 44.316106] usb 1-1: New USB device found, idVendor=046d, idProduct=0825
[ 44.322846] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=2
[ 44.330558] usb 1-1: SerialNumber: 06822680
[ 44.349241] uvcvideo: Found UVC 1.00 device <unnamed> (046d:0825)
[ 44.447420] uvcvideo 1-1:1.0: Entity type for entity Extension 4 was not initialized!
[ 44.455322] uvcvideo 1-1:1.0: Entity type for entity Extension 6 was not initialized!
[ 44.463208] uvcvideo 1-1:1.0: Entity type for entity Extension 7 was not initialized!
[ 44.471080] uvcvideo 1-1:1.0: Entity type for entity Processing 2 was not initialized!
[ 44.479020] uvcvideo 1-1:1.0: Entity type for entity Extension 3 was not initialized!
[ 44.486859] uvcvideo 1-1:1.0: Entity type for entity Camera 1 was not initialized!
[ 44.495945] input: UVC Camera (046d:0825) as /devices/platform/5b0d0000.usb/ci_hdrc.0/usb1/1-1/1-1:1.0/input/input2
130|mek_8q:/ $ ls -l /dev/video0
crw-rw---- 1 system camera 81, 2 2020-01-06 05:47 /dev/video0
and detect as video0.
Thanks & Regards,
VinothS,
Hi,
USB Camera is working with this predefined application (not in AOSP build). I don't how it is possible without kernel support for UVC - USB camera.
followed for predefined APK,
Thanks & Regardsm
VinothS,
Hi, I got following error from framework when I try to access the default camera application and application itself crashed.
# am start -a android.media.action.VIDEO_CAPTURE
mek_8q:/ # logcat | grep CameraService
01-02 09:22:54.863 1754 1754 E CameraService: cameraIdIntToStrLocked: input id 0 invalid: valid range (0, 0)
01-02 09:22:54.864 1754 1754 I CameraService: CameraService::connect call (PID -1 "com.android.camera2", camera ID ) for HAL version default and Camera API version 1
01-02 09:22:54.864 1754 1754 E CameraService: CameraService::connect X (PID 4114) rejected (invalid camera ID )
source/frameworks/av/services/camera/libcameraservice/CameraService.cpp
Thanks & Regards,
VinothS,
I have the same issue to access camera.
12-17 06:39:40.246 1465 1658 E CameraService: cameraIdIntToStrLocked: input id 0 invalid: valid range (0, 0)
12-17 06:39:40.246 1465 1658 I CameraService: CameraService::connect call (PID -1 "photo.android.hd.camera", camera ID ) for HAL version default and Camera API version 1
12-17 06:39:40.247 1465 1658 E CameraService: CameraService::connect X (PID 3468) rejected (invalid camera ID )
.....................................................................................................................
I am using the same target and android 9 auto version.
I got the /dev/video* nodes.
I set the front_camera and back_camera properties.
To debug, I am not getting logs from the HAL.
I confirmed camera.imx8.so is present at /vendor/lib64/hw.
and cameraserver is running as
mek_8q:/ # ps -ef | grep camera
cameraserver 1438 1 0 06:44:43 ? 00:00:00 android.hardware.camera.provider@2.4-service
cameraserver 1465 1 0 06:44:44 ? 00:00:00 cameraserver
Could you please help me on why I am not getting any logs with FslCameraHAL tag?
Is there anything else I need to do for getting those logs for debugging.
Hello,
Unfortunately, Android Auto is not supported by us. However, what I suggest is to add the following configuration in the init.rc.
setprop back_camera_name uvc
Unfortunately, this is as far as we could go.
Best regards,
Diego.