Dear all,
I'm working with different iMX based platform, from iMX6* to iMX8*
We are used to look at SOC Unique ID to identify products on field because this is guarantee to be unique for each single component
I've notice a major changes between iMX8MP and the others (even iMX8MM for example): usually SOC Unique ID is a 32 bit number, but on iMX8MP is a 64 bit number
I'm wondering if we can use a 32 bit subset of these 64 bit and yet assume that this number is unique across all SOCs, so we can have a higher level of software compatibility across the whole iMX family
Any clue or additional information?
Kind Regards and Thanks in advance,
Andrea
已解决! 转到解答。
BTW a colleague of mine asked the same question to NXP dedicated support and have the confirm that:
The UID[127-64] located on bank 40, world 0 and word 1.
so we have an official answer to share.
Hope this help others in our same situation
Hi @andreascian
Sorry for replying to you with delay.
More details hope to help you, SoC UID is a read-only fuse value, which is programmed by the factory to identify a unique SoC, and this value is randomly generated. duplicate would happen if use only 32bits.
Best regards
Harvey
Hi Harvey
on iMX8MP I've also found some additional UNIQUE_ID bits into the fusemap, see fuse address 0xE00-0xE10 named as UNIQUE_ID[127:64]
Does it means that UNIQUE_ID is 128 bit wide on this platform?
sorry for replying to this old thread, but can you help me in figuring out which bank/register is associated with these upper 64 bits?
IIUC 0xE00 should correspond to bank 40 register 0 but can please confirm this?
BTW a colleague of mine asked the same question to NXP dedicated support and have the confirm that:
The UID[127-64] located on bank 40, world 0 and word 1.
so we have an official answer to share.
Hope this help others in our same situation
I reply to myself because I also opened a support ticket. Support team already reply that I was wrong and SOC UniqueID is 64 bit in both iMX8MP and iMX8MM and that's guarantee unique only it's full 64 bit format