iMX8MP HAB Secure boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8MP HAB Secure boot

1,268 Views
wudiqiang2046
Contributor I

I installed Debian 12 img to the Live USB, and then I successfully enabled CONFIG_IMX_HAB by modifying the u-boot configuration file, compiled and copied it to the system, then I inserted the USB into the device, the system booted from the USB, and then installed the system into the device, then I unplugged the USB and booted the system in the device, and entered u-boot and could use the hab_status command to output information. But when I plugged in the USB again, I found that I could not boot from the USB, why is this? Is it because if secure boot is enabled, I can no longer boot from the USB?

0 Kudos
Reply
1 Reply

1,214 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi

As far as I know, Debian 12 does not support secure boot so far.

 

Regards

Harvey

0 Kudos
Reply