iMX8M Quad / iMX8M Plus Quad || PCIe Speed and Bandwidth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8M Quad / iMX8M Plus Quad || PCIe Speed and Bandwidth

698件の閲覧回数
JyotiVaishnav
Contributor II

Hello NXP Team, 

We are planning to use i.MX 8M Quad or i.MX 8M Plus Quad. 

Can you please share the details of the PCIe interface for both the processor how much Speed and Bandwidth both the processor will support.  . 

 

0 件の賞賛
返信
3 返答(返信)

681件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

For the i.MX8MQ has two pcie interface and the i.MX8MP has only one, for the pcie features you can see details in the RM, here take the i.MX8MP as example:

b45499_0-1695195477400.png

 

0 件の賞賛
返信

661件の閲覧回数
JyotiVaishnav
Contributor II

Hello @Rita_Wang 

Thanks for sharing the information. 

In iMX8M Quad there are two PCIe interface available, on one PCIe we are planning to connect the SSD and on the other PCIe AI Chip

Is it okay to connect ? 

0 件の賞賛
返信

629件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you can use.

0 件の賞賛
返信