iMX8 Nano DDR4 DRAM_VREF capacitor values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX8 Nano DDR4 DRAM_VREF capacitor values

1,012 次查看
frank_vanhooft
Contributor III

Looking at the NXP reference design for the iMX8 Nano with DDR4, there are some 1uF and 0.01uF capacitors used to filter the generated DRAM_VREF signal.  Are these capacitor values critical? Specifically, is there any problem with using 4.7uF in those 3 locations? (Because we already have a bunch of 4.7uF's on the board, so I'd like to limit the number of BOM items - particularly that 0.01uF as it's the only one on the board.)

Thanks a lot.

pastedImage_1.png

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

917 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

  The C389 and C390 can change to 4.7uF from 1uF, please note the value of the two capacitor must be the same, But C110 can not be changed, C110 and C389 are in parallel.

0 项奖励
回复

917 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

I am confirming it and give you reply as soon as possible.

0 项奖励
回复