iMX7D A7 core power down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX7D A7 core power down

690 Views
sunildhaduk
Contributor IV

Hello,

I want to use M4 core only in iMX7D (Sabre Board) and want to shut down both A7 cores.

Please tell me which register settings will be required to put both A7 core in shut down?

How to power off A7 core, L2 controller and SCU supply using internal switches and using PMIC (PF3000)?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

540 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Sunil,

you can set A7 cores to be in low power modes, but not power them off or turning their clocks off.

As you can see in Figure 5-15. CCM Clock Tree Root Slices of i.MX 7Dual Applications Processor Reference Manual there is no clock gate to the A7 cores as it is for the M4.

pastedImage_1.png


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply