iMX6UL resolution under VGA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL resolution under VGA

2,176 Views
julbert
Contributor II

Hi,


I'm find misleading table at the attached pdf file's 25 page.

The table at the right side describes the iMX6UL processor's supported resolutions.
As I see there are no display support under VGA resolution.

My intuition is that lower resolutions ! have to OK for the UltraLite, but I have to be sure.

I want to use the UltraLite with a 480x272 resolution display is it possible ?

Regards János

Labels (1)
3 Replies

1,832 Views
igorpadykov
NXP Employee
NXP Employee

Hi János

you are right, lower resolutions are supported by UltraLite too.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,832 Views
CrankSoftware
Contributor II

The default screen that comes with the board is 480x272. Here is a link to a video we did of the UL running our demos at 480x272

iMX6UltraLite | Crank Software 

Regards,

Jason

1,832 Views
julbert
Contributor II

Dear Jason,

Thanks for the fast reply!

0 Kudos
Reply