Hi,
I'm find misleading table at the attached pdf file's 25 page.
The table at the right side describes the iMX6UL processor's supported resolutions.
As I see there are no display support under VGA resolution.
My intuition is that lower resolutions ! have to OK for the UltraLite, but I have to be sure.
I want to use the UltraLite with a 480x272 resolution display is it possible ?
Regards János
Hi János
you are right, lower resolutions are supported by UltraLite too.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The default screen that comes with the board is 480x272. Here is a link to a video we did of the UL running our demos at 480x272
iMX6UltraLite | Crank Software
Regards,
Jason
Dear Jason,
Thanks for the fast reply!