iMX6Q Pinning Parallel Camera 12-bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6Q Pinning Parallel Camera 12-bit

ソリューションへジャンプ
2,134件の閲覧回数
michael_irsfeld
Contributor I

Hello,

I'm trying to interface two cameras (Bayer12) via parallel sensor interface. In datasheet of iMX6Q on table 64 I can only find which IPU ports i should use for a 16-bit camera. Which IPU-Ports should I use for 12-bit camera?

Thanks
Michael

ラベル(3)
0 件の賞賛
返信
1 解決策
1,941件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi michael,

For possible sensor connections, please look at the datasheet(s),

for example - Table (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC.

https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

IPU0-1 can be used for 12bit.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,942件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi michael,

For possible sensor connections, please look at the datasheet(s),

for example - Table (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC.

https://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

IPU0-1 can be used for 12bit.

0 件の賞賛
返信