Hello,
I have been searching around forum for design resources for i.MX6 SoloX and I have found the design files for Sabre board with SoloX. Unfortunately I can't fit this layout to my potential application so I have to go for a MAPBGA 400 package.
Is it possible to get at least verified schematic symbol for MCIMX6X3xxxxxx (MPBGA400 SoloX) importable to Altium designer?
Any help appreciated, it would accelerate start of the design a lot.
解決済! 解決策の投稿を見る。
Please find attached the archive, containing a fake i.MX6SX schematics, consisting of only the i.MX6SX MAPBGA400 schematic symbol for all available package types: 14x14mm, 17x17mm No PCIe and 17x17mm With PCIe. These schematics are saved in the OrCAD 16.2 format that seems to be easily importable into the current version of the Altium Designer tool. Please try it.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur, hi Martin,
I tried to import all three package types: 14x14mm, 17x17mm No PCIe and 17x17mm With PCIe
with my Altium Designer 15.0.7 installation.
Unfortunately in all 3 cases the import ends with following Altium Error Message :
Access violation at address ... in module 'Orcad7ld.dll'.
Read of address 00000000 at 4F....
Which Version did you use, Martin ?
Have you any idea for the reason ?
Kind regards,
Jens
Thank you very much Arthur, it works, was successful to import it¨to Altium Designer.
Please find attached the archive, containing a fake i.MX6SX schematics, consisting of only the i.MX6SX MAPBGA400 schematic symbol for all available package types: 14x14mm, 17x17mm No PCIe and 17x17mm With PCIe. These schematics are saved in the OrCAD 16.2 format that seems to be easily importable into the current version of the Altium Designer tool. Please try it.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------