Does anyone know where I can get a schematic/PCB symbol for the iMX6 Solo/DualLite processor?
解決済! 解決策の投稿を見る。
Hi Clive,
I can't find how to save the library as *.llb, but I managed to save it in 16.2 format. I'm also attaching sch-27516 in 16.2 in case you want to extract something from there. About the pcb symbol, allegro doesn't seem to have the option to save it as an old version, but I saved it as *.brd instead of *.dra. If this doesn't work for you I'll try to find an alternative.
Best regards.
Jorge.
I'm working on a new design with iMX6, and we are targeting to use iMX6 Dual POP package. Is there schematic symbol and/or footprint available for this device (MCIMX6D5EZK08AD).
Regards,
Boris Snajder
Can you help to convert the schematic from orcad 16 version to orcad ver10?
I have an older version and cannot open the new version
Here's the layout in Altium format for the SABRE Board for Smart Devices Based on the i.MX 6 Series Product Summary Page revision C3.
https://dl.dropboxusercontent.com/u/109867706/EVALBOARD_20130430.zip
If you want the footprints: Tools => Make integrated library.
Dear Peter,
could u please send the Altium format for the SABRE Board for Smart Devices Based on the i.MX 6 Series Product Summary Page revision C3.
it nowadays gives a 404
thanks in advance
Dear Peter,
Thanks for the PCB however, Tools => Make integrated library. does not work (most likely because no schematic )
Do you by any chance have the altium schematic as well??
So l can fetch the actual fetch the integrated library from the board?
Which symbol is it that you require?
I'm sorry but I don't have the schematic part saved, but I did convert a number of the parts on the board.
The quad imx6
Would be most helpfull
Verstuurd vanaf mijn iPhone
Op 10 sep. 2013 om 16:33 heeft "Peter Hygren" <admin@community.freescale.com> het volgende geschreven:
iMX6 Solo/DualLite processor schematic/PCB symbol
reply from Peter Hygren in i.MX Community - View the full discussion
Which symbol is it that you require?
I'm sorry but I don't have the schematic part saved, but I did convert a number of the parts on the board.
Reply to this message by replying to this email, or go to the message on Freescale Community
Start a new discussion in i.MX Community by email or at Freescale Community
Following iMX6 Solo/DualLite processor schematic/PCB symbol in these streams: Inbox
Attaching footprint and symbol library for IMX6Q and IMX6D (they share symbol and footprint).
In the PCB library I've added 2 footprints for the processor, one extracted from the SABRE Smart Devices board, and one I created myself. The symbol is linked to the footprint I created, and it's been verified to work on a number of boards now with no complaints from assembly line.
Regards,
Peter Hygren
Hi,
does anybody have a symbol/footprint for the iMX6 Quad version?
cheers Karl
What's with all the missing pads?
Hi Peter,
This footprint is for the i.MX6 SoloLite. I've asked Yuri for the Solo/DualLite footprint - see my previous post.
Cheers,
Clive
Yuri, works a treat. Thanks, Clive
Hi Clive
How did you manage to get the symbol into Altium Designer? The importer simply say "not recognized"...
Could you please upload you AD version? Thanks a lot!
Best regards,
-Rob
Clive and Rob,
I am traveling the same path you did with Yuri's files. Any chance you can post the complete Altium Project of the imported Ref Design?
Regards,
DAU
Thanks for the file Clive. I am trying to put together a complete Altium project - schematics plus pcb with cross probing nets. I have started with SCH-27516_16_2 but I'm not sure which PCB matches. Can you explain the numbering? I have documents with the following numbers 27516, 27392, 27417, 27452. Are there descriptions of each of these somewhere?
Regards,
DAU
Hi Clive
Thank you very much! I owe you a beer or two!
Kind regards,
-Rob